You can find the results of your wiki search below. If you didn't find what you were looking for, you can create or edit the page named after your query with the appropriate button, or search the rest of Analog.com. If that doesn't work, try Google.
^^
| AD-FMCBRIDGE1A | FMC Card with level translators and power supplies; ... gnal rails|
| Custom cable| For power rails|
The FMC Xmicrowave bridge Kit contains both the FMC Xmicrowave Bridge Board and the FMC Xmicrowave Protoplate Board.
{{ :resources:eval:user-guides:ad-
]
=== ADXUD1AEBZ ===
* [[digikey>HDR-169468-01|FMC extension]]
* [[digikey>H3AKH-1406G|14-Pin PMOD... e (optional)]]
<note>The [[digikey>HDR-169468-01|FMC extension]] is used both to move the interposer b... m/shop/us/products/avnet-engineering-services/aes-fmc-ext-g-3074457345635221630/|1x FMC riser]]
<note>If the suggested vendor for the FMC Riser has no stoc
ev D or later board
* [[:resources:eval:sdp:sdp-fmc|SDP to FMC Interposer]]
* 12Vdc, 3A power supply
* Micro-USB cable
* Ethernet cable
* User i... edboard/ | ZedBoard]].\\ {{ resources:fpga:xilinx:fmc:AD777x-ARDZ:zedboard.png?600 }}
* Insert the SD... ]] board to the SDP adaptor and into the ZedBoard FMC connector.\\
* Connect USB UART J14 (Micro USB)
nels that are interfaced with an FPGA through the FMC Low Pin Count (LPC) Connector. Current revision o... adi>ADAQ23876]] is routed to the FPGA through the FMC LPC connector using a serial low voltage differen... the [[adi>AD3552R]] DAC from the FPGA through the FMC LPC connector using a Quad-SPI dual data rate int... ators are used on the board to interface with the FMC connector signals and the various logic levels us
===== ADRV2CRR-FMC Carrier Board Hardware Overview =====
{{:resources:eval:user-guides:adrv9009_zu11eg:adrv2crr-fmc_desc.png|}}
The ADRV2CRR-FMC is the carrier board to allow users evaluate the functionality of the AD... Wiki-page]].
==== Power Input ====
The ADRV2CRR-FMC has a single 12V supply input, distributed to the
ware-and-software/evaluation-boards-kits/ADRV1CRR-FMC.html|ADRV1CRR-FMC]] carrier board. The ADRV9364-Z7020 supports a subset of features because the Z... V1CRR-BOB.html|ADRV1CRR-BOB]] carrier.
^ ADRV1CRR-FMC ^ ADRV1CRR-BOB ^
| {{https://www.analog.com/-/med... analog/en/evaluation-board-images/images/adrv1crr-fmc-angle-web.gif?250}} | {{https://www.analog.com/-/
~~NOTOC~~
===== AD-DAC-FMC-EBZ reference HDL design =====
The [[https://github.com/analogdevicesinc/hdl/tree/main/projects/dac_fmc_ebz|dac_fmc_ebz]] is a generic reference design that can be configured to support one of the following... b.com/analogdevicesinc/hdl/tree/main/projects/dac_fmc_ebz
</WRAP>
==== Software support ====
<note imp
====== AD-FMCADC2-EBZ FMC Board ======
<note warning>**NOTE:**\\
Support for the ad-fmcadc2-ebz is dis... di>AD9625]] single channel ADC at 2500 MSPS, in a FMC form factor which supports the JESD204B high speed serial interface. This board meets most of the FMC specifications in terms of mechanical size, mount... d more. For that information, please refer to the FMC specification.
Although this board does meet mos
====== AD-FMCADC5-EBZ FMC Board ======
<note warning>**NOTE:**\\
Support for the ad-fmcadc5-ebz is dis... s Inc.
Although this board does meet most of the FMC specifications, it is not meant as a [[wp>Commerc... duct is required, please refer to one of the many FMC manufacturers.
ADI also provides reference desig... == Hardware =====
The AD-FMCADC5-EBZ is a double FMC wide board and requires two fully populated (tran
ld programmable gate array (FPGA) mezzanine card (FMC) form factor, powered with 12 V either from the FMC connector or an external supply. The digital inter... and 2) \\ TWOLANES = Low (Pins 2 and 3) |
| P4 | FMC Connector (LPC) | Low pin count FMC connector used to connect the EVAL-CN0577-FMCZ hardware to various
MK180]] rev A
* AD9081-FMCA-EBZ/AD9082-FMCA-EBZ FMC board.
* USB type-C cable
* Ethernet cables
... ?900 |}}
* Connect the [[adi>AD9081-FMCA-EBZ]] FMC board to the FPGA carrier **FMC+** FMCP1 socket.
* Connect USB UART J207 (Type-C USB) to your host P... d be assigned. Go to this web address to set VADJ_FMC to 1.5V.
* To change VADJ_FMC On BEAM, click 'T
P_H1]] which connects to the EVAL-ADMX100X-FMCZ's FMC connector.
{{ :resources:eval:user-guides:admx:e... evaluation board via (P5) module connector.
* FMC connector: The SDP-H1 will connect to the FMC connector that is on the bottom of the board.
* Power ... oard to the EVAL-ADMX100X-FMCZ evaluation board's FMC connector (P1).
- Connect the SDP controller U
a_ebz_hdl##board_setup&nofooter&noeditbtn}}
==== FMC Pin Connection Configuration Change ====
<WRAP c... on of the Arria10 SoC Development Kit some of the FMC header pins are connected to a dedicated clock ch... of the Arria10 SoC Development Kit underneath the FMC A connector (J29). The following picture shows th... eval:user-guides:ad-fmcdaq2-ebz:quickstart:a10soc_fmc_rework.jpg |}}
===== Connections =====
* Inse