Fulltext results:
- FMCOMMS11 HDL Reference Design @resources:eval:user-guides:ad-fmcomms11-ebz
- nnels are connected to the appropriate high speed FMC lane. The lane remapping is done after the JESD20... GE_PIN AH10} [get_ports rx_data_p[0]] ; ## C06 FMC_HPC_DP0_M2C_P set_property -dict {PACKAGE_PIN AH9 } [get_ports rx_data_n[0]] ; ## C07 FMC_HPC_DP0_M2C_N set_property -dict {PACKAGE_PIN AJ8 } [get_ports rx_data_p[1]] ; ## A02 FMC_HPC_DP1_M2C_P set_property -dict {PACKAGE_PIN A
- AD-FMCXMWBR1-EBZ Hardware @resources:eval:user-guides:ad-fmcxmwbr1-ebz
- ^^ | AD-FMCBRIDGE1A | FMC Card with level translators and power supplies; ... gnal rails| | Custom cable| For power rails| The FMC Xmicrowave bridge Kit contains both the FMC Xmicrowave Bridge Board and the FMC Xmicrowave Protoplate Board. {{ :resources:eval:user-guides:ad-
- ADRV2CRR-FMC Production Testing @resources:eval:user-guides:adrv2crr-fmc
- ====== ADRV2CRR-FMC Production Testing ====== ===== Overview ===== Production tests for ADRV9009-ZU11E... s presented bellow should be inserted in ADRV2CRR-FMC P15 slot. * CAT5 ethernet cable: Using ethern... (pins 3 - SDA, 2 - SCL and 6 – GND) and ADRV2CRR-FMC P19 pin header. Using this connection and item 1 ... d for powering up the Raspberry Pi * ADRV2CRR-FMC: is the carrier board that can be tested selectin
- FMCOMMS8 Quick Start Guide @resources:eval:user-guides:ad-fmcomms8-ebz
- from folder zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8 * [[ https://github.com/an... ===== * ADRV9009-ZU11EG SoM board * ADRV2CRR-FMC carrier board * FMCOMMS8 evaluation board * M... V9009-ZU11EG'' System on Module to the ''ADRV2CRR-FMC'' carrier board. * Connect the ''FMCOMMS8'' to the ''ADRV2CRR-FMC'' carrier board using the FMC HPC connector. *
- X-Band Platform Hardware @resources:eval:user-guides:x-band-platform
- ] === ADXUD1AEBZ === * [[digikey>HDR-169468-01|FMC extension]] * [[digikey>H3AKH-1406G|14-Pin PMOD... e (optional)]] <note>The [[digikey>HDR-169468-01|FMC extension]] is used both to move the interposer b... m/shop/us/products/avnet-engineering-services/aes-fmc-ext-g-3074457345635221630/|1x FMC riser]] <note>If the suggested vendor for the FMC Riser has no stoc
- EVAL-AD2S1210SDZ Evaluation Board on ZedBoard User Guide
- ev D or later board * [[:resources:eval:sdp:sdp-fmc|SDP to FMC Interposer]] * 12Vdc, 3A power supply * Micro-USB cable * Ethernet cable * User i... edboard/ | ZedBoard]].\\ {{ resources:fpga:xilinx:fmc:AD777x-ARDZ:zedboard.png?600 }} * Insert the SD... ]] board to the SDP adaptor and into the ZedBoard FMC connector.\\ * Connect USB UART J14 (Micro USB)
- EVAL-CN0585-FMCZ User Guide @resources:eval:user-guides:circuits-from-the-lab
- nels that are interfaced with an FPGA through the FMC Low Pin Count (LPC) Connector. Current revision o... adi>ADAQ23876]] is routed to the FPGA through the FMC LPC connector using a serial low voltage differen... the [[adi>AD3552R]] DAC from the FPGA through the FMC LPC connector using a Quad-SPI dual data rate int... ators are used on the board to interface with the FMC connector signals and the various logic levels us
- ADRV2CRR-FMC Carrier Board Hardware Overview @resources:eval:user-guides:adrv9009-zu11eg
- ===== ADRV2CRR-FMC Carrier Board Hardware Overview ===== {{:resources:eval:user-guides:adrv9009_zu11eg:adrv2crr-fmc_desc.png|}} The ADRV2CRR-FMC is the carrier board to allow users evaluate the functionality of the AD... Wiki-page]]. ==== Power Input ==== The ADRV2CRR-FMC has a single 12V supply input, distributed to the
- ADRV9009-ZU11EG Multi-SOM Synchronization @resources:eval:user-guides:adrv9009-zu11eg
- t/dts/xilinx/zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-jesd204-fsm-multisom-primary.dts | zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-jesd204-fsm-multisom-primary.dts]] | | ... t/dts/xilinx/zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-jesd204-fsm-multisom-secondary.dts | zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-jesd204-fsm-multisom-secondary.dts]] |
- ADRV9361-Z7035 Quick Start Guide @resources:eval:user-guides:adrv9361-z7035
- ware-and-software/evaluation-boards-kits/ADRV1CRR-FMC.html|ADRV1CRR-FMC]] carrier board. The ADRV9364-Z7020 supports a subset of features because the Z... V1CRR-BOB.html|ADRV1CRR-BOB]] carrier. ^ ADRV1CRR-FMC ^ ADRV1CRR-BOB ^ | {{https://www.analog.com/-/med... analog/en/evaluation-board-images/images/adrv1crr-fmc-angle-web.gif?250}} | {{https://www.analog.com/-/
- ADRV9009-ZU11EG RF System-on-Module
- er board is required. The Analog Devices ADRV2CRR-FMC Carrier board is designed for this purpose. An a... ring) **The Carrier box includes:** * ADRV2CRR-FMC carrier board(needed to evaluate the RF-SOM), SD-... hernet Phy * USB 2.0 Phy * 12V supply via FMC connectors * uSD Card holder * Storage and ... sources:eval:user-guides:adrv9009-zu11eg:adrv2crr-fmc_carrier_board|ADRV2CRR-FMC]] Carrier Board. Rev
- ADRV9009-ZU11EG Production Testing @resources:eval:user-guides:adrv9009-zu11eg
- s presented bellow should be inserted in ADRV2CRR-FMC P15 slot. * CAT5 ethernet cable: Using ethern... (pins 3 - SDA, 2 - SCL and 6 – GND) and ADRV2CRR-FMC P19 pin header. Using this connection and item 1 ... d for powering up the Raspberry Pi * ADRV2CRR-FMC: is the carrier board that can be tested selectin... u. It can be tested or used when testing ADRV2CRR-FMC * QSFP loopback: should be connected to P3 on
- AD-DAC-FMC-EBZ reference HDL design
- ~~NOTOC~~ ===== AD-DAC-FMC-EBZ reference HDL design ===== The [[https://github.com/analogdevicesinc/hdl/tree/main/projects/dac_fmc_ebz|dac_fmc_ebz]] is a generic reference design that can be configured to support one of the following... b.com/analogdevicesinc/hdl/tree/main/projects/dac_fmc_ebz </WRAP> ==== Software support ==== <note imp
- ADRV936X_RFSOM production testing @resources:eval:user-guides:pzsdr
- Then, insert the next module for testing. ===== FMC Carrier ===== ==== Overview ==== The carrier te... signals are measured, 3 of them generated by the FMC loopback at the same frequency of 156MHz and one is generated by the AD9517 PLL * SFP+, FMC loopback test. This is an instance of the axi_adx... es. One transceiver lane (lane 0) is used for the FMC connector P2 and the other one (lane 1) for the S
- AD-FMCOMMS6-EBZ Hardware @resources:eval:user-guides:ad-fmcomms6-ebz
- Main components ===== {{ :resources:fpga:xilinx:fmc:fmcomms6:main_components.jpg?direct&600 }} =====... lacements of the board. {{:resources:fpga:xilinx:fmc:fmcomms6:fmcomms6_top.jpg?direct&400 | }} \\ \... 2 inches (or about 89mm x 69mm). This exceeds the FMC specifications of 84mm x 69mm). {{:resources:fpga:xilinx:fmc:fmcomms6:fmcomms6_dim.jpg?direct&400 | }} \\ \
- AD-FMCOMMS8-EBZ Arria10 SoC Quick Start Guide @resources:eval:user-guides:ad-fmcomms8-ebz:quickstart
- Introduction to boards based on the AD9361/AD9363/AD9364 @resources:eval:user-guides:ad-fmcomms2-ebz
- AD-FMCXMWBR1-EBZ on ZynqMP ADRV9009-ZU11EG-ADRV2CRR-FMC @resources:eval:user-guides:ad-fmcxmwbr1-ebz:software:linux
- AD9081/AD9082 Versal ACAP VCK190/VMK180 Quick Start Guide @resources:eval:user-guides:ad9081_fmca_ebz:quickstart
- ADMX1001 and ADMX1002, Ultra-low Distortion, Low Noise Signal Generator and Acquisition Evaluation Modules @resources:eval:user-guides:admx
- EVAL-ADRV9371 Arria10 SoC Development Kit Quick Start Guide @resources:eval:user-guides:adrv9371:quickstart
- AD-FMCOMMS1-EBZ Quick Start Guide on Xilinx FPGA Boards Without OS @resources:eval:user-guides:ad-fmcomms1-ebz:quickstart
- EVAL-ADRV9009 Arria10 SoC Development Kit Quick Start Guide @resources:eval:user-guides:adrv9009:quickstart
- AD-FMCDAQ2-EBZ Arria10 SoC Development Kit Quick Start Guide @resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart
- AD9081/AD9082 Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide @resources:eval:user-guides:ad9081_fmca_ebz:quickstart
- AD9081-FMCA-EBZ / AD9082-FMCA-EBZ (Single MxFE) HDL Reference Design @resources:eval:user-guides:ad9081_fmca_ebz
- AD-FMCOMMS2/3/4/5-EBZ Zynq and ZED Quick Start Guide @resources:eval:user-guides:ad-fmcomms2-ebz:quickstart
- ADRV9002 Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide @resources:eval:user-guides:adrv9002:quickstart
- ADRV9009-W/PCBZ Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide @resources:eval:user-guides:adrv9009:quickstart
- AD-FMCMOTCON1-EBZ Linux on Zynq Quick Start Guide @resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart
- AD-FMCDAQ2-EBZ ZynqMP ZCU102 Quick Start Guide @resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart
- AD-FMCDAQ3-EBZ Virtex UltraScale+ VCU118 Quick Start Guide @resources:eval:user-guides:ad-fmcdaq3-ebz:quickstart
- AD-FMCJESDADC1-EBZ Microblaze Quick Start Guide @resources:eval:user-guides:ad-fmcjesdadc1-ebz:quickstart
- AD-FMCOMMS1-EBZ KC705/VC707 Quick Start Guide @resources:eval:user-guides:ad-fmcomms1-ebz:quickstart
- AD-FMCOMMS2-EBZ Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide @resources:eval:user-guides:ad-fmcomms2-ebz:quickstart
- AD9208-DUAL-EBZ Virtex UltraScale+ VCU118 Quick Start Guide @resources:eval:user-guides:ad9208_dual_ebz:quickstart
- Linux on the Xilinx KC705 Kintex™-7 FPGA development Board @resources:eval:user-guides:ad-fmcomms1-ebz:software:linux
- Quickstart: Setup your CN0506 in ZC706 @resources:eval:user-guides:circuits-from-the-lab:cn0506:quickstart
- AD-FMCDAQ2-EBZ/AD-FMCDAQ3-EBZ Microblaze Quick Start Guide @resources:eval:user-guides:ad-fmcdaq2-ebz:quickstart
- AD-FMCDAQ3-EBZ Kintex UltraScale KCU105 Quick Start Guide @resources:eval:user-guides:ad-fmcdaq3-ebz:quickstart
- AD9081/AD9082 Virtex UltraScale+ VCU118 Quick Start Guide @resources:eval:user-guides:ad9081_fmca_ebz:quickstart
- Linux on the Xilinx ML605 Virtex6 FPGA development Board @resources:eval:user-guides:ad-fmcomms1-ebz:software:linux
- AD-FMCDAQ2-EBZ/AD-FMCDAQ3-EBZ on Zynq ZC706 @resources:eval:user-guides:ad-fmcdaq2-ebz:software:linux
- AD-FMCMOTCON2-EBZ Linux on Zynq Quick Start Guide @resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart
- EVAL-ADRV9026/ADRV9029 Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide @resources:eval:user-guides:adrv9026:quickstart
- Shell Scripts for the FMC RF boards @resources:eval:user-guides:ad-fmcomms1-ebz:software:linux:applications
- Portable Radio Reference Design - Assembly Instructions @resources:eval:user-guides:pzsdr:carriers:portable-radio-reference-design
- Evaluating the ADF5902, 24 GHz, ISM Band, Multichannel FMCW Radar Transmitter @resources:eval:user-guides:eval-adf5902:software
- Evaluating the ADF4377 Microware Wideband Synthesizer with Integrated VCO @resources:eval:user-guides:eval-adf4377:software