The CN0363 HDL reference design and software are designed to operate with the following hardware and FPGA development system:
The equipment should be connected as shown below, make sure that all power is off before starting to make the connections.
Boot (JP7-JP11) and MIO0 (JP6) jumpers are set to SD card mode. To use USB peripheral devices with ZedBoard, install jumpers JP2 and JP3. The FMC interface spans over two PL I/O banks, banks 34 and 35. To meet the FMC spec, these banks are powered from an adjustable voltage set by jumper, J18. Selectable voltages include 1.8V and 2.5V (currently set).
For more detailed information on the ZedBoard jumper settings, check out the ZedBoard Hardware User Guide, available on the ZedBoard doc page, the Jumper Settings chapter.