Wiki

No renderer 'pdf' found for mode 'pdf'
This version (04 Nov 2021 16:17) was approved by Robin Getz.The Previously approved version (26 Mar 2020 00:31) is available.Diff

AD-FMCOMMS3-EBZ User Guide

The AD-FMComms3-EBZ is an FMC board for the AD9361, a highly integrated RF Agile Transceiver™. While the complete chip level design package can be found on the the ADI web site. Information on the card, and how to use it, the design package that surrounds it, and the software which can make it work, can be found here.

The purpose of the AD-FMComms3-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform which operates over a much wider tuning range (70 MHz – 6 GHz). It’s expected that the RF performance of this platform can meet the datasheet specifications at 2.4 GHz, but not at the entire RF tuning range that the board supports (but it will work much better than the AD-FMCOMMS2-EBZ over the complete RF frequency). We will provide typical performance data for the entire range (70 MHz – 6 GHz) which is supported by the platform. This is primarily for system investigation and bring up of various waveforms from a software team before their custom hardware is complete, where they want to see waveforms, but are not concerned about the last 1dB or 1% EVM of performance.

The AD-FMComms3-EBZ board is very similar to the AD-FMComms2-EBZ board with only one exception, the RX/TX RF differential to single ended transformer. The AD-FMComms3-EBZ is more targetted for wider tuning range applications, that is why we use the TCM1-63AX+ from Mini-Circuits as the RF transformer of choice. We affectionately call the FMCOMMS3-EBZ the “Software Engineers” platform, and the FMCOMMS2-EBZ, the “RF Engineers” platform to denote the difference.

  1. FMCOMMS3 Hardware: This provides a brief description of the AD-FMCOMMS3-EBZ board by itself, and is a good reference for those who want to understand a little more about the board. If you just want to use the board, you can skip this section, and come back to it when you want to incorporate the AD9361 into your product.
    1. Hardware (including schematics)
  2. Use the AD-FMCOMMS3-EBZ Board to better understand the AD9361
    1. Linux Applications
    2. Push custom data into/out of the AD-FMCOMMS3-EBZ
  3. Design with the AD9361
    1. Simulation
    2. Hardware in the Loop / How to design your own custom BaseBand
      1. MATLAB/Simulink Examples
      2. FM Radio/Tuner (listen to FM signals on the HDMI monitor)
    3. Targeting
    4. Complete Workflow
    5. Design a custom AD9361 based platform
      1. HDL Reference Design which you must use in your FPGA.
  4. Additional Documentation about SDR Signal Chains

Warning

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

resources/eval/user-guides/ad-fmcomms3-ebz.txt · Last modified: 04 Nov 2021 16:17 by Robin Getz