This is an old revision of the document!
Analog Devices Kuiper Linux is a distribution based on Raspbian for the Raspberry Pi. It incorporates Linux device drivers for ADI products, and is created with ease of use in mind.
The reasoning behind creating this distribution is to minimize the barriers to integrating ADI hardware devices into a Linux-based system. When starting with a generic Linux distribution, the kernel typically would have to be rebuilt with the desired drivers enabled. While this is not difficult for an engineer that is familiar with the process, it can be a daunting task even when everything goes right.
ADI Kuiper Linux solves this problem, and includes a host of additional applications, software libraries, and utilities including:
While Rasbpian targets Raspberry Pi platform boards, ADI Kuiper Linux supports several other platforms including the Xilinx and Intel FPGAs.
The AD-FMC-SDCARD or AD-FMC-SDCARD is an microSD Card and SD Card adapter (to use the Micro SD Card in an SD Card Slot) comes pre-formatted with an ADI Kuiper Linux image on it. This will usually ship with many evaluation boards.
If you have a preformatted SD Card (one that normally comes with one of the ADI FMC Cards), you can skip down to the Preparing the image section. You still will need to do some manual configuration, since the SD Card supports different base platforms, and different FMC Cards.
You will also need to update the image, since the pre-formatted image will be 6 or more months old, and issues have been fixed since then.
The BOLD is what you should type. It's not too much more than Special Agent Oso's three special steps, and it also allows you to go for that specialty coffee you have been craving.
For different platforms you'll need different images. Currently we provide a single pre-build images, that can work on all the platforms we support.
Now, depending if you are using Linux or Windows, follow these instructions to write the file to your SD card.
The SD card includes a few images on it's BOOT
partition. One of these images needs to be selected before the system will boot properly. In order to run any of these images, just copy the images from the subdirectory into the base directory, and then boot it. For newer versions of the SD card, uImage (Image for ZynqMP) files are in subdirectories for FPGA board generation. Be sure to move the correct uImage (Image for ZynqMP) into the root of the BOOT
partition as well. So the root of 'BOOT' should contain:
If you notice that the file/board you want isn't in your actual SD-Card, that's because you need to upgrade it first. Just pick something with the same base board, boot it, and then run the update scripts, and then copy the right files to the BOOT
partition.
Supported images include:
Directory on the SD image | Carrier | On Carrier Devices | Add on card | doc |
---|---|---|---|---|
socfpga_arria10_socdk_ad9081 | DK-SOC-10AS066S-A | EVAL-ad9081 | ||
socfpga_arria10_socdk_adrv9002 | DK-SOC-10AS066S-A | EVAL-adrv9002 | ||
socfpga_arria10_socdk_adrv9009 | DK-SOC-10AS066S-A | EVAL-ADRV9008-9009 | doc | |
socfpga_arria10_socdk_adrv9371 | DK-SOC-10AS066S-A | EVAL-ADRV9371 | doc | |
socfpga_arria10_socdk_cn0506_mii | DK-SOC-10AS066S-A | |||
socfpga_arria10_socdk_daq2 | DK-SOC-10AS066S-A | AD-FMCDAQ2-EBZ | doc | |
socfpga_arria10_socdk_fmclidar1 | DK-SOC-10AS066S-A | AD-FMCLIDAR1-EBZ | doc | |
socfpga_arria10_socdk_fmcomms8 | DK-SOC-10AS066S-A | EVAL-AD-FMCOMMS8-EBZ | ||
socfpga_cyclone5_de10_nano_cn0540 | Intel Cyclone 5 De10 Nano Kit | CN0540 board | ||
socfpga_cyclone5_sockit_arradio | Intel Cyclone 5 SoC Kit | Arradio board | ||
zynq-adrv9361-z7035-bob | ADRV1CRR-BOB | ADRV9361 | doc | |
zynq-adrv9361-z7035-bob-cmos | ADRV1CRR-BOB | ADRV9361 | doc | |
zynq-adrv9361-z7035-fmc | ADRV1CRR-FMC | ADV7511 | doc | |
zynq-adrv9361-z7035-packrf | ADRV-PACKRF | ADRV9361 | doc | |
zynq-adrv9364-z7020-bob | ADRV1CRR-BOB | ADRV9364 | doc | |
zynq-adrv9364-z7020-bob-cmos | ADRV1CRR-BOB | ADRV9364 | doc | |
zynq-adrv9364-z7020-packrf | PackRF | ADRV9364 | doc | |
zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb | ADRV2CRR-FMC | ADRV9009-ZU11EG | doc | |
zynqmp-zcu102-rev10-ad9172-fmc-ebz-mode4 | ZCU102 | EVAL-AD9172 | ||
zynqmp-zcu102-rev10-ad9361-fmcomms2-3 | ZCU102 | AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ | doc or doc | |
zynqmp-zcu102-rev10-ad9361-fmcomms5 | ZCU102 | AD-FMCOMMS5-EBZ | doc | |
zynqmp-zcu102-rev10-ad9364-fmcomms4 | ZCU102 | AD-FMCOMMS4-EBZ | doc | |
zynqmp-zcu102-rev10-adrv9002 | ZCU102 | ADRV9002NP/W1/PCBZ ADRV9002NP/W2/PCBZ | doc | |
zynqmp-zcu102-rev10-adrv9008-1 | ZCU102 | EVAL-ADRV9008-9009 | doc | |
zynqmp-zcu102-rev10-adrv9008-2 | ZCU102 | EVAL-ADRV9008-9009 | doc | |
zynqmp-zcu102-rev10-adrv9009 | ZCU102 | EVAL-ADRV9008-9009 | doc | |
zynqmp-zcu102-rev10-adrv9371 | ZCU102 | ADRV9371 | doc | |
zynqmp-zcu102-rev10-adrv9375 | ZCU102 | ADRV9375 | doc | |
zynqmp-zcu102-rev10-fmcdaq2 | ZCU102 | AD-FMCDAQ2-EBZ | doc | |
zynqmp-zcu102-rev10-fmcdaq3 | ZCU102 | eval-fmcdaq3-ebz | doc | |
zynqmp-zcu102-rev10-fmclidar1 | ZCU102 | AD-FMCLIDAR1-EBZ | doc | |
zynq-zc702-adv7511 | ZC702 | ADV7511 | ||
zynq-zc702-adv7511-ad9361-fmcomms2-3 | ZC702 | ADV7511 | AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ | doc or doc |
zynq-zc702-adv7511-ad9361-fmcomms5 | ZC702 | ADV7511 | AD-FMCOMMS5-EBZ | doc |
zynq-zc702-adv7511-ad9364-fmcomms4 | ZC702 | ADV7511 | AD-FMCOMMS4-EBZ | doc |
zynq-zc706-adv7511 | ZC706 | ADV7511 | ||
zynq-zc706-adv7511-ad6676-fmc | ZC706 | ADV7511 | EVAL-AD6676 | |
zynq-zc706-adv7511-ad9172-fmc-ebz | ZC706 | ADV7511 | ||
zynq-zc706-adv7511-ad9265-fmc-125ebz | ZC706 | ADV7511 | AD9265-FMC-125EBZ | |
zynq-zc706-adv7511-ad9361-fmcomms2-3 | ZC706 | ADV7511 | AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ | doc or doc |
zynq-zc706-adv7511-ad9361-fmcomms5 | ZC706 | ADV7511 | AD-FMCOMMS5-EBZ | doc |
zynq-zc706-adv7511-ad9361-fmcomms5-ext-lo-adf5355 | ZC706 | ADV7511 | AD-FMCOMMS5-EBZ external LO | doc |
zynq-zc706-adv7511-ad9364-fmcomms4 | ZC706 | ADV7511 | AD-FMCOMMS4-EBZ | doc |
zynq-zc706-adv7511-ad9434-fmc-500ebz | ZC706 | ADV7511 | AD9434-FMC-500EBZ | doc |
zynq-zc706-adv7511-ad9625-fmcadc2 | ZC706 | ADV7511 | AD-FMCADC2-EBZ | doc |
zynq-zc706-adv7511-ad9625-fmcadc3 | ZC706 | ADV7511 | AD-FMCADC3-EBZ | |
zynq-zc706-adv7511-ad9739a-fmc | ZC706 | ADV7511 | EVAL-AD9739A | doc |
zynq-zc706-adv7511-adrv9008-1 | ZC706 | ADV7511 | EVAL-ADRV9008-9009 | doc |
zynq-zc706-adv7511-adrv9008-2 | ZC706 | ADV7511 | EVAL-ADRV9008-9009 | doc |
zynq-zc706-adv7511-adrv9009 | ZC706 | ADV7511 | EVAL-ADRV9008-9009 | doc |
zynq-zc706-adv7511-adrv9371 | ZC706 | ADV7511 | ADRV9371 | doc |
zynq-zc706-adv7511-adrv9375 | ZC706 | ADV7511 | ADRV9375 | doc |
zynq-zc706-adv7511-fmcdaq2 | ZC706 | ADV7511 | AD-FMCDAQ2-EBZ | doc |
zynq-zc706-adv7511-fmcdaq3-revC | ZC706 | ADV7511 | eval-fmcdaq3-ebz | doc |
zynq-zc706-adv7511-fmcjesdadc1 | ZC706 | ADV7511 | AD-FMCJESDADC1-EBZ | |
zynq-zc706-adv7511-fmclidar1 | ZC706 | ADV7511 | AD-FMCLIDAR1-EBZ | doc |
zynq-zc706-adv7511-fmcomms11 | ZC706 | ADV7511 | AD-FMCOMMS11-EBZ | doc |
zynq-zed-adv7511 | Zed Board | ADV7511 | ||
zynq-zed-adv7511-ad9361-fmcomms2-3 | Zed Board | ADV7511 | AD-FMCOMMS2-EBZ or AD-FMCOMMS3-EBZ | doc or doc |
zynq-zed-adv7511-ad9364-fmcomms4 | Zed Board | ADV7511 | AD-FMCOMMS4-EBZ | doc |
zynq-zed-adv7511-ad9467-fmc-250ebz | Zed Board | ADV7511 | AD9467-FMC-250EBZ | |
zynq-zed-adv7511-cn0363 | Zed Board | ADV7511 | EVAL-CN0363-PMDZ | |
zynq-zed-imageon | Zed Board | ADV7511 | FMC-IMAGEON | |
zynq-coraz7s-cn0540 | Cora Z7 Board | CN0540 board | ||
zynq-coraz7s-cn0501 | Cora Z7 Board |
We have heard of some versions of Windows, and some specific SD readers/writers that don't like the FAT parition that we make on the SD Cards - sorry - we have no idea, and have no way to replicate things (that we have found). If it doesn't work for you - try a different windows machine.
the U-Boot terminals below are for, well - U-Boot. If you see a kernel booting, you aren't running in U-Boot. This means reset the board, and when the system says “Hit any key to stop autoboot” - hit any key. If you are unfamiliar with U-Boot, check out the Main Doc.
First you have to use the default environment from the SD card (otherwise the system may not boot):
env default -a saveenv
Then you need to update the MAC address of the board. For some reason, Xilinx doesn't do this on their boards, and you will not get the proper MAC address. Depending on where to do it:
setenv ethaddr XX:XX:XX:XX:XX:XX (whatever is on the sticker on the board saveenv reset
ifconfig eth2 down ifconfig eth2 hw ether XX:XX:XX:XX:XX:XX (what ever is on the sticker on the board) ifconfig eth2 up
These boot messages may change based on your specific platform.
rgetz@brain:~/newest$ kermit -l /dev/ttyACM0 -b 115200 -c Connecting to /dev/ttyACM0, speed 115200 Escape character: Ctrl-\ (ASCII 28, FS): enabled Type the escape character followed by C to get back, or followed by ? to see other options. ---------------------------------------------------- U-Boot SPL 2021.07-16360-gee63370553-dirty (Jun 09 2022 - 23:13:35 +0300) FPGA: Checking FPGA configuration setting ... FPGA: Start to program peripheral/full bitstream ... FPGA: Early Release Succeeded. FPGA: Checking FPGA configuration setting ... FPGA: Start to program peripheral/full bitstream ... FPGA: Early Release Succeeded. U-Boot SPL 2021.07-16360-gee63370553-dirty (Jun 09 2022 - 23:13:35 +0300) DDRCAL: Success FPGA: Checking FPGA configuration setting ... FPGA: Start to program core bitstream ... Full Configuration Succeeded. FPGA: Enter user mode. WDT: Started with servicing (10s timeout) Trying to boot from MMC1 U-Boot 2021.07-16360-gee63370553-dirty (Jun 09 2022 - 23:13:35 +0300)socfpga_arria10, Build: jenkins-master-quartus_boot_on_ubuntu_master-97 CPU: Altera SoCFPGA Arria 10 BOOT: SD/MMC External Transceiver (1.8V) Model: Altera SOCFPGA Arria 10 DRAM: 1 GiB WDT: Started with servicing (10s timeout) MMC: dwmmc0@ff808000: 0 Loading Environment from MMC... OK In: serial Out: serial Err: serial Model: Altera SOCFPGA Arria 10 Net: eth0: ethernet@ff800000 Hit any key to stop autoboot: 0 150 bytes read in 4 ms (36.1 KiB/s) ## Executing script at 02100000 Failed to load 'soc_system.rbf' Full Configuration Succeeded. FPGA: Enter user mode. 15038392 bytes read in 730 ms (19.6 MiB/s) fpga - loadable FPGA image support Usage: fpga [operation type] [device number] [image address] [image size] fpga operations: dump [dev] [address] [size] Load device to memory buffer info [dev] list known device information load [dev] [address] [size] Load device from memory buffer loadb [dev] [address] [size] Load device from bitstream buffer (Xilinx only) loadmk [dev] [address] Load device generated with mkimage For loadmk operating on FIT format uImage address must include subimage unit name in the form of addr:<subimg_uname> switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... Found /extlinux/extlinux.conf Retrieving file: /extlinux/extlinux.conf 162 bytes read in 5 ms (31.3 KiB/s) 1: Linux Default Retrieving file: /extlinux/../zImage 8289256 bytes read in 408 ms (19.4 MiB/s) append: root=/dev/mmcblk0p2 rw rootwait earlyprintk console=ttyS0,115200n8 Retrieving file: /extlinux/../socfpga_arria10_socdk_sdmmc.dtb 30586 bytes read in 9 ms (3.2 MiB/s) Kernel image @ 0x1000000 [ 0x000000 - 0x7e7be8 ] ## Flattened Device Tree blob at 02000000 Booting using the fdt blob at 0x2000000 Loading Device Tree to 09ff5000, end 09fff779 ... OK Starting kernel ... Deasserting all peripheral resets [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.10.0-98183-gf814ae972859-dirty (liviu@LADACE-Debian) (arm-none-linux-gnueabihf-gcc (GNU Toolchain for the A-profile Architecture 10.2-2020.11 (arm-10.16)) 10.2.1 20201103, GNU ld (GNU Toolchain for the A-profile Architecture 10.2-2020.11 (arm-10.16)) 2.35.1.20201028) #27 SMP Wed May 25 16:01:50 EEST 2022
Complete Boot Log (Click to expand)
Complete Boot Log (Click to expand)
[ 0.000000] CPU: ARMv7 Processor [414fc091] revision 1 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: Altera SOCFPGA Arria 10 [ 0.000000] printk: bootconsole [earlycon0] enabled [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] cma: Reserved 128 MiB at 0x38000000 [ 0.000000] Zone ranges: [ 0.000000] Normal [mem 0x0000000000000000-0x000000002fffffff] [ 0.000000] HighMem [mem 0x0000000030000000-0x000000003fffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000000000000-0x000000003fffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000003fffffff] [ 0.000000] percpu: Embedded 19 pages/cpu s45324 r8192 d24308 u77824 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260608 [ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rw rootwait earlyprintk console=ttyS0,115200n8 [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 884076K/1048576K available (13312K kernel code, 1284K rwdata, 7440K rodata, 1024K init, 348K bss, 33428K reserved, 131072K cma-reserved, 131072K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] ftrace: allocating 42085 entries in 83 pages [ 0.000000] ftrace: allocated 83 pages with 4 groups [ 0.000000] rcu: Hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] Rude variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] L2C-310 erratum 769419 enabled [ 0.000000] L2C-310 enabling early BRESP for Cortex-A9 [ 0.000000] L2C-310: enabling full line of zeros but not enabled in Cortex-A9 [ 0.000000] L2C-310 ID prefetch enabled, offset 1 lines [ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled [ 0.000000] L2C-310 cache controller enabled, 8 ways, 512 kB [ 0.000000] L2C-310: CACHE_ID 0x410030c9, AUX_CTRL 0x76560001 [ 0.000000] random: get_random_bytes called from start_kernel+0x39c/0x558 with crng_init=0 [ 0.000000] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns [ 0.000005] sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns [ 0.007886] Switching to timer-based delay loop, resolution 10ns [ 0.014168] Console: colour dummy device 80x30 [ 0.018614] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=1000000) [ 0.029098] pid_max: default: 32768 minimum: 301 [ 0.033798] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.041076] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.049358] CPU: Testing write buffer coherency: ok [ 0.054259] CPU0: Spectre v2: using BPIALL workaround [ 0.059451] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.065541] Setting up static identity map for 0x100000 - 0x100060 [ 0.071799] rcu: Hierarchical SRCU implementation. [ 0.076836] smp: Bringing up secondary CPUs ... [ 0.081933] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.081940] CPU1: Spectre v2: using BPIALL workaround [ 0.092713] smp: Brought up 1 node, 2 CPUs [ 0.096792] SMP: Total of 2 processors activated (400.00 BogoMIPS). [ 0.103043] CPU: All CPU(s) started in SVC mode. [ 0.108126] devtmpfs: initialized [ 0.115824] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 [ 0.123762] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.133573] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.144486] NET: Registered protocol family 16 [ 0.150612] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.158377] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. [ 0.166360] hw-breakpoint: maximum watchpoint size is 4 bytes. [ 0.178562] OF: /soc/gpio@ffc02a00/gpio-controller@0: could not get #gpio-cells for /soc/clkmgr@ffd04000/clocks/l4_sp_clk [ 0.191504] OF: /soc/gpio@ffc02a00/gpio-controller@0: could not get #gpio-cells for /soc/clkmgr@ffd04000/clocks/l4_sp_clk [ 0.212418] vgaarb: loaded [ 0.215392] SCSI subsystem initialized [ 0.219290] usbcore: registered new interface driver usbfs [ 0.224797] usbcore: registered new interface driver hub [ 0.230122] usbcore: registered new device driver usb [ 0.235284] usb_phy_generic soc:usbphy: supply vcc not found, using dummy regulator [ 0.245476] mc: Linux media interface: v0.10 [ 0.249753] videodev: Linux video capture interface: v2.00 [ 0.255312] pps_core: LinuxPPS API ver. 1 registered [ 0.260254] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.269376] PTP clock support registered [ 0.273547] jesd204: found 0 devices and 0 topologies [ 0.278599] FPGA manager framework [ 0.282059] Advanced Linux Sound Architecture Driver Initialized. [ 0.289059] clocksource: Switched to clocksource timer1 [ 0.814051] NET: Registered protocol family 2 [ 0.818906] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) [ 0.827312] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) [ 0.835085] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.842298] TCP: Hash tables configured (established 8192 bind 8192) [ 0.848723] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.855377] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 0.862577] NET: Registered protocol family 1 [ 0.867321] RPC: Registered named UNIX socket transport module. [ 0.873246] RPC: Registered udp transport module. [ 0.877928] RPC: Registered tcp transport module. [ 0.882620] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.889045] PCI: CLS 0 bytes, default 64 [ 0.894135] workingset: timestamp_bits=30 max_order=18 bucket_order=0 [ 0.905441] NFS: Registering the id_resolver key type [ 0.910533] Key type id_resolver registered [ 0.914697] Key type id_legacy registered [ 0.918694] Installing knfsd (copyright (C) 1996 okir@monad.swb.de). [ 0.925534] ntfs: driver 2.1.32 [Flags: R/W]. [ 0.930026] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 0.936524] fuse: init (API version 7.32) [ 0.940868] bounce: pool size: 64 pages [ 0.944693] io scheduler mq-deadline registered [ 0.949230] io scheduler kyber registered [ 0.957511] dma-pl330 ffda1000.pdma: Loaded driver for PL330 DMAC-341330 [ 0.964223] dma-pl330 ffda1000.pdma: DBUFF-512x8bytes Num_Chans-8 Num_Peri-32 Num_Events-8 [ 0.974943] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled [ 0.982120] printk: console [ttyS0] disabled [ 0.986427] ffc02100.serial1: ttyS0 at MMIO 0xffc02100 (irq = 45, base_baud = 6250000) is a 16550A [ 0.995416] printk: console [ttyS0] enabled [ 0.995416] printk: console [ttyS0] enabled [ 1.003753] printk: bootconsole [earlycon0] disabled [ 1.003753] printk: bootconsole [earlycon0] disabled [ 1.015314] brd: module loaded [ 1.018644] at24 0-0051: supply vcc not found, using dummy regulator [ 1.026304] at24 0-0051: 4096 byte 24c32 EEPROM, writable, 32 bytes/write [ 1.034084] spi_altera ff200040.spi: regoff 0, irq 48 [ 1.040511] altr_a10sr_gpio altr_a10sr_gpio.0.auto: DMA mask not set [ 1.047986] libphy: Fixed MDIO Bus: probed [ 1.052567] CAN device driver interface [ 1.056629] socfpga-dwmac ff800000.ethernet: IRQ eth_wake_irq not found [ 1.063246] socfpga-dwmac ff800000.ethernet: IRQ eth_lpi not found [ 1.069526] socfpga-dwmac ff800000.ethernet: No sysmgr-syscon node found [ 1.076198] socfpga-dwmac ff800000.ethernet: Unable to parse OF data [ 1.082581] socfpga-dwmac: probe of ff800000.ethernet failed with error -524 [ 1.089769] stmmaceth ff800000.ethernet: IRQ eth_wake_irq not found [ 1.096011] stmmaceth ff800000.ethernet: IRQ eth_lpi not found [ 1.102086] stmmaceth ff800000.ethernet: User ID: 0x10, Synopsys ID: 0x37 [ 1.108850] stmmaceth ff800000.ethernet: DWMAC1000 [ 1.113722] stmmaceth ff800000.ethernet: DMA HW capability register supported [ 1.120841] stmmaceth ff800000.ethernet: RX Checksum Offload Engine supported [ 1.127943] stmmaceth ff800000.ethernet: COE Type 2 [ 1.132807] stmmaceth ff800000.ethernet: TX Checksum insertion supported [ 1.139484] stmmaceth ff800000.ethernet: Enhanced/Alternate descriptors [ 1.146068] stmmaceth ff800000.ethernet: Enabled extended descriptors [ 1.152490] stmmaceth ff800000.ethernet: Ring mode enabled [ 1.157950] stmmaceth ff800000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 1.173670] libphy: stmmac: probed [ 1.177073] Micrel KSZ9031 Gigabit PHY stmmac-0:07: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=stmmac-0:07, irq=POLL) [ 1.190760] usbcore: registered new interface driver asix [ 1.196178] usbcore: registered new interface driver ax88179_178a [ 1.202304] usbcore: registered new interface driver cdc_ether [ 1.208130] usbcore: registered new interface driver net1080 [ 1.213804] usbcore: registered new interface driver cdc_subset [ 1.219725] usbcore: registered new interface driver zaurus [ 1.225310] usbcore: registered new interface driver cdc_ncm [ 1.231429] dwc2 ffb00000.usb: supply vusb_d not found, using dummy regulator [ 1.238653] dwc2 ffb00000.usb: supply vusb_a not found, using dummy regulator [ 1.246013] dwc2 ffb00000.usb: EPs: 16, dedicated fifos, 8064 entries in SPRAM [ 1.253648] dwc2 ffb00000.usb: DWC OTG Controller [ 1.258354] dwc2 ffb00000.usb: new USB bus registered, assigned bus number 1 [ 1.265430] dwc2 ffb00000.usb: irq 46, io mem 0xffb00000 [ 1.270874] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 1.279113] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 1.286304] usb usb1: Product: DWC OTG Controller [ 1.290994] usb usb1: Manufacturer: Linux 5.10.0-98183-gf814ae972859-dirty dwc2_hsotg [ 1.298787] usb usb1: SerialNumber: ffb00000.usb [ 1.303852] hub 1-0:1.0: USB hub found [ 1.307616] hub 1-0:1.0: 1 port detected [ 1.312338] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.318839] ehci-pci: EHCI PCI platform driver [ 1.323776] usbcore: registered new interface driver uas [ 1.329160] usbcore: registered new interface driver usb-storage [ 1.335214] usbcore: registered new interface driver usbserial_generic [ 1.341746] usbserial: USB Serial support registered for generic [ 1.347745] usbcore: registered new interface driver ftdi_sio [ 1.353494] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.360844] usbcore: registered new interface driver upd78f0730 [ 1.366749] usbserial: USB Serial support registered for upd78f0730 [ 1.376546] rtc-ds1307 0-0068: SET TIME! [ 1.384754] rtc-ds1307 0-0068: registered as rtc0 [ 1.389543] i2c /dev entries driver [ 1.393645] usbcore: registered new interface driver uvcvideo [ 1.399381] USB Video Class driver (1.1.1) [ 1.407645] ltc2978: probe of 0-005c failed with error -121 [ 1.413942] Synopsys Designware Multimedia Card Interface Driver [ 1.420180] dw_mmc ff808000.dwmmc0: IDMAC supports 32-bit address mode. [ 1.426844] dw_mmc ff808000.dwmmc0: Using internal DMA controller. [ 1.433036] dw_mmc ff808000.dwmmc0: Version ID is 270a [ 1.438197] dw_mmc ff808000.dwmmc0: DW MMC controller at irq 41,32 bit host data width,1024 deep fifo [ 1.447540] mmc_host mmc0: card is polling. [ 1.453462] ledtrig-cpu: registered to indicate activity on CPUs [ 1.459576] usbcore: registered new interface driver usbhid [ 1.464345] mmc_host mmc0: Bus speed (slot 0) = 50000000Hz (slot req 400000Hz, actual 396825HZ div = 63) [ 1.465125] usbhid: USB HID core driver [ 1.490963] fpga_manager fpga0: SoCFPGA Arria10 FPGA Manager registered [ 1.498177] usbcore: registered new interface driver snd-usb-audio [ 1.506251] NET: Registered protocol family 10 [ 1.511420] Segment Routing with IPv6 [ 1.515131] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.521517] NET: Registered protocol family 17 [ 1.525961] NET: Registered protocol family 15 [ 1.530557] can: controller area network core [ 1.534941] NET: Registered protocol family 29 [ 1.539395] can: raw protocol [ 1.542352] can: broadcast manager protocol [ 1.546521] can: netlink gateway - max_hops=1 [ 1.551013] 8021q: 802.1Q VLAN Support v1.8 [ 1.552310] mmc_host mmc0: Bus speed (slot 0) = 50000000Hz (slot req 50000000Hz, actual 50000000HZ div = 0) [ 1.555215] NET: Registered protocol family 36 [ 1.564943] mmc0: new high speed SDHC card at address aaaa [ 1.569338] Key type dns_resolver registered [ 1.575303] mmcblk0: mmc0:aaaa SC32G 29.7 GiB [ 1.579361] oprofile: no performance counters [ 1.587935] oprofile: using timer interrupt. [ 1.592299] ThumbEE CPU extension supported. [ 1.592852] mmcblk0: p1 p2 p3 [ 1.596566] Registering SWP/SWPB emulation handler [ 1.628855] adrv9002 spi0.0: adrv9002_setup, 2804: failed with "Failed to reset device and set SPI Config" (3) [ 1.639954] adrv9002 spi0.0: adrv9002_setup, 2804: failed with "Failed to reset device and set SPI Config" (3) [ 1.651046] adrv9002 spi0.0: adrv9002_init, 4197: failed with "Failed to reset device and set SPI Config" (3) [ 1.660988] cf_axi_adc: probe of ff220000.axi-adrv9002-rx1-lpc failed with error -14 [ 1.671202] of_cfs_init [ 1.673672] of_cfs_init: OK [ 1.676654] ALSA device list: [ 1.679631] No soundcards found. [ 1.683233] dw-apb-uart ffc02100.serial1: forbid DMA for kernel console [ 1.707544] random: fast init done [ 1.942481] EXT4-fs (mmcblk0p2): recovery complete [ 1.948189] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 1.956309] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 1.965770] devtmpfs: mounted [ 1.971587] Freeing unused kernel memory: 1024K [ 1.976516] Run /sbin/init as init process [ 2.495793] systemd[1]: System time before build time, advancing clock. [ 2.546077] systemd[1]: systemd 247.3-7+rpi1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified) [ 2.569272] systemd[1]: Detected architecture arm. Welcome to Kuiper GNU/Linux 11.2 (bullseye)! [ 2.622132] systemd[1]: Set hostname to <analog>. [ 4.137436] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is deprecated and will eventually be removed. [ 4.378487] systemd[1]: Queued start job for default target Graphical Interface. [ 4.387531] random: systemd: uninitialized urandom read (16 bytes read) [ 4.394498] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 4.406868] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 4.416537] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 4.449268] random: systemd: uninitialized urandom read (16 bytes read) [ 4.456609] systemd[1]: Created slice system-modprobe.slice. [ OK ] Created slice system-modprobe.slice. [ 4.489256] random: systemd: uninitialized urandom read (16 bytes read) [ 4.496572] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 4.529917] systemd[1]: Created slice system-systemd\x2dfsck.slice. [ OK ] Created slice system-systemd\x2dfsck.slice. [ 4.559661] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 4.589562] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 4.619502] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped. [ 4.631946] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 4.659334] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 4.690278] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 4.719816] systemd[1]: Listening on fsck to fsckd communication Socket. [ OK ] Listening on fsck to fsckd communication Socket. [ 4.749507] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 4.802106] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 4.810944] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 4.839975] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 4.879147] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 4.909763] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 4.939873] systemd[1]: Condition check resulted in Huge Pages File System being skipped. [ 4.948438] systemd[1]: Condition check resulted in POSIX Message Queue File System being skipped. [ 4.960413] systemd[1]: Mounting RPC Pipe File System... Mounting RPC Pipe File System... [ 4.992209] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 5.022090] systemd[1]: Mounting Kernel Trace File System... Mounting Kernel Trace File System... [ 5.049485] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped. [ 5.065551] systemd[1]: Starting Restore / save the current clock... Starting Restore / save the current clock... [ 5.102840] systemd[1]: Starting Set the console keyboard layout... Starting Set the console keyboard layout... [ 5.140096] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped. [ 5.155786] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 5.192594] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 5.212630] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 5.254201] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped. [ 5.263665] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 5.276012] systemd[1]: Starting Journal Service... Starting Journal Service... [ 5.296804] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 5.342287] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 5.382711] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 5.426047] systemd[1]: Mounted RPC Pipe File System. [ OK ] Mounted RPC Pipe File System. [ 5.472608] systemd[1]: Mounted Kernel Debug File System. [ OK ] Mounted Kernel Debug File System. [ 5.488602] systemd[1]: Mounted Kernel Trace File System. [ OK ] Mounted Kernel Trace File System. [ 5.520488] systemd[1]: Finished Restore / save the current clock. [ OK ] Finished Restore / save the current clock. [ 5.596975] systemd[1]: modprobe@configfs.service: Succeeded. [ 5.611072] systemd[1]: Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module configfs. [ 5.629523] systemd[1]: Started Journal Service. [ 5.645346] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ OK ] Started Journal Service. [ OK ] Finished Set the console keyboard layout. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ OK ] Finished Remount Root and Kernel File Systems. Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... Starting Load/Save Random Seed... Starting Apply Kernel Variables... [ 6.015539] systemd-journald[98]: Received client request to flush runtime journal. Starting Create System Users... [ 6.056206] systemd-journald[98]: File /var/log/journal/1064eace00dd4e3daeb15d4eed400196/system.journal corrupted or uncleanly shut down, renaming and replacing. [ OK ] Mounted FUSE Control File System. [ OK ] Finished Coldplug All udev Devices. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create System Users. Starting Helper to synchronize boot up for ifupdown... Starting Create Static Device Nodes in /dev... Starting Wait for udev To …plete Device Initialization... [ OK ] Finished Helper to synchronize boot up for ifupdown. [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Starting Rule-based Manage…for Device Events and Files... [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Started Rule-based Manager for Device Events and Files. Starting Show Plymouth Boot Screen... [ OK ] Started Show Plymouth Boot Screen. [ OK ] Started Forward Password R…s to Plymouth Directory Watch. [ OK ] Reached target Local Encrypted Volumes. [ OK ] Finished Load/Save Random Seed. [ OK ] Reached target Hardware activated USB gadget. Starting Load Kernel Modules... [ OK ] Found device /dev/ttyS0. [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ OK ] Found device /dev/disk/by-partuuid/0b25bea5-01. Starting File System Check…isk/by-partuuid/0b25bea5-01... [ OK ] Started File System Check Daemon to report status. [ OK ] Finished Wait for udev To Complete Device Initialization. [ OK ] Finished File System Check…/disk/by-partuuid/0b25bea5-01. Mounting /boot... [ OK ] Mounted /boot. [ OK ] Reached target Local File Systems. Starting Set console font and keymap... Starting Raise network interfaces... Starting Preprocess NFS configuration... Starting Tell Plymouth To Write Out Runtime Data... Starting Create Volatile Files and Directories... [ OK ] Finished Set console font and keymap. [ OK ] Finished Tell Plymouth To Write Out Runtime Data. [ OK ] Finished Preprocess NFS configuration. [ OK ] Reached target NFS client services. [ OK ] Reached target Remote File Systems (Pre). [ OK ] Reached target Remote File Systems. [ OK ] Finished Create Volatile Files and Directories. Starting Update UTMP about System Boot/Shutdown... [ OK ] Finished Update UTMP about System Boot/Shutdown. [ OK ] Reached target System Initialization. [ OK ] Started CUPS Scheduler. [ OK ] Started Daily apt download activities. [ OK ] Started Daily apt upgrade and clean activities. [ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems. [ OK ] Started Discard unused blocks once a week. [ OK ] Started Daily rotation of log files. [ OK ] Started Daily man-db regeneration. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Paths. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on CUPS Scheduler. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on Erlang Port Mapper Daemon Activation Socket. [ OK ] Listening on GPS (Global P…ioning System) Daemon Sockets. [ OK ] Listening on triggerhappy.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Regular background program processing daemon. [ OK ] Started D-Bus System Message Bus. Starting dphys-swapfile - …unt, and delete a swap file... Starting Remove Stale Onli…t4 Metadata Check Snapshots... Starting Creating IIOD Context Attributes...... Starting Authorization Manager... Starting DHCP Client Daemon... Starting LSB: Switch to on…nless shift key is pressed)... Starting LSB: rng-tools (Debian variant)... Starting Check for Raspberry Pi EEPROM updates... Starting System Logging Service... Starting User Login Management... Starting triggerhappy global hotkey daemon... Starting Disk Manager... Starting WPA supplicant... [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Finished Check for Raspberry Pi EEPROM updates. [ OK ] Started triggerhappy global hotkey daemon. [ OK ] Started System Logging Service. [ OK ] Started Authorization Manager. [ OK ] Started DHCP Client Daemon. Starting Modem Manager... [ OK ] Started WPA supplicant. [FAILED] Failed to start dphys-swap…mount, and delete a swap file. See 'systemctl status dphys-swapfile.service' for details. [ OK ] Finished Raise network interfaces. [ OK ] Reached target Network. [ OK ] Reached target Network is Online. Starting CUPS Scheduler... [ OK ] Started Erlang Port Mapper Daemon. Starting Load USB gadget scheme... Starting HTTP based time synchronization tool... Starting Internet superserver... Starting /etc/rc.local Compatibility... Starting OpenBSD Secure Shell server... Starting Permit User Sessions... [ OK ] Started LSB: Switch to ond…(unless shift key is pressed). [ OK ] Started LSB: rng-tools (Debian variant). [ OK ] Found device /dev/ttyGS0. [ OK ] Finished Load USB gadget scheme. [ OK ] Started /etc/rc.local Compatibility. Mounting Mount FunctionFS instance... [ OK ] Started Internet superserver. [ OK ] Mounted Mount FunctionFS instance. [ OK ] Finished Permit User Sessions. Starting Light Display Manager... Starting Hold until boot process finishes up... [ OK ] Started HTTP based time synchronization tool. [ OK ] Started User Login Management. [ OK ] Started Unattended Upgrades Shutdown. [ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots. [FAILED] Failed to start VNC Server for X11. Raspbian GNU/Linux 11 analog ttyS0 analog login: root (automatic login) Password: Linux analog 5.10.0-98183-gf814ae972859-dirty #27 SMP Wed May 25 16:01:50 EEST 2022 armv7l The programs included with the Debian GNU/Linux system are free software; the exact distribution terms for each program are described in the individual files in /usr/share/doc/*/copyright. Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent permitted by applicable law. Last login: Fri Jun 17 14:45:22 BST 2022 on ttyS0 root@analog:~#
Even thought this is Linux, this is a persistent file systems. You have to take care not to corrupt the file system -- please shut down things, don't just turn off the power switch. Depending on your monitor, the standard power off could be hiding. You can do this from the terminal as well with:
sudo shutdown -h now
or
sudo poweroff
The default user is the “analog” user, the password for this user is “analog”. The password for the “root” account is “analog” as well.
User | Password |
---|---|
root | analog |
analog | analog |
There are 2 things to update:
Upgrading one side, without upgrading the other might cause more problems than it solves. If you are upgrading, please upgrade both.
Staying up to date is a combination of:
If you need to use a proxy for any of these:
There are a number of ADI provided tools in the file system. There is an easy way to rebuild these projects from source. The only requirement is an healthy image and active Internet connection.
In order to update all ADI tools - simply call the update script as shown below: In case you only want to update a certain project, the script accepts a single parameter, the ADI github project name. (https://github.com/analogdevicesinc)
If you are using an old image & old update tools script - you may need to run the update tools script twice (the first time it updates the update script, and the second time it updates everything else). This has been resolved in the most recent update script (the script updates itself, and switches over to the new one), so you only need to do this if you are using an older version.
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:~# sudo adi_update_tools.sh * Cloning fmcomms1-eeprom-cal * Cloning into 'fmcomms1-eeprom-cal'... remote: Counting objects: 19, done. remote: Compressing objects: 100% (15/15), done. remote: Total 19 (delta 6), reused 12 (delta 3) Unpacking objects: 100% (19/19), done. * Building fmcomms1-eeprom-cal * cc -Wall -Wextra -pedantic -std=gnu99 -c -o main.o main.c cc -Wall -Wextra -pedantic -std=gnu99 -o xcomm_cal main.o -lm install -d /usr/local/bin install ./xcomm_cal /usr/local/bin/ Building fmcomms1-eeprom-cal finished Successfully * Cloning iio-cmdsrv * Cloning into 'iio-cmdsrv'... remote: Counting objects: 199, done. remote: Compressing objects: 100% (124/124), done. remote: Total 199 (delta 73), reused 199 (delta 73) Receiving objects: 100% (199/199), 44.46 KiB | 80 KiB/s, done. Resolving deltas: 100% (73/73), done. * Building iio-cmdsrv * cc -Wall -Wextra -pedantic -std=gnu99 -s -c -o iio_cmdsrv.o iio_cmdsrv.c cc -Wall -Wextra -pedantic -std=gnu99 -s -o iio_cmdsrv iio_cmdsrv.o -lm install -d /usr/local/bin install ./iio_cmdsrv /usr/local/bin/ install ./scripts/* /usr/local/bin/ Building iio-cmdsrv finished Successfully * Cloning iio-oscilloscope * Cloning into 'iio-oscilloscope'... [-snip-]
The default ADI ZYNQ image supports a variety of ZYNQ boards and reference designs. In order to keep those boot files up to date. There is a another script that downloads the latest builds from the ADI Wiki page and installs them onto the FAT32 partition on the SD Card. The only requirement is a healthy image and active Internet connection.
In order to update all ADI tools, simply call the adi_update_boot.sh script as shown below:
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:~# sudo adi_update_boot.sh --2013-12-11 14:22:46-- http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/latest_zynq_boot.txt Resolving wiki.analog.com (wiki.analog.com)... 195.170.124.184 Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected. HTTP request sent, awaiting response... 200 OK Length: 153 [text/plain] Saving to: `latest_zynq_boot.txt' 100%[======================================>] 153 --.-K/s in 0s 2013-12-11 14:24:13 (3.96 MB/s) - `latest_zynq_boot.txt' saved [153/153] sed: can't read /media/boot/VERSION: No such file or directory CURRENT VERSION: NEW VERSION : build-2013-12-10 --2013-12-11 14:24:13-- http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/zynq_boot_build-2013-12-10.tgz Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected. HTTP request sent, awaiting response... 200 OK Length: 28330816 (27M) [application/x-gzip] Saving to: `zynq_boot_build-2013-12-10.tgz' 100%[======================================>] 28,330,816 9.64M/s in 2.8s 2013-12-11 14:24:16 (9.64 MB/s) - `zynq_boot_build-2013-12-10.tgz' saved [28330816/28330816] CURRENT BOARD CONFIG: /media/boot/zynq-zed-adv7511-xcomm Extracting - Be patient! ..............DONE root@linaro-ubuntu-desktop:~#
It may happen that you have to copy manually the boot files to complete the update.
To do so, plug the SD card into your computer, and:
(Replace ${CONFIG} with the config name that applies in your case, e.g. “zynq-zed-adv7511-ad9361” for a FMCOMMS2/3 on a ZedBoard.)
The device tree is a data structure for describing hardware. Rather than hard coding every detail of a device into an operating system, many aspect of the hardware can be described in a data structure that is passed to the operating system at boot time.
For your convenience – all device tree files (dtb) for our designs are included in the SD Card boot partition. Sometimes it's desired to change certain device tree properties permanently.
For example a custom board has a different reference clock.
This specifies any shell prompt running on the target
analog@analog:~$ cd /media/analog/BOOT/ analog@analog:/media/analog/BOOT$ dtc -I dtb devicetree.dtb -O dts -o devicetree.dts analog@analog:/media/analog/BOOT$ mousepad devicetree.dts & analog@analog:/media/analog/BOOT$ dtc -I dts devicetree.dts -O dtb -o devicetree.dtb analog@analog:/media/analog/BOOT$
On the embedded Linux target there is Samba_(software) service running. Allowing you to access (Add/map Network Location/Drive) everything under /media on the target.
The only thing you need to do is:
ifconfig
By default, only read access is possible. If you want to be able to copy files onto the image over the network share, the permissions need to be changed first. This can be done by running the following command on the board:
Modify network share permissions
sudo chmod 777 /media/*
Be aware that with this change anybody on your network will now be able to write to the image.
Use rsync, or ssh, or scp, or just plug in the SD card to your Linux machine, and mount the ext4 file system. If you really need help - ask.
On first boot, there are a few things that should be configured first. Click the ADI triangle start menu, Preferences, Raspberry Pi Configuration. Enter the root password when prompted, this will bring up a configuration menu. Under Localisation, set the Locale, Timezone, Keyboard, and WiFi Country appropriately (Not doing this may result in connection failures.)
Reboot the system after this step for changes to take effect, before doing anything else. (It's a bit disconcerting when you see see strange symbols show up as you edit a configuration file because the keyboard language is set incorrectly…)
The system will likely need to be configured according to what devices are connected to the platform board (for example, an AD7124-8 ADC connected to a Raspberry Pi) The most straightforward way to do this for Raspberry Pi is to edit the config.txt file, which is located in the boot partition. This is a FAT partition that is accessible in Linux, Windows, or MacOS. Any text editor can be used, including the Mousepad editor that is included with Kuiper Linux. Using the Raspberry Pi itself also avoids problems with USB encryption, often present on company computers. Connect a keyboard, mouse, and monitor to the Raspberry Pi and connect power. The ADI Kuiper Linux desktop should appear.
Before editing, it is a good idea to make a backup of the original file, just in case something goes wrong (which it won't, but still…) Open a terminal and enter the following command (noting that “analog@analog:~ $” is the prompt, and does not need to be typed):
analog@analog:~ $ sudo cp /boot/config.txt /boot/config.backup analog@analog:~ $ sudo mousepad /boot/config.txt
This will bring up the text editor. At this point, the appropriate device tree overlays can be included, for example, add the following line to enable the ADXL345 3-axis SPI accelerometer, noting that the lirc-rpi lines are shown for reference, and any line beginning with “#” is ignored:
# Uncomment this to enable the lirc-rpi module #dtoverlay=lirc-rpi dtoverlay=rpi-adxl345
This usually represents a default overlay, with SPI port and interrupt mapping defined in the kernel source. A number of other overlays are included with Kuiper Linux, for individual devices and various reference designs. Alternative configurations can be created by cloning and editing the appropriate dts file.
After editing config.txt, reboot for changes to take effect.
If any IIO devices are attached and were enabled in config.txt, run iio_info to verify that the drivers loaded properly. Example:
analog@analog:~ $ iio_info Library version: 0.21 (git tag: 1c0781b) Compiled with backends: local xml ip IIO context created with local backend. Backend version: 0.21 (git tag: 1c0781b) Backend description string: Linux analog 4.19.86-v7l+ #3 SMP Tue Sep 1 19:43:06 UTC 2020 armv7l IIO context has 2 attributes: local,kernel: 4.19.86-v7l+ uri: local: IIO context has 5 devices: iio:device0: ad7127-8 (buffer capable) 8 channels found: voltage0-voltage1: (input, index: 0, format: be:u24/32>>0) 6 channel-specific attributes found: attr 0: filter_low_pass_3db_frequency value: 3 attr 1: offset value: 0 ... ...
The Linaro based GNU/Linux image found/distributed here is a modular operating system consisting of hundreds of software components. Most (but not all) of the components are open source packages, developed independently, and accompanied by separate license terms (such as GPLv2, GPLv3, LGPL, BSD, modified BSD or others). Your license rights with respect to individual components accompanied by separate license terms are defined by those terms (The license agreement for each component is generally located in the component's source code); nothing (including obtaining these components as part of an aggregate) shall restrict, limit, or otherwise affect any rights or obligations you may have, or conditions to which you may be subject, under such license terms.
The license terms of components found in the Linaro image normally (but not always) permit you to copy, modify, and redistribute the component, and may include obligations - including distributing the changes to the source.
If you include this software components from this image in your product, it is up to you and your legal team to make sure your product complies with the licensing requirements of whatever software package that you include.
You may make and use unlimited copies of the Software for your distribution and use within your organization. You may make and distribute unlimited copies of the Software outside your organization.