This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcomms3-ebz [26 Mar 2020 00:31] – Update MATLAB Links Travis Collins | resources:eval:user-guides:ad-fmcomms3-ebz [04 Nov 2021 16:17] (current) – fix link Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCOMMS3-EBZ User Guide ====== | ====== AD-FMCOMMS3-EBZ User Guide ====== | ||
- | The AD-FMComms3-EBZ is an FMC board for the [[adi> | + | The AD-FMComms3-EBZ is an FMC board for the [[adi> |
The purpose of the AD-FMComms3-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform which operates over a much wider tuning range (70 MHz – 6 GHz). It’s expected that the RF performance of this platform can meet the datasheet specifications at 2.4 GHz, but not at the entire RF tuning range that the board supports (but it will work **much** better than the [[AD-FMCOMMS2-EBZ]] over the complete RF frequency). We will provide typical performance data for the entire range (70 MHz – 6 GHz) which is supported by the platform. This is primarily for system investigation and bring up of various waveforms from a software team before their custom hardware is complete, where they want to see waveforms, but are not concerned about the last 1dB or 1% EVM of performance. | The purpose of the AD-FMComms3-EBZ is to provide an RF platform to software developers, system architects, etc, who want a single platform which operates over a much wider tuning range (70 MHz – 6 GHz). It’s expected that the RF performance of this platform can meet the datasheet specifications at 2.4 GHz, but not at the entire RF tuning range that the board supports (but it will work **much** better than the [[AD-FMCOMMS2-EBZ]] over the complete RF frequency). We will provide typical performance data for the entire range (70 MHz – 6 GHz) which is supported by the platform. This is primarily for system investigation and bring up of various waveforms from a software team before their custom hardware is complete, where they want to see waveforms, but are not concerned about the last 1dB or 1% EVM of performance. |