This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD-FMCOMMS2-EBZ on:
Download the pre-build image for you device in question.
Latest Build: 2022_08_05 - 2021_R1
Linux branch: 2021_R1
Linux repository: https://github.com/analogdevicesinc/linux.git
HDL branch: hdl_2021_r1
HDL repository: https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | 2021_r1_kc705_ad9467_fmc.zip |
KC705 | FMCOMMS2-3 | 2021_r1_kc705_fmcomms2-3.zip |
KCU105 | ADRV9371X | 2021_r1_kcu105_adrv9371x.zip |
KCU105 | FMCDAQ2 | 2021_r1_kcu105_fmcdaq2.zip |
KCU105 | FMCOMMS2-3 | 2021_r1_kcu105_fmcomms2-3.zip |
VC707 | AD6676EVB | 2021_r1_vc707_ad6676evb.zip |
VC707 | FMCADC5 | 2021_r1_vc707_fmcadc5.zip |
VC707 | FMCOMMS2-3 | 2021_r1_vc707_fmcomms2-3.zip |
VC707 | FMCOMMS4 | 2021_r1_vc707_fmcomms4.zip |
Latest Build: 2021_07_27 - 2019_R2
Linux branch: 2019_R2
Linux repository: https://github.com/analogdevicesinc/linux.git
HDL branch: hdl_2019_r2
HDL repository: https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | 2019_r2_kc705_ad9467_fmc.zip |
KC705 | FMCDAQ2 | 2019_r2_kc705_fmcdaq2.zip |
KC705 | FMCJESDADC1 | 2019_r2_kc705_fmcjesdadc1.zip |
KC705 | FMCOMMS2-3 | 2019_r2_kc705_fmcomms2-3.zip |
KC705 | FMCOMMS4 | 2019_r2_kc705_fmcomms4.zip |
KCU105 | ADRV9371X | 2019_r2_kcu105_adr9371x.zip |
KCU105 | FMCDAQ2 | 2019_r2_kcu105_fmcdaq2.zip |
KCU105 | FMCOMMS2-3 | 2019_r2_kcu105_fmcomms2-3.zip |
KCU105 | FMCOMMS4 | 2019_r2_kcu105_fmcomms4.zip |
VC707 | AD6676EVB | 2019_r2_vc707_ad6676evb.zip |
VC707 | FMCADC2 | 2019_r2_vc707_fmcadc2.zip |
VC707 | FMCADC5 | 2019_r2_vc707_fmcadc5.zip |
VC707 | FMCJESDADC1 | 2019_r2_vc707_fmcjesdadc1.zip |
VC707 | FMCOMMS2-3 | 2019_r2_vc707_fmcomms2-3.zip |
VCU118 | AD9081 | 2019_r2_vcu118_ad9081.zip |
VCU118 | AD9081 M8 L4 | 2019_r2_vcu118_ad9081_m8_l4.zip |
VCU118 | AD9208 Dual | 2019_r2_vcu118_dual_ad9208.zip |
VCU118 | FMCDAQ3 | 2019_r2_vcu118_fmcdaq3.zip |
Latest Build: 2018_05_08 - 2018_R1
Linux branch:2018_R1
Linux repository:https://github.com/analogdevicesinc/linux.git
Vivado branch:hdl_2018_r1
Vivado repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | 2018_r1_kc705_ad9467_fmc.zip |
KC705 | FMCDAQ2 | 2018_r1_kc705_fmcdaq2.zip |
KC705 | FMCJESDADC1 | 2018_r1_kc705_fmcjesdadc1.zip |
KC705 | FMCOMMS2-3 | 2018_r1_kc705_fmcomms2-3.zip |
KC705 | FMCOMMS4 | 2018_r1_kc705_fmcomms4.zip |
KCU105 | ADRV9371X | 2018_r1_kcu105_adr9371x.zip |
KCU105 | FMCDAQ2 | 2018_r1_kcu105_fmcdaq2.zip |
KCU105 | FMCDAQ3 | 2018_r1_kcu105_fmcdaq3.zip |
KCU105 | FMCOMMS2-3 | 2018_r1_kcu105_fmcomms2-3.zip |
KCU105 | FMCOMMS4 | 2018_r1_kcu105_fmcomms4.zip |
VC707 | AD6676EVB | 2018_r1_vc707_ad6676evb.zip |
VC707 | FMCADC2 | 2018_r1_vc707_fmcadc2.zip |
VC707 | FMCADC5 | 2018_r1_vc707_fmcadc5.zip |
VC707 | FMCDAQ2 | 2018_r1_vc707_fmcdaq2.zip |
VC707 | FMCJESDADC1 | 2018_r1_vc707_fmcjesdadc1.zip |
VC707 | FMCOMMS2-3 | 2018_r1_vc707_fmcomms2-3.zip |
VC707 | FMCOMMS4 | 2018_r1_vc707_fmcomms4.zip |
There are two ways of loading the design. One is using the XMD command line. Open a xmd command window/shell and enter the commands manually.
Below is just a example and the file-names may vary.
Xilinx XMD command console
XMD has been replaced with XSCT/XSDB in newer releases of VIVADO. In windows, you can run the XSCT terminal from start menu → Xilinx Design Tools → Xilinx Software Command Line Tool…
Xilinx XSCT command console
****** Xilinx System Debugger (XSDB) v2021.1 **** Build date : Jun 10 2021-20:11:58 ** Copyright 1986-2020 Xilinx, Inc. All Rights Reserved. xsdb% connect attempting to launch hw_server ****** Xilinx hw_server v2021.1 **** Build date : Jun 10 2021 at 20:11:57 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 tcfchan#0 xsdb% fpga -f system_top.bit 100% 4MB 1.7MB/s 00:02 xsdb% targets 1 xc7k325t 2 MicroBlaze Debug Module at USER2 3 MicroBlaze #0 (Running) xsdb% target 3 xsdb% dow simpleImage.kc705_fmcomms2-3.strip Downloading Program -- /home/liacob/microblaze/simpleImage.kc705_fmcomms2-3/simpleImage.kc705_fmcomms2-3.strip section, .text: 0x80000000 - 0x804763ab section, __fdt_blob: 0x804763ac - 0x804863ab section, .rodata: 0x80487000 - 0x808b110f section, .builtin_fw: 0x808b1110 - 0x808b1133 section, __ksymtab: 0x808b1134 - 0x808b746b section, __ksymtab_gpl: 0x808b746c - 0x808bc483 section, __ksymtab_strings: 0x808bc484 - 0x808d6973 section, __param: 0x808d6974 - 0x808d6e5f section, __modver: 0x808d6e60 - 0x808d6fff section, __ex_table: 0x808d7000 - 0x808d844f section, .notes: 0x808d8450 - 0x808d848b section, .sdata2: 0x808d848c - 0x808d8fff section, .data: 0x808d9000 - 0x8095893f section, .init.text: 0x80959000 - 0x8097a75b section, .init.data: 0x8097a75c - 0x8097c053 section, .init.ivt: 0x8097c054 - 0x8097c07b section, .init.setup: 0x8097c07c - 0x8097c3f3 section, .initcall.init: 0x8097c3f4 - 0x8097c80f section, .con_initcall.init: 0x8097c810 - 0x8097c813 section, .init.ramfs: 0x8097c814 - 0x80c2a9fb section, .bss: 0x80c2b000 - 0x80c4225b 100% 12MB 0.2MB/s 00:56 Setting PC to Program Start Address 0x80000000 Successfully downloaded /home/liacob/microblaze/simpleImage.kc705_fmcomms2-3/simpleImage.kc705_fmcomms2-3.strip xsdb% Info: MicroBlaze #0 (target 3) Stopped at 0x0 (Stop) xsdb% con Info: MicroBlaze #0 (target 3) Running xsdb%
The second method is to run the tcl script which takes care of loading the bit file and the linux image. Run Vivado TCL Shell from Windows start menu → Xilinx Design Suite → Vivado → Vivado TCL Shell. (In Linux, source the settings.sh file first)
Then run the tcl script:
Vivado TCL shell or Linux console
****** Xilinx System Debugger (XSDB) v2021.1 **** Build date : Jun 10 2021-20:11:58 ** Copyright 1986-2020 Xilinx, Inc. All Rights Reserved. xsdb% source run.tcl attempting to launch hw_server ****** Xilinx hw_server v2021.1 **** Build date : Jun 10 2021 at 20:11:57 ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 100% 4MB 1.7MB/s 00:02 Downloading Program -- /home/liacob/microblaze/simpleImage.kc705_fmcomms2-3/simpleImage.kc705_fmcomms2-3.strip section, .text: 0x80000000 - 0x804763ab section, __fdt_blob: 0x804763ac - 0x804863ab section, .rodata: 0x80487000 - 0x808b110f section, .builtin_fw: 0x808b1110 - 0x808b1133 section, __ksymtab: 0x808b1134 - 0x808b746b section, __ksymtab_gpl: 0x808b746c - 0x808bc483 section, __ksymtab_strings: 0x808bc484 - 0x808d6973 section, __param: 0x808d6974 - 0x808d6e5f section, __modver: 0x808d6e60 - 0x808d6fff section, __ex_table: 0x808d7000 - 0x808d844f section, .notes: 0x808d8450 - 0x808d848b section, .sdata2: 0x808d848c - 0x808d8fff section, .data: 0x808d9000 - 0x8095893f section, .init.text: 0x80959000 - 0x8097a75b section, .init.data: 0x8097a75c - 0x8097c053 section, .init.ivt: 0x8097c054 - 0x8097c07b section, .init.setup: 0x8097c07c - 0x8097c3f3 section, .initcall.init: 0x8097c3f4 - 0x8097c80f section, .con_initcall.init: 0x8097c810 - 0x8097c813 section, .init.ramfs: 0x8097c814 - 0x80c2a9fb section, .bss: 0x80c2b000 - 0x80c4225b 100% 12MB 0.2MB/s 00:56 Setting PC to Program Start Address 0x80000000 Successfully downloaded /home/liacob/microblaze/simpleImage.kc705_fmcomms2-3/simpleImage.kc705_fmcomms2-3.strip Info: MicroBlaze #0 (target 3) Running xsdb% Info: tcfchan#0 closed xsdb%
If you are interested in the Linux console messages and command line interface, connect a USB cable to the USB UART port. Terminal settings are 115200,8N1.
There are two users:
user | password |
---|---|
root | analog |
analog | analog |
If you FPGA carrier board (KC705, vc707, ml605) features a LCD display and the board is connected to a DHCP enabled network. You should also see it's IP address printed on the display. This allows you to connect remote to the board as well. (ssh, libiio remote)
Unlike shown in the picture below you won't see the second line. In case the IP address is 192.168.2.2, this indicates that DHCP failed and it's now using it's default address. This address may not be within your subnet, and things therefore may fail.
You should see the kernel start-up messages as follows:
This specifies any shell prompt running on the target
Ramdisk addr 0x00000000, Compiled-in FDT at 0x804763ac Linux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (crosstool-NG 1.20.0)) #1853 Tue Jul 27 13:32:24 IST 2021 setup_memory: max_mapnr: 0x30000 setup_memory: min_low_pfn: 0x80000 setup_memory: max_low_pfn: 0xb0000 setup_memory: max_pfn: 0xb0000 Zone ranges: DMA [mem 0x0000000080000000-0x00000000afffffff] Normal empty Movable zone start for each node Early memory node ranges node 0: [mem 0x0000000080000000-0x00000000bfffffff] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff] On node 0 totalpages: 196608 DMA zone: 1536 pages used for memmap DMA zone: 0 pages reserved DMA zone: 196608 pages, LIFO batch:63 setup_cpuinfo: initialising setup_cpuinfo: Using full CPU PVR support ERROR: Microblaze HW_MUL-different for PVR and DTS wt_msr_noirq pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists, mobility grouping on. Total pages: 195072 Kernel command line: console=ttyUL0,115200 Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 766124K/786432K available (4568K kernel code, 510K rwdata, 4416K rodata, 2886K init, 92K bss, 20308K reserved, 0K cma-reserved) Kernel virtual memory layout: * 0xffffe000..0xfffff000 : fixmap * 0xffffe000..0xffffe000 : early ioremap * 0xb0000000..0xffffe000 : vmalloc & ioremap NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 irq-xilinx: mismatch in kind-of-intr param irq-xilinx: /amba_pl/interrupt-controller@41200000: num_irq=16, edge=0xffffc5de /amba_pl/timer@41c00000: irq=1 clocksource: xilinx_clocksource: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns xilinx_timer_shutdown xilinx_timer_set_periodic sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns Calibrating delay loop... 49.35 BogoMIPS (lpj=246784) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) devtmpfs: initialized random: get_random_u32 called from bucket_table_alloc.isra.6+0x1e8/0x218 with crng_init=0 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 256 (order: -1, 3072 bytes) NET: Registered protocol family 16 jesd204: found 0 devices and 0 topologies clocksource: Switched to clocksource xilinx_clocksource NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) TCP established hash table entries: 8192 (order: 3, 32768 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes) TCP: Hash tables configured (established 8192 bind 8192) UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. random: fast init done Skipping unavailable RESET gpio -2 (reset) workingset: timestamp_bits=30 max_order=18 bucket_order=0 jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) io scheduler mq-deadline registered io scheduler kyber registered Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled 40600000.serial: ttyUL0 at MMIO 0x40600000 (irq = 4, base_baud = 0) is a uartlite console [ttyUL0] enabled brd: module loaded Xilinx SystemACE device driver, major=254 60000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x008962 NOR chip too large to fit in mapping. Attempting to cope... Intel/Sharp Extended Query Table at 0x010A Intel/Sharp Extended Query Table at 0x010A Intel/Sharp Extended Query Table at 0x010A Intel/Sharp Extended Query Table at 0x010A Intel/Sharp Extended Query Table at 0x010A Using buffer write method Using auto-unlock on power-up/resume cfi_cmdset_0001: Erase suspend on write enabled erase region 0: offset=0x0,size=0x20000,blocks=1023 erase region 1: offset=0x7fe0000,size=0x8000,blocks=4 Reducing visibility of 131072KiB chip to 32768KiB 4 fixed-partitions partitions found on MTD device 60000000.flash Creating 4 MTD partitions on "60000000.flash": 0x000000000000-0x000001380000 : "fpga" 0x000001380000-0x000001400000 : "boot" 0x000001400000-0x000001440000 : "bootenv" 0x000001440000-0x000002000000 : "image" xilinx_spi 44a70000.axi_quad_spi: no CS gpios available libphy: Fixed MDIO Bus: probed xilinx_emaclite 40e00000.ethernet: Device Tree Probing libphy: Xilinx Emaclite MDIO: probed xilinx_emaclite 40e00000.ethernet: MAC address is now 00:0a:35:00:00:02 xilinx_emaclite 40e00000.ethernet: Xilinx EmacLite at 0x40E00000 mapped to 0xB007A000, irq=2 i2c /dev entries driver i2c i2c-0: Added multiplexed i2c bus 1 i2c i2c-0: Added multiplexed i2c bus 2 at24 3-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write i2c i2c-0: Added multiplexed i2c bus 3 i2c i2c-0: Added multiplexed i2c bus 4 i2c i2c-0: Added multiplexed i2c bus 5 i2c i2c-0: Added multiplexed i2c bus 6 i2c i2c-0: Added multiplexed i2c bus 7 i2c i2c-0: Added multiplexed i2c bus 8 pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548 ad9361 spi0.0: ad9361_probe : enter (ad9361) ad9361 spi0.0: ad9361_probe : AD936x Rev 2 successfully initialized cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x79024000 mapped to 0x(ptrval), probed DDS AD9361 axi_sysid 45000000.axi-sysid-0: [fmcomms2] on [kc705] git <43c6ae1ca9faf268f30c7ef489f1428fc30a8b23> clean [2021-06-09 21:38:35] UTC NET: Registered protocol family 17 cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x79020000 mapped to 0x(ptrval), probed ADC AD9361 as MASTER Freeing unused kernel memory: 2884K This architecture does not have kernel memory protection. Run /init as init process Starting logging: OK Initializing random number generator... random: dd: uninitialized urandom read (512 bytes read) done. Starting network: udhcpc: started, v1.27.2 udhcpc: sending discover xilinx_emaclite 40e00000.ethernet eth0: Link is Down udhcpc: sending discover udhcpc: sending discover udhcpc: sending discover udhcpc: sending discover udhcpc: sending discover udhcpc: sending discover udhcpc: no lease, failing Starting dropbear sshd: random: dropbear: uninitialized urandom read (32 bytes read) OK Starting IIO Server Daemon Welcome to Buildroot buildroot login: root Password: #
Please see also here:Oscilloscope
The IIO Oscilloscope application can be used to connect to another platform that has a connected device in order to configure the device and read data from it.
Build and start osc on a network enabled Linux host.
Once the application is launched goto Settings → Connect and enter the IP address of the target in the popup window.