Wiki

This version is outdated by a newer approved version.DiffThis version (25 Mar 2024 14:16) is a draft.
Approvals: 0/1
The Previously approved version (12 Feb 2024 20:26) is available.Diff

This is an old revision of the document!


Microcontroller no-OS Drivers

The majority of ADI's products are peripherals to a non-ADI digital engine (FPGA, microprocessor, or microcontroller). While there is major work underway on FPGAs (Xilinx and Altera) and microprocessors (running an operating system like Linux), the efforts on microcontrollers are fragmented due to the diverse nature of the microcontroller market. The goal of these projects (microcontroller/no-OS) is to be able to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, to help customers using microcontrollers with ADI parts.

Drivers List

Accelerometers

Analog to Digital Converters

Analog Front End

Capacitive to Digital & Touch Screen Controllers

D/A Converters (DAC)

Digital Input/Output (DIO) Devices

Clock Generation Devices

Filter Devices

Gyroscopes

IMUs (Inertial Measurement Units)

  • ADIS16505: Precision, Miniature MEMS IMU
  • ADIS1657x: Precision, Miniature MEMS IMU

Impedance Analyzer

Mobile I/O Expander & Keypad Controller

Multiplexers

Optical

Digital Potentiometers

RF Transceivers

Digital Temperature Sensors

Power

resources/no-os/drivers.1711372564.txt.gz · Last modified: 25 Mar 2024 14:16 by Radu Sabau