Wiki

This version (14 Jan 2021 05:45) was approved by Robin Getz.The Previously approved version (30 Sep 2019 12:34) is available.Diff

AD5758 - No-OS Driver

Supported Devices

Evaluation Boards

Overview

The AD5758 is a single-channel, voltage and current output digital-to-analog converter (DAC) that operates with a power supply range from −33 V minimum on AVSS to +33 V maximum on AVDD1 with a maximum operating voltage between the two rails of 60 V. On-chip DPC minimizes package power dissipation, which is achieved by regulating the supply voltage (VDPC+) to the VIOUT output driver circuitry from 5 V to 27 V using a buck dc-to-dc converter, optimized for minimum on-chip power dissipa-tion. The CHART pin enables a HART signal to be coupled onto the current output.

The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, DSP, and microcontroller interface standards. The interface also features an optional SPI cyclic redundancy check (CRC) and a watchdog timer. The AD5758 offers improved diagnostic features from its predecessors, such as output current monitoring and an integrated 12-bit diagnostic ADC. Additional robustness is provided by the inclusion of a fault protection switch on VIOUT, +VSENSE, and −VSENSE pins.

Applications

  • Process control
  • Actuator control
  • PLC and DCS applications
  • HART network connectivity

HDL Design Description

In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design in general.

In order to build the HDL design the user has to go through the following steps:

  1. Confirm that you have the right tools (the reference design requires Vivado 2018.3)
  2. Clone the HDL GitHub repository (the project is located at ad5758_sdz)

Software Setup

In order to perform the software setup the user has to go through the following steps:

  1. Confirm that you have the right tools (the reference design requires XSDK)
  2. Clone the No-OS GitHub repository (the project is located at ad5758-sdz )
  3. Follow the instructions provided by software_setup.

Driver Description

Functions Declarations

Function Description
static uint8_t ad5758_compute_crc8(uint8_t *data, uint8_t data_size)
Compute CRC8 checksum.
static int32_t ad5758_spi_reg_read(struct ad5758_dev *dev, uint8_t reg_addr, uint16_t *reg_data);
Read from device.
static int32_t ad5758_spi_reg_write(struct ad5758_dev *dev, uint8_t reg_addr, uint16_t reg_data);
Write to device.
static int32_t ad5758_spi_write_mask(struct ad5758_dev *dev, uint8_t reg_addr, uint32_t mask, uint16_t data);
SPI write to device using a mask.
int32_t ad5758_set_crc(struct ad5758_dev *dev, uint8_t crc_en);
Enable/disable SPI CRC function.
int32_t ad5758_wait_for_refresh_cycle(struct ad5758_dev *dev);
Busy wait until CAL_MEM_UNREFRESHED bit in the DIGITAL_DIAG_RESULTS clears.
int32_t ad5758_soft_reset(struct ad5758_dev *dev);
Initiate a software reset.
int32_t ad5758_calib_mem_refresh(struct ad5758_dev *dev);
Initiate a calibration memory refresh to the shadow registers.
int32_t ad5758_set_dc_dc_conv_mode(struct ad5758_dev *dev, enum ad5758_dc_dc_mode mode);
Configure the dc-to-dc controller mode.
int32_t ad5758_set_dc_dc_ilimit(struct ad5758_dev *dev, enum ad5758_dc_dc_ilimt ilimit);
Set the dc-to-dc converter current limit.
int32_t ad5758_fault_prot_switch_en(struct ad5758_dev *dev, uint8_t enable);
Enable/disable VIOUT Fault Protection Switch.
int32_t ad5758_internal_buffers_en(struct ad5758_dev *dev, uint8_t enable);
Enable/disable Enable Internal Buffers.
int32_t ad5758_set_out_range(struct ad5758_dev *dev, enum ad5758_output_range range);
Select Output Range.
int32_t ad5758_slew_rate_config(struct ad5758_dev *dev, enum ad5758_slew_rate_clk clk, uint8_t enable);
Configure the slew rate by setting the clock and enable/disable the control.
int32_t ad5758_dac_input_write(struct ad5758_dev *dev, uint16_t code);
Write DAC data to the input register.
int32_t ad5758_dac_output_en(struct ad5758_dev *dev, uint8_t enable);
Enable/disable VIOUT.
int32_t ad5758_clear_dig_diag_flag(struct ad5758_dev *dev, enum ad5758_dig_diag_flags flag);
Clear the error flags for the on-chip digital diagnostic features.
int32_t ad5758_set_clkout_config(struct ad5758_dev *dev, enum ad5758_clkout_config config, enum ad5758_clkout_freq freq);
Configure CLKOUT by setting the frequency and enabling/disabling the option.
int32_t ad5758_select_adc_ip(struct ad5758_dev *dev, enum ad5758_adc_ip adc_ip_sel);
Select which node to multiplex to the ADC.
int32_t ad5758_select_adc_depth(struct ad5758_dev *dev, uint8_t num_of_channels);
Set depth of the sequencer.
int32_t ad5758_set_adc_channel_input(struct ad5758_dev *dev, uint8_t channel, enum ad5758_adc_ip adc_ip_sel);
Load the desired channel into the sequencer with the adc input.
int32_t ad5758_set_adc_mode(struct ad5758_dev *dev, enum ad5758_adc_mode adc_mode, uint8_t enable);
Configure the ADC into one of four modes of operation.
int32_t ad5758_init(struct ad5758_dev **device, struct ad5758_init_param init_param);
Set up the device from power-on or reset condition with the correct.

Types Declarations

enum ad5758_dc_dc_mode {
	DC_DC_POWER_OFF,
	DPC_CURRENT_MODE,
	DPC_VOLTAGE_MODE,
	PPC_CURRENT_MODE,
};
 
enum ad5758_dig_diag_flags {
	DIAG_SPI_CRC_ERR,
	DIAG_SLIPBIT_ERR,
	DIAG_SCLK_COUNT_ERR,
	DIAG_INVALID_SPI_ACCESS_ERR = 4,
	DIAG_CAL_MEM_CRC_ERR,
	DIAG_INVERSE_DAC_CHECK_ERR,
	DIAG_DAC_LATCH_MON_ERR = 8,
	DIAG_THREE_WI_RC_ERR,
	DIAG_WDT_ERR = 11,
	DIAG_ERR_3WI,
	DIAG_RESET_OCCURRED,
};
 
enum ad5758_clkout_config {
	CLKOUT_DISABLE,
	CLKOUT_ENABLE,
};
 
enum ad5758_clkout_freq {
	CLKOUT_FREQ_416_KHZ,
	CLKOUT_FREQ_435_KHZ,
	CLKOUT_FREQ_454_KHZ,
	CLKOUT_FREQ_476_KHZ,
	CLKOUT_FREQ_500_KHZ,
	CLKOUT_FREQ_526_KHZ,
	CLKOUT_FREQ_555_KHZ,
	CLKOUT_FREQ_588_KHZ,
};
 
enum ad5758_slew_rate_clk {
	SR_CLOCK_240_KHZ,
	SR_CLOCK_200_KHZ,
	SR_CLOCK_150_KHZ,
	SR_CLOCK_128_KHZ,
	SR_CLOCK_64_KHZ,
	SR_CLOCK_32_KHZ,
	SR_CLOCK_16_KHZ,
	SR_CLOCK_8_KHZ,
	SR_CLOCK_4_KHZ,
	SR_CLOCK_2_KHZ,
	SR_CLOCK_1_KHZ,
	SR_CLOCK_512_HZ,
	SR_CLOCK_256_HZ,
	SR_CLOCK_128_HZ,
	SR_CLOCK_64_HZ,
	SR_CLOCK_16_HZ,
};
 
enum ad5758_dc_dc_ilimt {
	ILIMIT_150_mA,
	ILIMIT_200_mA,
	ILIMIT_250_mA,
	ILIMIT_300_mA,
	ILIMIT_350_mA,
	ILIMIT_400_mA,
};
 
enum ad5758_output_range {
	RANGE_0V_5V,
	RANGE_0V_10V,
	RANGE_M5V_5V,
	RANGE_M10V_10V,
	RANGE_0mA_20mA = 8,
	RANGE_0mA_24mA,
	RANGE_4mA_24mA,
	RANGE_M20mA_20mA,
	RANGE_M24mA_24mA,
	RANGE_M1mA_22mA,
};
 
enum ad5758_adc_ip {
	ADC_IP_MAIN_DIE_TEMP,
	ADC_IP_DCDC_DIE_TEMP,
	ADC_IP_REFIN = 3,
	ADC_IP_REF2,
	ADC_IP_VSENSE = 13,
	ADC_IP_MVSENSE,
	ADC_IP_INT_AVCC = 20,
	ADC_IP_REGOUT,
	ADC_IP_VLOGIC,
	ADC_IP_INT_CURR_MON_VOUT,
	ADC_IP_REFGND,
	ADC_IP_AGND,
	ADC_IP_DGND,
	ADC_IP_VDPC,
	ADC_IP_AVDD2,
	ADC_IP_AVSS,
	ADC_IP_DCDC_DIE_NODE,
	ADC_IP_REFOUT,
};
 
enum ad5758_adc_mode {
	ADC_MODE_KEY_SEQ = 2,
	ADC_MODE_AUTO_SEQ,
	ADC_MODE_SINGLE_CONV,
	ADC_MODE_SINGLE_KEY_CONV,
};
 
struct ad5758_dev {
	/* SPI */
	struct spi_desc *spi_desc;
        /* GPIO */
        struct gpio_desc *reset_n;
        struct gpio_desc *ldac_n;
	/* Device Settings */
	uint8_t crc_en;
	enum ad5758_dc_dc_mode dc_dc_mode;
};
 
struct ad5758_init_param {
	/* SPI */
	struct spi_init_param spi_init;
        /* GPIO */
	struct gpio_init_param reset_n;
	struct gpio_init_param ldac_n;
	/* Device Settings */
	uint8_t crc_en;
	enum ad5758_dc_dc_mode dc_dc_mode;
	enum ad5758_clkout_config clkout_config;
	enum ad5758_clkout_freq clkout_freq;
	enum ad5758_dc_dc_ilimt dc_dc_ilimt;
	enum ad5758_output_range output_range;
	enum ad5758_slew_rate_clk slew_rate_clk;
};

Reference Design

Downloads

resources/tools-software/uc-drivers/ad5758.txt · Last modified: 14 Jan 2021 05:38 by Robin Getz