Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (19 Apr 2019 21:10) is a draft.
Approvals: 0/1

This is an old revision of the document!


Linux Drivers

Building the ADI Linux kernel

Common elements for all kernel builds:

  • make sure you have make installed on your system, but we generally recommend installing the build-essentials tools for your Linux distribution
  • some builds will require you to have u-boot-tools installed, to have the mkimage utilities available, so it's good to have them available/installed

Target specific details:

The rapid increase in use of free and open-source software (FOSS), in particular Linux, represents the most significant, all-encompassing, and long-term trend that the embedded industry has seen since the early 1980s.1) Like many, Analog Devices creates and maintains Linux Drivers for various Analog Devices products.

Select a driver from the list below.

Driver List

Backlight

Battery Charger

Battery Gas Gauge

GPIO

Secondary function

HWMon & PMBus

HWMon

PMbus

I2C Mux

IIO - Accelerometers

IIO - Amplifiers

IIO - Analog to Digital Converters

IIO - Capacitance to Digital Converters

IIO - Digital to Analog Converters

* AD8801 : Octal 8-Bit TrimDAC with Power Shutdown & Mid-Scale Preset AD8801 * AD8803 : Octal 8-Bit TrimDAC with Power Shutdown & Mid-Scale Preset AD8803

IIO - Direct Digital Synthesis

IIO - Frequency Synthesizers / Phase-Locked Loop

IIO - Gyroscopes

IIO - Impedance Converters and Network Analyzers

IIO - Inertial Measurement Units

IIO - Resolvers

IIO - Receivers

IIO - Transceivers

Input - Keyboard

Input - Misc

Input - Touchscreens

LED

Miscellaneous

Multifunction Device

Multiplexers

Networking - MAC802154

Regulators

Power-Off

Sound

Video

1)
IDC study/survey from over 5000 developers in 116 countries. Open Source in Global Software: Market Impact, Disruption, and Business Models. 2006.
resources/tools-software/linux-drivers-all.1555701050.txt.gz · Last modified: 19 Apr 2019 21:10 by Robin Getz