Wiki

This version (04 Nov 2019 18:46) was approved by travisfcollins.The Previously approved version (11 Jul 2019 01:02) is available.Diff

Hacking the ADALM-PLUTO

Hacking the ADALM-PLUTO is possible (and encouraged). In this case - what we mean by hacking is the act of programming or extending the functionality or use cases of the PlutoSDR, in a spirit of playfulness and exploration. In order to do that, you should be familiar with the device, from a user and developer standpoint.

Many aspects of the PlutoSDR are based from the AD-FMCOMMS3-EBZ, and you should be familiar with that, as it will help understand how to extend the PlutoSDR.

  1. Hardware including:

Resources For Building Your Own SDR

Hopefully you have reviewed the documentation on the AD9361, and the FMCOMMS2, FMCOMMS3, FMCOMMS4. Those guides provide alot of background on the combination of the ad9361, ad9363, or ad9364 and the Xilinx Zynq.

  1. Testing the ADALM-PLUTO SDR.
university/tools/pluto/hackers.txt · Last modified: 04 Nov 2019 18:46 by travisfcollins