Wiki

This version (06 Jan 2021 16:41) was approved by Robin Getz.The Previously approved version (04 Jul 2019 17:51) is available.Diff

ADALM-PLUTO for Developers

The people who typical read these pages are those who write custom software or HDL (for the FPGA) that run directly on the Pluto device. This may put the Pluto in different modes, and support different external USB devices (including USB/LAB, or USB/WiFi), extending the capabilities of the device, or completely changing the data that is transferred to the host. Since the goal of the project is to keep things as open as possible, the details on how to compile kernels, create bit files, assemble FIT files and load them into the device, should be found here.

While we do have a few examples, and show how to re-create the default software loads, since this the hardware can be nearly a blank slate for your project, you can do anything you want.

Content

university/tools/pluto/developers.txt · Last modified: 12 Oct 2019 00:40 by Robin Getz