You can find the results of your wiki search below. If you didn't find what you were looking for, you can create or edit the page named after your query with the appropriate button, or search the rest of Analog.com. If that doesn't work, try Google.
= Downloads =====
* {{:resources:fpga:xilinx:fmc:ad-fmcomms1-ebz:quickstart:ml605_restoring_cf_fla... (Sandisk Ulra II or similar)
* AD-FMCOMMS1-EBZ FMC Board.
===== Software Installs =====
* Format... switches on the board:
{{ :resources:fpga:xilinx:fmc:ad-fmcomms1-ebz:ml605.png?500 |ML605 Diagram}}
- Connect the AD-FMCOMMS1-EBZ FMC board to the ML605, on the LPC FMC connector (20)
(Sandisk Ulra II or similar)
* AD-FMCOMMS1-EBZ FMC Board.
* Rohde & Schwarz FSEA30, FSEA20, FSEB20... switches on the board:
{{ :resources:fpga:xilinx:fmc:ad-fmcomms1-ebz:ml605.png?500 |ML605 Diagram}}
- Connect the AD-FMCOMMS1-EBZ FMC board to the ML605, on the LPC FMC connector (20).
- Turn on the power switch on the ML605 board (18
e transmited RF data.
{{ :resources:fpga:xilinx:fmc:dscn1188.png?direct&400 |FMComms + Zynq Board}}
<WRAP alert round>The AD-FMCOMMS1-EBZ FMC Card is not fully ANSI/VITA 57.1 compatible:
* ... rk with FPGA Development systems which include an FMC connector. It may not mechanically fit on other A... ive paths
* Allows high channel density
* LPC FMC Compatible, meets VITA specifications except card
cking and power supply.
{{:resources:fpga:xilinx:fmc:ad-fmcomms1-ebz:cf_xcomm_kc705_bd.jpg?600|Block d... n board crystal (50MHz) or from the FPGA (through FMC). The clock
path mainly consists of an [[adi>AD9... the schematic ''9548_REF_[PN]'' nets) tied to the FMC connector's ''LA_17_[PN]_CC'' pin. This allows th... eceives all the power from the FPGA board through FMC.
==== Optional add-on boards ====
While the boa
Close Solder Jumper:
{{ :resources:fpga:xilinx:fmc:adc2.png?200|Settings for RF Section enabled}}
^ ...
Close Solder Jumpers:
{{ :resources:fpga:xilinx:fmc:dac1.png?130|}}
^ JUMPER ^ A (1) ^ COM (2) ^ B (3...
Close Solder Jumper:
{{ :resources:fpga:xilinx:fmc:adc1.png?200|Settings for RF Section bypassed}}
^...
Close Solder Jumpers:
{{ :resources:fpga:xilinx:fmc:dac2.png?130|}}
^ JUMPER ^ A (1) ^ COM (2) ^ B (3
===
* Xilinx KC705 or VC707
* AD-FMCOMMS1-EBZ FMC Board.
* Micro / Mini-USB Cable
====== Testing ======
* Connect the AD-FMCOMMS1-EBZ FMC board to the FPGA carrier, on the KC705: FMC LPC or VC707: FMC2 connector.
* Connect USB JTAG (Micro USB) to your host PC.
* Turn on the power
Microblaze Linux Kernel image for the AD-FMCOMMS1 FMC board connected to an [[xilinx>KC705]].
===== Re... t device-trees for the different FPGA carrier and FMC module combination exist type:
<code>
Dave@HAL9... ore information =====
* [[resources/fpga/xilinx/fmc/ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ Reference Design]
information also check:
* [[http://www.vita.com/fmc|VITA's FMC info]]
* [[adi>en/evaluation/eval-fmcomms/eb.html#buy-nav|Buy the AD-FMComms1-EBZ]]
{{na
- Plug the FMComms1-EBZ into the ZedBoard via the FMC connector (J1). Ensure that the VADJ SELECT is se... the instructions on the [[/resources/fpga/xilinx/fmc/ad-fmcomms1-ebz/iio_scope|IIO Scope]] page
Here
Microblaze Linux Kernel image for the AD-FMCOMMS1 FMC board connected to an [[xilinx>ML605]].
<WRAP ro... ore information =====
* [[resources/fpga/xilinx/fmc/ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ Reference Design]