Wiki

This version (15 Jan 2016 16:35) was approved by charlyelkhoury.The Previously approved version (22 Oct 2014 13:55) is available.Diff

AD-FMCOMMS1-EBZ Hardware

Picture and Main components

Outline

For those that don't want to load up the Allegro viewer, here is a basic outline/component placements of the board.

Size

The size of the board (not including the SMA connectors, which project beyond the edge of the board) is 3.51 inches by 2.72 inches (or about 89mm x 69mm). This exceeds the FMC specifications of 84mm x 69mm).

Downloads

Navigation - AD-FMCOMMS1-EBZ

resources/eval/user-guides/ad-fmcomms1-ebz/hardware.txt · Last modified: 15 Jan 2016 16:35 by charlyelkhoury