FMComms1 Demo System
Congratulations, you are about to assemble a demo system, which should have everything you need to properly demo the FMComms1 system and the Xilinx Zynq-7000 All Programmable SoC.
If you don't have a box, and you need to self assemble your kit, please refer to the standard zynq documents.
Contents:
Required external equipment:
Instructions:
Reseat the
SD Card in the Zedboard (on bottom – J12). To ensure it didn’t come loose during shipping.
Plug the FMComms1-EBZ into the ZedBoard via the FMC connector (J1). Ensure that the VADJ SELECT is set to 2.5V (J18).
Attach either (it doesn’t matter which).
Pulse Antennas to the FMComms1-EBZ Rx and Tx connectors (RF_OUT and RF_IN)
SMA cable between the FMComms1-EBZ Rx and Tx connectors (RF_OUT and RF_IN)
Plug the
USB Keyboard/Mouse into the mini
USB cable, and then the
USB cable into the
USB OTG connector (J13). If the mouse/keyboard are wireless make sure they are turned on.
Connect the HDMI Display device to the Zed Board HDMI OUT connector (J9)
Plug the power cable into the Zed Board (J20)
Plug the power cable into the AC power source. You may need to swap the ends to plug in the wall.
Turn the Zed Board on (SW8).
Wait 90 seconds for the IIOscope to come up.
Follow the instructions on the
IIO Scope page
Here are some pictures showing the FMComms1 board connected to the Zedboard: