This is an old revision of the document!
This driver supports the
The AXI DAC DDS HDL driver is the driver for the HDL interface core which is used on various FPGA designs. The driver is implemented as an Linux IIO driver. It's register map can be found here: Base register map (common to all cores)
This driver implements a polyphase dual tone DDS core per channel together with an waveform buffer mechanism. The buffer can be filled by arbitrary data, which is then typically cyclically repeated.
Source | Mainlined? |
---|---|
drivers/iio/frequency/cf_axi_dds.c | WIP |
Function | File |
---|---|
driver | drivers/iio/frequency/ad9122.c |
driver | drivers/iio/frequency/ad9144.c |
driver | drivers/iio/frequency/ad9162.c |
driver | drivers/iio/frequency/ad9172.c |
driver | drivers/iio/frequency/cf_axi_dds.c |
driver | drivers/iio/frequency/cf_axi_dds_buffer_stream.c |
include | drivers/iio/frequency/cf_axi_adc.h |
The AXI DAC/DDS driver is a platform driver and can only be instantiated via device tree.
Required devicetree properties:
Optional Parameters:
Example:
&spi0 { status = "okay"; adc0_ad9361: ad9361-phy@0 { #address-cells = <1>; #size-cells = <0>; #clock-cells = <1>; compatible = "ad9361"; /* SPI Setup */ reg = <0>; spi-cpha; spi-max-frequency = <10000000>; /* Clocks */ clocks = <&ad9361_clkin 0>; clock-names = "ad9361_ext_refclk"; clock-output-names = "rx_sampl_clk", "tx_sampl_clk"; [--- snip ---] } } &fpga_axi { tx_dma: dma@7c420000 { compatible = "adi,axi-dmac-1.00.a"; reg = <0x7c420000 0x10000>; #dma-cells = <1>; interrupts = <0 56 0>; clocks = <&clkc 16>; dma-channel { adi,source-bus-width = <64>; adi,destination-bus-width = <64>; adi,type = <1>; adi,cyclic; }; }; cf_ad9361_dac_core_0: cf-ad9361-dds-core-lpc@79024000 { compatible = "adi,axi-ad9361-dds-6.00.a"; reg = <0x79024000 0x1000>; clocks = <&adc0_ad9361 13>; clock-names = "sampl_clk"; dmas = <&tx_dma 0>; dma-names = "tx"; adi,axi-dds-default-scale = <0>; }; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AXI ADC HDL driver may depend on CONFIG_SPI
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Direct Digital Synthesis *** [--snip--] <*> Analog Devices CoreFPGA AXI DDS driver <*> Analog Devices AD9122 DAC [--snip--]
In case the driver probes successfully and the device gets instantiated. Your systems kernel messages should include a line, which may look like the one shown below.
cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (8.00.b) at 0x79024000 mapped to 0xf0998000, probed DDS AD9361
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
Some device attributes control the DDS HDL Core, others features of the DAC and associated clock providers.
This specifies any shell prompt running on the target
analog:/sys/bus/iio/devices/iio:device2# cd /sys/bus/iio/devices/ root@analog:/sys/bus/iio/devices# ls iio:device0 iio:device1 iio:device2 iio:device3 root@analog:/sys/bus/iio/devices# root@analog:/sys/bus/iio/devices# cd iio\:device2 root@analog:/sys/bus/iio/devices/iio:device2# ls -l total 0 drwxr-xr-x 5 root root 0 Jan 1 00:00 . drwxr-xr-x 4 root root 0 Jan 1 00:00 .. drwxrwxrwx 2 root root 0 Jan 1 00:00 buffer -rw-rw-rw- 1 root root 4096 Jan 1 00:00 dev -rw-rw-rw- 1 root root 4096 Jan 1 00:00 name lrwxrwxrwx 1 root root 0 Jan 1 00:00 of_node -> ../../../../../firmware/devicetree/base/fpga-axi@0/cf-ad9361-dds-core-lpc@79024000 -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage0_TX1_I_F1_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage0_TX1_I_F1_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage0_TX1_I_F1_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage0_TX1_I_F1_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage1_TX1_I_F2_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage1_TX1_I_F2_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage1_TX1_I_F2_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage1_TX1_I_F2_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage2_TX1_Q_F1_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage2_TX1_Q_F1_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage2_TX1_Q_F1_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage2_TX1_Q_F1_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage3_TX1_Q_F2_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage3_TX1_Q_F2_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage3_TX1_Q_F2_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage3_TX1_Q_F2_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage4_TX2_I_F1_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage4_TX2_I_F1_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage4_TX2_I_F1_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage4_TX2_I_F1_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage5_TX2_I_F2_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage5_TX2_I_F2_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage5_TX2_I_F2_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage5_TX2_I_F2_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage6_TX2_Q_F1_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage6_TX2_Q_F1_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage6_TX2_Q_F1_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage6_TX2_Q_F1_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage7_TX2_Q_F2_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage7_TX2_Q_F2_phase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage7_TX2_Q_F2_raw -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage7_TX2_Q_F2_scale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_altvoltage_sampling_frequency -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage0_calibphase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage0_calibscale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage1_calibphase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage1_calibscale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage2_calibphase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage2_calibscale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage3_calibphase -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage3_calibscale -rw-rw-rw- 1 root root 4096 Jan 1 00:00 out_voltage_sampling_frequency drwxrwxrwx 2 root root 0 Jan 1 00:00 power drwxrwxrwx 2 root root 0 Jan 1 00:00 scan_elements lrwxrwxrwx 1 root root 0 Jan 1 00:00 subsystem -> ../../../../../bus/iio -rw-rw-rw- 1 root root 4096 Jan 1 00:00 uevent root@analog:/sys/bus/iio/devices/iio:device2#
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# cat name cf-ad9361-dds-core-lpc
Values are in Hz.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_frequency 9279985 root@analog:/sys/bus/iio/devices/iio:device2# echo 500000 > out_altvoltage0_TX1_I_F1_frequency root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_frequency 500163
Values are in milli degrees.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_phase 89995 root@analog:/sys/bus/iio/devices/iio:device2# echo 91000 > out_altvoltage0_TX1_I_F1_phase root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_phase 90995
1 for enable, 0 for disable.
With the introduction of the big channel MUX (REG_CHAN_CNTRL_7, DAC_DDS_SEL) starting with HDV Version > 7.00, the RAW attribute has some side effects, that need to be understood. In many situations for example when the Buffer mode is used, it’s not desirable to write this attribute.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_raw 1
DDS amplitude: range 0.00 … 1.00 (relative to full scale)
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale 0.500000 root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale 1.000000 0.500000 0.250000 0.125000 ... root@analog:/sys/bus/iio/devices/iio:device2# echo 0.25 > out_altvoltage0_TX1_I_F1_scale root@analog:/sys/bus/iio/devices/iio:device2# cat out_altvoltage0_TX1_I_F1_scale 0.250000
Depending on the platform. These attributes may control converter internal or external processing blocks.
The AD9122 features Gain, DC Offset, and Phase adjustment for sideband suppression. These features can be controlled via following attributes:
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device2# grep “” out_voltage* out_voltage0_calibbias:0 out_voltage0_calibscale:505 out_voltage0_phase:0 out_voltage1_calibbias:0 out_voltage1_calibscale:505 out_voltage1_phase:0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device3> ls -l buffer total 0 -rw-r--r-- 1 root root 4096 Jan 1 00:12 enable -rw-r--r-- 1 root root 4096 Jan 1 00:12 length -r--r--r-- 1 root root 4096 Jan 1 00:12 watermark
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
watermark
A single positive integer specifying the maximum number of scan
elements to wait for.
Poll will block until the watermark is reached.
Blocking read will wait until the minimum between the requested
read amount or the low water mark is available.
Non-blocking read will retrieve the available samples from the
buffer even if there are less samples then watermark level. This
allows the application to block on poll with a timeout and read
the available samples after the timeout expires and thus have a
maximum delay guarantee.
data_available
A read-only value indicating the bytes of data available in the
buffer. In the case of an output buffer, this indicates the
amount of empty space available to write data to. In the case of
an input buffer, this indicates the amount of data available for
reading.
length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length.
Newer versions of the kernel will report the alignment requirements
associated with a device through the `length_align_bytes` property.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device3> ls -l scan_elements total 0 -rw-r--r-- 1 root root 4096 Jan 1 00:00 out_voltage0_en -r--r--r-- 1 root root 4096 Jan 1 00:00 out_voltage0_index -r--r--r-- 1 root root 4096 Jan 1 00:00 out_voltage0_type -rw-r--r-- 1 root root 4096 Jan 1 00:00 out_voltage1_en -r--r--r-- 1 root root 4096 Jan 1 00:00 out_voltage1_index -r--r--r-- 1 root root 4096 Jan 1 00:00 out_voltage1_type
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture.
Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer
and therefore in the form in which it is read from user-space.
Form is [s|u]bits/storage-bits. s or u specifies if signed
(2's complement) or unsigned. bits is the number of bits of
data and storage-bits is the space (after padding) that it
occupies in the buffer. Note that some devices will have
additional information in the unused bits so to get a clean
value, the bits value must be used to mask the buffer output
value appropriately. The storage-bits value also specifies the
data alignment. So u12/16 will be a unsigned 12 bit integer
stored in a 16 bit location aligned to a 16 bit boundary.
For other storage combinations this attribute will be extended
appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this
scan element in the buffer. Note these are not dependent on
what is enabled and may not be contiguous. Thus for user-space
to establish the full layout these must be used in conjunction
with all _en attributes to establish which channels are present,
and the relevant _type attributes to establish the data storage
format.
Some IIO drivers feature an optional debug facility, allowing users to read or write registers directly. Special care needs to be taken when using this feature, since you can modify registers on the back of the driver.
Accessing debugfs requires root privileges.
In order to identify if the IIO device in question feature this option you first need to identify the IIO device number.
Therefore read the name attribute of each IIO device
This specifies any shell prompt running on the target
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name /sys/bus/iio/devices/iio:device0/name:ad7291 /sys/bus/iio/devices/iio:device1/name:ad9361-phy /sys/bus/iio/devices/iio:device2/name:xadc /sys/bus/iio/devices/iio:device3/name:adf4351-udc-rx-pmod /sys/bus/iio/devices/iio:device4/name:adf4351-udc-tx-pmod /sys/bus/iio/devices/iio:device5/name:cf-ad9361-dds-core-lpc /sys/bus/iio/devices/iio:device6/name:cf-ad9361-lpc root@analog:~#
Change directory to /sys/kernel/debug/iio/ iio:deviceX and check if the direct_reg_access file exists.
This specifies any shell prompt running on the target
root@analog:~# cd /sys/kernel/debug/iio/iio\:device1 root@analog:/sys/kernel/debug/iio/iio:device1# ls direct_reg_access direct_reg_access
Reading
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x40
Writing
Write ADDRESS VALUE
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device1# echo 0x7 0x50 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device1# cat direct_reg_access 0x50
Accessing HDL CORE registers
Special ADI device driver convention for devices that have both:
In this case when accessing the HDL Core Registers always set BIT31.
The register map for typical ADI HDL cores can be found here: Register Map
This specifies any shell prompt running on the target
root@analog:/sys/kernel/debug/iio/iio:device6# echo 0x80000000 > direct_reg_access root@analog:/sys/kernel/debug/iio/iio:device6# cat direct_reg_access 0x80062
There are three different clocks associated with the DAC.
The Data/Interface Clock (DCI) is shared with the DDS HDL Core.
The default AD9122 driver configuration uses a concept called Direct Clocking. This means an external clock provider must supply DCI and DACCLK. In case the DAC interpolation feature is not used and the DAC operates in Word-Mode then DCI = DACCLK.
When N interpolation is used following equation must be satisfied.
N = {1, 2, 4, 8}
DACCLK = N * DCI and DACCLK ⇐ 1230MHz
The out_altvoltage_interpolation_frequency_available attribute allows you to query the supported interpolation frequencies for a given Interface Clock (out_altvoltage_X_sampling_frequency) by exercising possible settings on the clock provider. In case the clock provider is not capable providing exactly the requested rate, the mode is removed from the list.
So following example:
Assuming the clock provider can only provide following rates: 1000MHz / X, X = {1..1023}.
This results in following rates:
1000, 500, 333.33, 250, 200, 166.66, 142.85, 125, 111.11, …
The half-band interpolation filters have selectable pass bands that allow the center frequencies to be moved in increments of one-half their input data rate. The premodulation block provides a digital upconversion of the incoming waveform by one-half the incoming data rate, fDATA. This can be used to frequency-shift base- band input data to the center of the interpolation filter pass band.
The available center shift frequencies for a given Interface Clock (out_altvoltage_X_sampling_frequency), can be queried using the out_altvoltage_interpolation_center_shift_frequency_available attribute.
This specifies any shell prompt running on the target
root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_1A_sampling_frequency 491520000 root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency_available 491520000 983040000 root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency 491520000 root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency 0
This specifies any shell prompt running on the target
[ Set data clock to 122.88 MHz ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 122880000 > out_altvoltage_1A_sampling_frequency [ List available interpolation DAC frequencies ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_frequency_available 122880000 245760000 491520000 983040000 [ Select 8x interpolation ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 983040000 > out_altvoltage_interpolation_frequency [ List available center shift frequencies ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency_available 0 61440000 122880000 184320000 245760000 307200000 368640000 430080000 491520000 552960000 614400000 675840000 737280000 798720000 860160000 921600000 [ Select 2x interpolation ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 245760000 > out_altvoltage_interpolation_frequency [ List available center shift frequencies ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# cat out_altvoltage_interpolation_center_shift_frequency_available 0 61440000 122880000 184320000 [ Select center shift frequencies ] root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device4# echo 61440000 > out_altvoltage_interpolation_center_shift_frequency