This is an old revision of the document!
This Quad-MxFE Software Quick Start Guide should be used in conjunction with the Quad-MxFE Quick Start Guide to begin using the system.
_revc
In windows, you can run the XSCT
or XSDB
terminal from start menu → Xilinx Design Tools → Xilinx Software Command Line Tool…
On Linux open command terminal and execute following commands:
This specifies a system console
xsct% source run.vcu118_quad_ad9081_204c_txmode_11_rxmode_4_revc.tcl attempting to launch hw_server Xilinx hw_server v2018.2 Build date : Jun 14 2018-20:42:52 Copyright 1986-2018 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application Xilinx hw_server v2018.2 Build date : Jun 14 2018-20:42:52 Copyright 1986-2018 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 100% 42MB 1.7MB/s 00:25 Downloading Program -- C:/Users/cfrick/Desktop/quadmxfe_matlab_code/FPGA_image/Quad_MxFE_for_VCU118_2021-04-28/simpleImage.vcu118_quad_ad9081_204c_txmode_11_rxmode_4_revc.strip section, .text: 0x80000000 - 0x805229df section, fdt_blob: 0x805229e0 - 0x805329df section, .rodata: 0x80533000 - 0x80a0d73f section, .pci_fixup: 0x80a0d740 - 0x80a0f3ff section, .builtin_fw: 0x80a0f400 - 0x80a0f423 section, ksymtab: 0x80a0f424 - 0x80a194af section, ksymtab_gpl: 0x80a194b0 - 0x80a21c3f section, ksymtab_strings: 0x80a21c40 - 0x80a3f0e4 section, param: 0x80a3f0e8 - 0x80a3f6c3 section, modver: 0x80a3f6c4 - 0x80a3ffff section, __ex_table: 0x80a40000 - 0x80a414ef section, .notes: 0x80a414f0 - 0x80a4152b section, .sdata2: 0x80a4152c - 0x80a41fff section, .data: 0x80a42000 - 0x80ace93f section, .data..percpu: 0x80acf000 - 0x80acefff section, .init.text: 0x80acf000 - 0x80af55ab section, .init.data: 0x80af55ac - 0x80af8253 section, .init.ivt: 0x80af8254 - 0x80af827b section, .init.setup: 0x80af827c - 0x80af865f section, .initcall.init: 0x80af8660 - 0x80af8aff section, .con_initcall.init: 0x80af8b00 - 0x80af8b03 section, .bss: 0x80af9000 - 0x80b1f3b3 section, .init.ramfs: 0x81000000 - 0x814bd68b 100% 15MB 0.2MB/s 01:20 Setting PC to Program Start Address 0x80000000 Successfully downloaded C:/Users/cfrick/Desktop/quadmxfe_matlab_code/FPGA_image/Quad_MxFE_for_VCU118_2021-04-28/simpleImage.vcu118_quad_ad9081_204c_txmode_11_rxmode_4_revc.strip Info: MicroBlaze #0 (target 3) Running xsct% Info: tcfchan#1 closed xsct%
When connecting the VCU118 USB UART to PC, it typically registers two USB COMx/ttyUSBx ports.
The first one is the connected to the system controller, while the second one is connected to the FPGA and features the serial terminal.
Observe following startup messages:
Ramdisk addr 0x00000000, Compiled-in FDT at 0x8046b89c Linux version 4.19.0-76252-ga6650ce-dirty (michael@mhenneri-D06) (gcc version 7.3.1 20180425 (crosstool-NG 1.20.0)) #1268 Wed Sep 2 14:54:16 CEST 2020 setup_memory: max_mapnr: 0x30000 setup_memory: min_low_pfn: 0x80000 setup_memory: max_low_pfn: 0xb0000 setup_memory: max_pfn: 0xb0000 Zone ranges: DMA [mem 0x0000000080000000-0x00000000afffffff] Normal empty Movable zone start for each node Early memory node ranges node 0: [mem 0x0000000080000000-0x00000000ffffefff] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffefff] On node 0 totalpages: 196608 DMA zone: 1536 pages used for memmap DMA zone: 0 pages reserved DMA zone: 196608 pages, LIFO batch:63 setup_cpuinfo: initialising setup_cpuinfo: Using full CPU PVR support ERROR: Microblaze HW_MUL-different for PVR and DTS wt_msr_noirq pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 pcpu-alloc: [0] 0 Built 1 zonelists, mobility grouping on. Total pages: 195072 Kernel command line: console=ttyUL0,115200 Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 764272K/786432K available (4526K kernel code, 489K rwdata, 4264K rodata, 4906K init, 93K bss, 22160K reserved, 0K cma-reserved) Kernel virtual memory layout: * 0xffffe000..0xfffff000 : fixmap * 0xffffe000..0xffffe000 : early ioremap * 0xb0000000..0xffffe000 : vmalloc & ioremap NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 irq-xilinx: /amba_pl/interrupt-controller@41200000: num_irq=16, edge=0x4f0 /amba_pl/timer@41c00000: irq=1 clocksource: xilinx_clocksource: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns xilinx_timer_shutdown xilinx_timer_set_periodic sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns Calibrating delay loop... 49.35 BogoMIPS (lpj=246784) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) devtmpfs: initialized random: get_random_u32 called from bucket_table_alloc.isra.7+0x1e8/0x218 with crng_init=0 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 256 (order: -1, 3072 bytes) NET: Registered protocol family 16 GPIO line 482 (ADRF5020_CTRL) hogged as output/high GPIO line 428 (GPIO_0 HDL mux mode) hogged as output/high jesd204: created con: id=0, topo=0, link=0, /amba_pl/axi_quad_spi@44a80000/hmc7043@4 <-> /amba_pl/axi-adxcvr-tx@44b60000 jesd204: created con: id=1, topo=0, link=2, /amba_pl/axi_quad_spi@44a80000/hmc7043@4 <-> /amba_pl/axi-adxcvr-rx@44a60000 jesd204: created con: id=2, topo=0, link=0, /amba_pl/axi-adxcvr-tx@44b60000 <-> /amba_pl/axi-jesd204-tx@44b90000 jesd204: created con: id=3, topo=0, link=2, /amba_pl/axi-adxcvr-rx@44a60000 <-> /amba_pl/axi-jesd204-rx@44a90000 jesd204: created con: id=4, topo=0, link=0, /amba_pl/axi-jesd204-tx@44b90000 <-> /amba_pl/axi-ad9081-tx-3@44b10000 jesd204: created con: id=5, topo=0, link=2, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-2@2 <-> /amba_pl/axi_quad_spi@44a70000/ad9081@3 jesd204: created con: id=6, topo=0, link=0, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-2@2 <-> /amba_pl/axi_quad_spi@44a70000/ad9081@3 jesd204: created con: id=7, topo=0, link=2, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-1@1 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-2@2 jesd204: created con: id=8, topo=0, link=0, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-1@1 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-2@2 jesd204: created con: id=9, topo=0, link=2, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-0@0 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-1@1 jesd204: created con: id=10, topo=0, link=0, /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-0@0 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-1@1 jesd204: created con: id=11, topo=0, link=2, /amba_pl/axi-jesd204-rx@44a90000 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-0@0 jesd204: created con: id=12, topo=0, link=0, /amba_pl/axi-ad9081-tx-3@44b10000 <-> /amba_pl/axi_quad_spi@44a70000/axi-ad9081-rx-0@0 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3: JESD204 link[2] transition uninitialized -> initialized jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3: JESD204 link[0] transition uninitialized -> initialized jesd204: found 10 devices and 1 topologies clocksource: Switched to clocksource xilinx_clocksource NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) TCP established hash table entries: 8192 (order: 3, 32768 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes) TCP: Hash tables configured (established 8192 bind 8192) UDP hash table entries: 512 (order: 1, 8192 bytes) UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. random: fast init done Skipping unavailable RESET gpio -2 (reset) workingset: timestamp_bits=30 max_order=18 bucket_order=0 jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) io scheduler mq-deadline registered io scheduler kyber registered Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled 40600000.serial: ttyUL0 at MMIO 0x40600000 (irq = 5, base_baud = 0) is a uartlite console [ttyUL0] enabled brd: module loaded Xilinx SystemACE device driver, major=254 xilinx_spi 44a70000.axi_quad_spi: no CS gpios available xilinx_spi 44a80000.axi_quad_spi: no CS gpios available xilinx_spi 44b80000.axi_quad_spi: no CS gpios available libphy: Fixed MDIO Bus: probed xilinx_axienet 40c00000.ethernet: TX_CSUM 2 xilinx_axienet 40c00000.ethernet: RX_CSUM 2 xilinx_axienet 40c00000.ethernet: missing/invalid xlnx,addrwidth property, using default libphy: Xilinx Axi Ethernet MDIO: probed i2c /dev entries driver i2c i2c-0: Added multiplexed i2c bus 1 at24 2-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write i2c i2c-0: Added multiplexed i2c bus 2 i2c i2c-0: Added multiplexed i2c bus 3 i2c i2c-0: Added multiplexed i2c bus 4 i2c i2c-0: Added multiplexed i2c bus 5 i2c i2c-0: Added multiplexed i2c bus 6 i2c i2c-0: Added multiplexed i2c bus 7 i2c i2c-0: Added multiplexed i2c bus 8 pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548 hmc425a amba_pl:hmc425a: amba_pl:hmc425a supply vcc-supply not found, using dummy regulator hmc425a amba_pl:hmc425a: Linked as a consumer to regulator.0 ad5592r spi2.0: Linked as a consumer to regulator.1 jesd204: /amba_pl/axi_quad_spi@44a80000/hmc7043@4,jesd204:4,parent=spi1.4: Using as SYSREF provider axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTY4 at 0x44A60000 mapped to 0x(ptrval). Number of lanes: 16. axi_adxcvr 44b60000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTY4 at 0x44B60000 mapped to 0x(ptrval). Number of lanes: 16. axi_sysid 45000000.axi-sysid-0: [ad] on [quadmxfe1] git <77ed1ee52339171167922d2a3f64372ce9eed601> clean [2020-07-30 15:54:12] UTC NET: Registered protocol family 17 ad9081 spi0.0: AD9081 Rev. 3 Grade 10 (API 1.0.5) probed ad9081 spi0.1: AD9081 Rev. 3 Grade 10 (API 1.0.5) probed ad9081 spi0.2: AD9081 Rev. 3 Grade 10 (API 1.0.5) probed ad9081 spi0.3: AD9081 Rev. 3 Grade 10 (API 1.0.5) probed iio_dmaengine_buffer_alloc:227 width 0 (DMA width >= 256-bits ?) cf_axi_dds 44b10000.axi-ad9081-tx-3: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44B10000 mapped to 0x(ptrval), probed DDS AD9081 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition initialized -> probed jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition initialized -> probed jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition probed -> idle jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition probed -> idle jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition idle -> device_init jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition idle -> device_init jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition device_init -> link_init jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition device_init -> link_init jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_init -> link_supported jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_init -> link_supported jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_supported -> link_pre_setup jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_supported -> link_pre_setup jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_pre_setup -> clk_sync_stage1 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_pre_setup -> clk_sync_stage1 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition clk_sync_stage1 -> clk_sync_stage2 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition clk_sync_stage1 -> clk_sync_stage2 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition clk_sync_stage2 -> clk_sync_stage3 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition clk_sync_stage2 -> clk_sync_stage3 jesd204: /amba_pl/axi-jesd204-rx@44a90000,jesd204:6,parent=44a90000.axi-jesd204-rx: Possible instantiation for multiple chips; HDL lanes 16, Link[2] lanes 4 jesd204: /amba_pl/axi-jesd204-tx@44b90000,jesd204:7,parent=44b90000.axi-jesd204-tx: Possible instantiation for multiple chips; HDL lanes 16, Link[0] lanes 4 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition clk_sync_stage3 -> link_setup jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition clk_sync_stage3 -> link_setup random: crng init done jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_setup -> opt_setup_stage1 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_setup -> opt_setup_stage1 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition opt_setup_stage1 -> opt_setup_stage2 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition opt_setup_stage1 -> opt_setup_stage2 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition opt_setup_stage2 -> opt_setup_stage3 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition opt_setup_stage2 -> opt_setup_stage3 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition opt_setup_stage3 -> opt_setup_stage4 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition opt_setup_stage3 -> opt_setup_stage4 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition opt_setup_stage4 -> opt_setup_stage5 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition opt_setup_stage4 -> opt_setup_stage5 jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition opt_setup_stage5 -> clocks_enable jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition opt_setup_stage5 -> clocks_enable jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition clocks_enable -> link_enable jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition clocks_enable -> link_enable ad9081 spi0.0: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.0: JESD TX (JRX) Link1 0xF lanes in DATA ad9081 spi0.1: JESD RX (JTX) Link1 in DATA, SYNC asserted, PLL locked, PHASE established, MODE valid ad9081 spi0.1: JESD TX (JRX) Link1 0xF lanes in DATA ad9081 spi0.2: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.2: JESD TX (JRX) Link1 0xF lanes in DATA ad9081 spi0.3: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.3: JESD TX (JRX) Link1 0xF lanes in DATA jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_enable -> link_running jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_enable -> link_running jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[2] transition link_running -> opt_post_running_stage jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@3,jesd204:3,parent=spi0.3: JESD204 link[0] transition link_running -> opt_post_running_stage iio_dmaengine_buffer_alloc:227 width 0 (DMA width >= 256-bits ?) cf_axi_adc 44a10000.axi-ad9081-rx-3: ADI AIM (10.01.b) at 0x44A10000 mapped to 0x80242c2b, probed ADC AD9081 as MASTER Freeing unused kernel memory: 4904K This architecture does not have kernel memory protection. Run /init as init process Starting syslogd: OK Starting klogd: OK Initializing random number generator... done. Starting network: udhcpc: started, v1.29.3 net eth0: Promiscuous mode disabled. net eth0: Promiscuous mode disabled. udhcpc: sending discover xilinx_axienet 40c00000.ethernet eth0: Link is Down xilinx_axienet 40c00000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx udhcpc: sending discover udhcpc: sending discover udhcpc: sending select for 10.44.3.52 udhcpc: lease of 10.44.3.52 obtained, lease time 43200 deleting routers adding dns 10.32.51.110 adding dns 10.64.53.110 Starting dropbear sshd: OK Starting IIO Server Daemon Welcome to Buildroot buildroot login:
Login: | root |
Password: | analog |
When the system starts it tries to acquire an IP using the DHCP protocol.
In case it fails DHCP it will configure a static IP address of 192.168.2.1
This specifies any shell prompt running on the target
# ifconfig eth0 Link encap:Ethernet HWaddr 00:0A:35:00:00:00 inet addr:10.44.3.93 Bcast:10.44.3.255 Mask:255.255.255.0 UP BROADCAST RUNNING MTU:1500 Metric:1 RX packets:418 errors:0 dropped:32 overruns:0 frame:0 TX packets:2 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:31911 (31.1 KiB) TX bytes:684 (684.0 B) #
This specifies any shell prompt running on the target
#resize #jesd_status -s
This specifies any shell prompt running on a remote PC
dave@hal9000:~$ slogin root@10.44.3.93 The authenticity of host '10.44.3.93 (10.44.3.93)' can't be established. ECDSA key fingerprint is SHA256:0AcYkl+45GBw+Fg5/oxbrh5No1UYXgkpNoLSYlrEjqs. Are you sure you want to continue connecting (yes/no)? yes Warning: Permanently added '10.44.3.93' (ECDSA) to the list of known hosts. root@10.44.3.93's password: # #resize #jesd_status
There are a few command line tools that are included with the libIIO.
When using remote backend please install libiio for your platform.
iio_info
and iio_attr
, iio_reg
requires an environmental variable IIOD_REMOTE
to be set with the target IP address.
The names of the iio devices can be obtained using iio_attr
command.
Example: Change main NCO frequency
This specifies a system console
C:\Users\dave>iio_attr -u ip:10.44.3.56 -i -c axi-ad9081-rx-3 voltage0_i main_nco_frequency 1200000000 dev 'axi-ad9081-rx-3', channel 'voltage0_i' (input), attr 'main_nco_frequency', value '1000000000' wrote 11 bytes to main_nco_frequency dev 'axi-ad9081-rx-3', channel 'voltage0_i' (input), attr 'main_nco_frequency', value '1200000000' C:\Users\dave>
Further information about libiio and it's usage can be found here:
Weblinks:
IIO Device | Device Name | Driver Documentation |
---|---|---|
iio:device0 | hmc425a | HMC425A Digital Step Attenuator Linux Driver |
iio:device1 | adf4371-0 | ADF4371 IIO Wideband Synthesizer Linux Driver |
iio:device2 | adf4371-1 | ADF4371 IIO Wideband Synthesizer Linux Driver |
iio:device3 | adf4371-2 | ADF4371 IIO Wideband Synthesizer Linux Driver |
iio:device4 | adf4371-3 | ADF4371 IIO Wideband Synthesizer Linux Driver |
iio:device5 | hmc7043 | HMC7044 Clock Jitter Attenuator with JESD204B Linux Driver |
iio:device6 | axi-ad9081-rx-0 | |
iio:device7 | axi-ad9081-rx-1 | |
iio:device8 | axi-ad9081-rx-2 | |
iio:device9 | axi-ad9081-tx-3 | AXI DAC HDL Linux Driver |
iio:device10 | axi-ad9081-rx-3 |
All these drivers feature a runtime API which can be controlled using IIO Oscilloscope, libiio, etc. However some configuration is static and done inside the device tree. For Microblaze projects (VCU118) the device tree is build into the kernel image. Please see instructions on Building custom kernel and devicetree images here:
IIO device axi-ad9081-rx-3
is special compared to the axi-ad9081-rx-[0..2]
, since it
controls the transport layer and therefore features the IIO buffer.
So all 16R data captures are controlled via this device, while
the other similar devices are there, to control the device instance specific controls.
Also axi-ad9081-rx-3
aka. spi0.3
instantiates last, it therefore brings up the JESD204 multi-link.
ad9081 spi0.0: JESD RX (JTX) Link1 in DATA, SYNC asserted, PLL locked, PHASE established, MODE valid ad9081 spi0.0: JESD TX (JRX) Link1 0x0 lanes in DATA ad9081 spi0.0: AD9081 Rev. 1 Grade 10 (API 0.7.4) probed ad9081 spi0.1: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.1: JESD TX (JRX) Link1 0x0 lanes in DATA ad9081 spi0.1: AD9081 Rev. 1 Grade 10 (API 0.7.4) probed ad9081 spi0.2: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.2: JESD TX (JRX) Link1 0x0 lanes in DATA ad9081 spi0.2: AD9081 Rev. 1 Grade 10 (API 0.7.4) probed ad9081 spi0.3: JESD RX (JTX) Link1 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid ad9081 spi0.3: JESD TX (JRX) Link1 0xF lanes in DATA ad9081 spi0.3: AD9081 Rev. 1 Grade 10 (API 0.7.4) probed
It's expected that JRX, JTX status information may contain error status until the last device probes and
the Link is finally enabled. Device axi-ad9081-tx-3
purely controls the TX transport layer, it therefore doesn't have any MxFE controls. Please use the iio_info command to get an overview on what controls and capabilities exists.
The ADI IIO Oscilloscope is a cross platform GUI application, which demonstrates how to interface different evaluation boards from within a Linux system. The application supports plotting of the captured data in four different modes (time domain, frequency domain, constellation and cross-correlation). The application also allows to view and modify several settings of the development platform's devices.
Documentation can be found here:
The MxFE AD9081 plugin is included in the official OSC release, which can be downloaded from here:
OSC
.Remote Devices
and press the Refresh
followed by the Ok
button.
Device To Channel Mapping (Rev. B/C Platforms):
axi-ad9081-rx-0: spi.0.0 - MxFE U48 voltage0_i: (input, index: 0, format: le:S16/16>>0) voltage0_q: (input, index: 1, format: le:S16/16>>0) voltage1_i: (input, index: 2, format: le:S16/16>>0) voltage1_q: (input, index: 3, format: le:S16/16>>0) voltage2_i: (input, index: 4, format: le:S16/16>>0) voltage2_q: (input, index: 5, format: le:S16/16>>0) voltage3_i: (input, index: 6, format: le:S16/16>>0) voltage3_q: (input, index: 7, format: le:S16/16>>0) axi-ad9081-rx-1: spi.0.1 - MxFE U49 voltage4_i: (input, index: 8, format: le:S16/16>>0) voltage4_q: (input, index: 9, format: le:S16/16>>0) voltage5_i: (input, index: 10, format: le:S16/16>>0) voltage5_q: (input, index: 11, format: le:S16/16>>0) voltage6_i: (input, index: 12, format: le:S16/16>>0) voltage6_q: (input, index: 13, format: le:S16/16>>0) voltage7_i: (input, index: 14, format: le:S16/16>>0) voltage7_q: (input, index: 15, format: le:S16/16>>0) axi-ad9081-rx-2: spi.0.2 - MxFE U61 voltage8_i: (input, index: 16, format: le:S16/16>>0) voltage8_q: (input, index: 17, format: le:S16/16>>0) voltage9_i: (input, index: 18, format: le:S16/16>>0) voltage9_q: (input, index: 19, format: le:S16/16>>0) voltage10_i: (input, index: 20, format: le:S16/16>>0) voltage10_q: (input, index: 21, format: le:S16/16>>0) voltage11_i: (input, index: 22, format: le:S16/16>>0) voltage11_q: (input, index: 23, format: le:S16/16>>0) axi-ad9081-rx-3: spi.0.3 - MxFE U76 voltage12_i: (input, index: 24, format: le:S16/16>>0) voltage12_q: (input, index: 25, format: le:S16/16>>0) voltage13_i: (input, index: 26, format: le:S16/16>>0) voltage13_q: (input, index: 27, format: le:S16/16>>0) voltage14_i: (input, index: 28, format: le:S16/16>>0) voltage14_q: (input, index: 29, format: le:S16/16>>0) voltage15_i: (input, index: 30, format: le:S16/16>>0) voltage15_q: (input, index: 31, format: le:S16/16>>0) voltage15_q: (input, index: 31, format: le:S16/16>>0)
And not more that 2 frequency plots can be enabled in the same window.
However multiple (independent) plot windows can be opened.
OSC will instantiate multiple notebook plugin tabs on the main window. One for each device AD9081-X
with an additional Debug plugin.
AD9081-3
again is special since it also has the controls for the TX transport layer core (axi-ad9081-tx-3
), and the HMC425
Digital Step Attenuator.
Set DDS mode to DAC Buffer Output
, select a file hit Load
button.
Optionally set a scale, and select the channels.
Under Device Selection
, select the IIO device which should be debugged/controlled.
In the IIO Device Attribute
section, all device and channel attributes can be read or written,
including all attributes which are not handled by the AD9081-X
device plugin itself.
In the Register
section select source SPI
, check Detailed Register Map
and AutoRead
, this will enable a complete AD9081 register view with description bitfields and dropdown options if available.
IIO devices axi-ad9081-tx-3
and axi-ad9081-rx-3
are again special, since beside the SPI option they also can access the AXI_CORE register space of the transport layer core.
MATLAB support is provided through the High Speed Converter Toolbox, with unique classes for transmit and receive functionality. Currently you must grab a development build but installers are provided for convenience.
To install the toolbox perform the follow:
More information on controlling the Quad-MxFE Platform with MATLAB can be found at: