iio_readdev
is part of the Libiio package, a library that has been developed to ease the development of software interfacing Linux Industrial I/O (IIO) devices. There are four main userspace helper/utilities:
analog@imhotep:~$ iio_readdev -h Usage: iio_readdev [-n <hostname>] [-t <trigger>] [-T <timeout-ms>] [-b <buffer-size>] [-s <samples>] <iio_device> [<channel> ...] Options: -h, --help Show this help and quit. -n, --network Use the network backend with the provided hostname. -u, --uri Use the context with the provided URI. -t, --trigger Use the specified trigger. -b, --buffer-size Size of the capture buffer. Default is 256. -s, --samples Number of samples to capture, 0 = infinite. Default is 0. -T, --timeout Buffer timeout in milliseconds. 0 = no timeout -a, --auto Scan for available contexts and if only one is available use it.
a quick example, captures 4 frames of 256 samples, (1024 samples in total), from the receive side of the ADALM-PLUTO.
analog@imhotep:~/github/libiio/build$ iio_info -s Library version: 0.9 (git tag: 263bd08) Compiled with backends: local xml ip usb serial Available contexts: 0: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=104473222a87000c0a000e009b8ed5102e [usb:3.80.5]
analog@imhotep:~$ iio_attr -u usb:3.80.5 -s -c *ad* dev 'cf-ad9361-dds-core-lpc', channel 'voltage0' (output, index: 0, format: le:S16/16>>0) dev 'cf-ad9361-dds-core-lpc', channel 'voltage1' (output, index: 1, format: le:S16/16>>0) dev 'cf-ad9361-lpc', channel 'voltage0' (input, index: 0, format: le:S12/16>>0) dev 'cf-ad9361-lpc', channel 'voltage1' (input, index: 1, format: le:S12/16>>0)In this case (which happens to use the ADALM-PLUTO, it is
cf-ad9361-lpc
for the input (rx), and cf-ad9361-dds-core-lpc
for the output.analog@imhotep:~$ iio_attr -u usb:3.80.5 -D ad9361-phy loopback 1 dev 'ad9361-phy', debug attr 'loopback', value :'0' wrote 2 bytes to loopback dev 'ad9361-phy', debug attr 'loopback', value :'1'
analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage0 frequency 50000 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage0' (output), id 'TX1_I_F1', attr 'frequency', value '9279985' wrote 5 bytes to frequency dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage0' (output), id 'TX1_I_F1', attr 'frequency', value '50034' analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage2 frequency 50000 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage2' (output), id 'TX1_I_F2', attr 'frequency', value '9279985' wrote 5 bytes to frequency dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage2' (output), id 'TX1_I_F2', attr 'frequency', value '50034'
analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage0 scale 0.4 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage0' (output), id 'TX1_I_F1', attr 'scale', value '0.000000' wrote 4 bytes to scale dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage0' (output), id 'TX1_I_F1', attr 'scale', value '0.400024' analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage1 scale 0.0 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage1' (output), id 'TX1_I_F2', attr 'scale', value '0.000000' wrote 4 bytes to scale dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage1' (output), id 'TX1_I_F2', attr 'scale', value '0.000000' analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage2 scale 0.4 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage2' (output), id 'TX1_I_F2', attr 'scale', value '0.000000' wrote 4 bytes to scale dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage2' (output), id 'TX1_I_F2', attr 'scale', value '0.400024' analog@imhotep:~$ iio_attr -a -c cf-ad9361-dds-core-lpc altvoltage3 scale 0.0 Using auto-detected IIO context at URI "usb:2.26.5" dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage3' (output), id 'TX1_I_F2', attr 'scale', value '0.000000' wrote 4 bytes to scale dev 'cf-ad9361-dds-core-lpc', channel 'altvoltage3' (output), id 'TX1_I_F2', attr 'scale', value '0.000000'
analog@imhotep:~$ iio_attr -a -i -c ad9361-phy voltage0 sampling_frequency 3000000 Using auto-detected IIO context at URI "usb:2.29.5" dev 'ad9361-phy', channel 'voltage0' (input), attr 'sampling_frequency', value '3000000' wrote 8 bytes to sampling_frequency dev 'ad9361-phy', channel 'voltage0' (input), attr 'sampling_frequency', value '3000000'
analog@imhotep:~$ iio_readdev -u usb:3.80.5 -b 256 -s 1024 cf-ad9361-lpc > samples.dat
hexdump
:analog@imhotep:~$ hexdump -d ./samples.dat | less 0000000 64086 65499 64097 65352 64124 65206 64165 65064 0000010 64220 64926 64289 64794 64371 64670 64466 64555 0000020 64572 64451 64688 64358 64813 64278 64946 64211 0000030 65085 64158 65228 64119 65374 64095 65520 64086 0000040 00131 64092 00277 64113 00421 64148 00561 64199 0000050 00695 64263 00822 64341 00940 64431 01048 64533 0000060 01145 64646 01230 64768 01302 64898 01360 65035 0000070 01404 65177 01433 65322 01448 65468 01447 00079 0000080 01431 00225 01401 00370 01356 00512 01296 00648
analog@imhotep:~$ iio_attr -a -i -c ad9361-phy voltage0 sampling_frequency dev 'ad9361-phy', channel 'voltage0' (input), attr 'sampling_frequency', value '30720000'You can expect that 30.72 MSPS is too fast to stream over USB with zero gaps between buffers. Increasing the buffer length is the best thing to do.