iio_attr
is part of the Libiio package, a library that has been developed to ease the development of software interfacing Linux Industrial I/O (IIO) devices. There are four main userspace helper/utilities:
analog@imhotep:~$ iio_attr -h Usage: iio_attr [OPTION]... -d [device] [attr] [value] -c [device] [channel] [attr] [value] -B [device] [attr] [value] -D [device] [attr] [value] -C [attr] Options: -h, --help : Show this help and quit. -I, --ignore-case : Ignore case distinctions. -q, --quiet : Return result only. -a, --auto : Use the first context found. Optional qualifiers: -u, --uri : Use the context at the provided URI. -i, --input-channel : Filter Input Channels only. -o, --output-channel : Filter Output Channels only. Attribute types: -s, --scan-channel : Filter Scan Channels only. -d, --device-attr : Read/Write device attributes -c, --channel-attr : Read/Write channel attributes. -C, --context-attr : Read IIO context attributes. -B, --buffer-attr : Read/Write buffer attributes. -D, --debug-attr : Read/Write debug attributes.
rgetz@brain:~/github/libiio$ iio_attr -a -C Using auto-detected IIO context at URI "usb:3.8.5" IIO context with 14 attributes: hw_model: Analog Devices PlutoSDR Rev.B (Z7010-AD9364) hw_model_variant: 0 hw_serial: 104473222a87000618000600473ed57ae0 fw_version: v0.31 ad9361-phy,xo_correction: 40000000 ad9361-phy,model: ad9364 local,kernel: 4.14.0-42540-g387d584 usb,idVendor: 0456 usb,idProduct: b673 usb,release: 2.0 usb,vendor: Analog Devices Inc. usb,product: PlutoSDR (ADALM-PLUTO) usb,serial: 104473222a87000618000600473ed57ae0 usb,libusb: 1.0.22.11312
rgetz@brain:~/github/libiio$ iio_attr -u usb:3.8.5 -d IIO context has 5 devices: iio:device0: adm1177, found 0 device attributes iio:device1: ad9361-phy, found 18 device attributes iio:device2: xadc, found 1 device attributes iio:device3: cf-ad9361-dds-core-lpc, found 0 device attributes iio:device4: cf-ad9361-lpc, found 0 device attributes
rgetz@brain:~/github/libiio$ iio_attr -u usb:3.8.5 -c IIO context has 5 devices: iio:device0: adm1177, found 2 channels iio:device1: ad9361-phy, found 9 channels iio:device2: xadc, found 10 channels iio:device3: cf-ad9361-dds-core-lpc, found 6 channels iio:device4: cf-ad9361-lpc, found 2 channels
the .
can be used as a wildcard if you don't know the name.
rgetz@brain:~/github/libiio$ iio_attr -u ip:192.168.2.1 -c adm1177 . dev 'adm1177', channel 'voltage0' (input), attr 'raw', value '771' dev 'adm1177', channel 'voltage0' (input), attr 'scale', value '6.433105468' dev 'adm1177', channel 'current0' (input), attr 'raw', value '776' dev 'adm1177', channel 'current0' (input), attr 'scale', value '0.516601562'
rgetz@brain:~/github/libiio$ iio_attr -u ip:192.168.2.1 -c ad9361-phy RX_LO dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'external', value '0' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'fastlock_load', value '0' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'fastlock_recall', ERROR: Invalid argument (-22) dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'fastlock_save', value '0 242,198,163,125,228,163,171,195,167,187,179,163,241,167,187,167' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'fastlock_store', value '0' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency', value '2400000000' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency_available', value '[70000000 1 6000000000]' dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'powerdown', value '0'
rgetz@brain:~/github/libiio$ iio_attr -u ip:192.168.2.1 -c ad9361-phy RX_LO frequency dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency', value '2400000000'
rgetz@brain:~/github/libiio$ iio_attr -u ip:192.168.2.1 -c ad9361-phy RX_LO frequency 2400000100 dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency', value '2400000000' wrote 11 bytes to frequency dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency', value '2400000100'