Wiki

This version (09 Nov 2016 21:31) was approved by Brandon Bushey.The Previously approved version (10 Mar 2016 21:25) is available.Diff

Hardware

This chapter contains hardware-related information about the base board and the various shields. Each sub-section contains a general description of the board, detailed description of the connectors, jumpers, and buttons (if any). It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects.

The following boards are currently available:

Navigation - EVAL-ADICUP360

resources/eval/user-guides/eval-adicup360/hardware.txt · Last modified: 09 Nov 2016 21:31 by Brandon Bushey