The EVAL-ADICUP360 base board consists of two basic blocks:
This page describes the hardware connectors, the jumpers and switches configuration options, the USB connectors, and links to download the schematics and the layout.
The following connectors are populated on the base board:
Connector | Pin No. | Pin Name | ADuCM360 pin or other function | Arduino Due Pin Name |
---|---|---|---|---|
PWMH | 10 | SCL | P2.0/SCL/UARTCLK | SCL1 |
9 | SDA | P2.1/SDA/UARTDCD | SDA1 | |
8 | AREF | VREF+ | AREF | |
7 | GND | AGND (Analog ground) | GND | |
6 | SCK | P0.1/SCLK1/SCL/SIN | PWM13 | |
5 | MISO | P0.0/MISO1 | PWM12 | |
4 | MOSI | P0.2/MOSI1/SDA/SOUT | PWM11 | |
3 | SS | P0.3/IRQ0/CS1 | PWM10 | |
2 | P0.4 | P0.4/RTS/ECLKO | PWM9 | |
1 | P0.5 | P0.5/CTS/IRQ1 | PWM8 | |
PWML | 8 | PWM5 | P2.2/BM | PWM7 |
7 | PWM4 | P1.4/PWM2/MISO0 | PWM6 | |
6 | PWM3 | P1.3/PWM1/DSR | PWM | |
5 | PWM2 | P1.2/PWM0/RI | PWM4 | |
4 | PWM1 | P1.1/IRQ4/PWMTRIP/DTR | PWM3 | |
3 | PWM0 | P1.0/IRQ3/PWMSYNC/EXTCLK | PWM2 | |
2 | TX | P0.7/POR/SOUT | TX0 | |
1 | RX | P0.6/IRQ2/SIN | RX0 | |
COMMUNICATION | 8 | P0.2 | P0.2/MOSI1/SDA/SOUT | TX3 |
7 | P0.1 | P0.1/SCLK1/SCL/SIN | RX3 | |
6 | P1.7 | P1.7/IRQ7/PWM5/CS0 | TX2 | |
5 | P1.6 | P1.6/IRQ6/PWM4/MOSI0 | RX2 | |
4 | P1.5 | P1.5/IRQ4/PWM3/SCLK0 | TX1 | |
3 | P1.4 | P1.4/PWM2/MISO0 | RX1 | |
2 | SDA | P2.1/SDA/UARTDCD | SDA | |
1 | SCL | P2.0/SCL/UARTCLK | SCL | |
ADCH | 1 | A8 | AIN8/EXTREF2IN- | A8 |
2 | A9 | AIN9/DACBUFF+ | A9 | |
3 | A10 | AIN10 | A10 | |
4 | A11 | AIN11/VBIAS1 | A11 | |
5 | DAC | DAC | DAC0 | |
6 | G_SW | GND_SW | DAC1 | |
7 | VREF+ | VREF+ | CANRX | |
8 | VREF- | VREF- | CANTX | |
ADCL | 1 | A0 | AIN0 | A0 |
2 | A1 | AIN1 | A1 | |
3 | A2 | AIN2 | A2 | |
4 | A3 | AIN3 | A3 | |
5 | A4 | AIN4/IEXC | A4 | |
6 | A5 | AIN5/IEXC | A5 | |
7 | A6 | AIN5/IEXC | A6 | |
8 | A7 | AIN7/VBIAS0/IEXC/EXTREF2IN+ | A7 | |
POWER | 1 | NC | - not connected - | NOT USED |
2 | IOREF | DVdd (+3.3V) | IOREF | |
3 | RESET | RESET | RESET | |
4 | 3.3V | DVdd (+3.3V) | 3V3 | |
5 | 5V | +5V | 5V | |
6 | GND | DGND (Digital Ground) | GND | |
7 | GND | DGND (Digital Ground) | GND | |
8 | Vin | The input line of the +5V linear voltage regulator | VIN | |
SPI | 1 | MISO | P0.0 | MISO |
2 | +5 | +5 | +5 | |
3 | SCLK | P0.1 | SCLK | |
4 | MOSI | P0.2 | MOSI | |
5 | RESET | RESET | RESET | |
6 | GND | DGND | GND | |
SPI_PMOD | 1 | CS | P1.7 | CHIP SELECT |
2 | MOSI | P1.6 | MOSI | |
3 | MISO | P1.4 | MISO | |
4 | SCLK | P1.5 | SCLK | |
5 | GND | DGND | GND | |
6 | VDD | DVDD | VDD | |
7 | INT | P1.0 | INT | |
8 | RESET | P1.1 | RESET | |
9 | GPIO | P1.2 | GPIO | |
10 | GPIO | P2.2 | GPIO | |
11 | GND | DGND | GND | |
12 | VDD | DVDD | VDD | |
I2C_PMOD | 1 | SCL | P2.0 | SCL |
2 | SCL | P2.0 | SCL | |
3 | SDA | P2.1 | SDA | |
4 | SDA | P2.1 | SDA | |
5 | GND | DGND | GND | |
6 | GND | DGND | GND | |
7 | VDD | DVDD | VDD | |
8 | VDD | DVDD | VDD |
There are 4 switches on the EVAL-ADICUP360 base board, which are used to multiplex pairs of pins (P0.1/P0.2, and P0.6/P0.7) to various different connectors on the board. Depending on how the pins are configured you may route them to the USB ports, use them for SPI communication or for UART communication.
The S1, S2, S3, S4 switches are used to route the P0.1/SCLK1/SCL/SIN, P0.2/MOSI1/SDA/SOUT, P0.6/IRQ2/SIN and P0.7/POR/SOUT pins when they have been assigned a UART function to either the Arduino I/O and the PMOD connectors or to the Virtual Serial ports implemented via the USER USB or the DEBUG USB connectors. Each pin can be routed separately, but the routing is usually done for the pairs TxD/RxD.
Most commonly used configurations are given in the table below. For any other more 'exotic' configuration, consult with the Schematics and the Layout of the board.
Here is the schematic of the switching network, the switches allow to route the P0.1/P0.2 and P0.6/P0.7 signals to multiple connector depending how you want to configure the pins. Above are the common configurations, but for complete details please reference the diagram.
The EVAL-ADICUP360 base board provides two buttons RESET and BOOT.
Button | Function |
---|---|
RESET | Provides a hardware RESET to ADuCM360 microcontroller. If the RESET line is connected to the Debug adapter, this button can be used to invoke the Debug adapter's Bootloader, see section Jumper Configuration. |
BOOT | When BOOT is held down during the reset and after, the ADuCM360 microcontroller enters UART download mode via P0.1 and P0.2. In this case, the user can download program via DEBUG USB or USER USB, depending on the jumpers settings, see section Jumper Configuration. BOOT button should be held press while a reset from the button is performed. |
EVAL-ADICUP360 Design and Integration Files