Wiki

This version (23 Jan 2018 16:13) was approved by Brandon.The Previously approved version (03 Aug 2017 18:20) is available.Diff

EVAL-CN0357-ARDZ Shield

CN0357 single-supply, low noise, portable gas detector circuit using an electrochemical sensor. The Alphasense CO-AX carbon monoxide sensor is used in this example. Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration.

The circuit shown in below uses the ADA4528-2, dual auto zero amplifier, which has a maximum offset voltage of 2.5 µV at room temperature and an industry leading 5.6 µV/√Hz of voltage noise density. In addition, the AD5270-20 programmable rheostat is used rather than a fixed transimpedance resistor, allowing for rapid prototyping of different gas sensor systems, without changing the bill of materials. The ADR3412 precision, low noise, micropower reference establishes the 1.2 V common-mode, pseudo ground reference voltage with 0.1% accuracy and 8 ppm/°C drift. For applications where measuring fractions of ppm gas concentration is important, using the ADA4528-2 and the ADR3412 makes the circuit performance suitable for interfacing with a 16-bit ADC, such as the AD7790.



Connectors and Jumper Configurations


Sensor Footprint


NOTE - Three electrode electrochemical toxic gas sensors can be used with the EVAL-CN0357-ARDZ The footprint can accommodate 3 different sizes of sensors.
The Alphasense CO-AX electrochemical gas sensor was used during testing and programming.

Recommended PCB Sockets(for Alphasense Sensors)

  • A Series Sensors - Mill-Max 0364-0-15-15-13-27-10-0
  • B Series Sensors - Mill-Max 0294-0-15-15-06-27-10-0
  • D Series Sensors - Mill-Max 0667-0-15-15-30-27-10-0
  • The sensor may be connected to the M1 footprint using the appropriate pin sockets

Jumper P1 Settings

  • “0” position - Sensor output connected to ADC(defualt)
  • “1” position - Sensor output connected to A1 pin of ANALOG header, for connection to external ADCs


Chip Select

This set of jumpers allows for changing the pin mapping of the AD7790 and AD5270 chip select lines to different Arduino digital pins. Place jumper/shunt as shown to connect to the corresponding Digital IO pin.

AD7790 CS Selection

Pin 1 shunted to Pin 2
CS connected to Digital Pin 10


Pin 3 shunted to Pin 4
CS connected to Digital Pin 9


Pin 5 shunted to Pin 6
CS connected to Digital Pin 8



AD5270 CS Selection

Pin 1 shunted to Pin 2
CS connected to Digital Pin 7


Pin 3 shunted to Pin 4
CS connected to Digital Pin 6


Pin 5 shunted to Pin 6
CS connected to Digital Pin 5


Software

Schematic, Bill of Materials, Gerber Files, Layout Files

Change Log

RevB to RevC:

  • Replaced R15,R16,R17,R19 and R20 to headers AD7790_CS and AD5270_CS for CS line selection
  • Connected ICSP SPI lines MOSI,MISO and SCLK to DIGI1 headers(arduino pins D11,D12 and D13) respectively
  • No longer need external 7V to 12V wall power supply
    • Board Powered through 5V pin (Arduino POWER header)

End of Document

resources/eval/user-guides/eval-adicup360/hardware/cn0357.txt · Last modified: 23 Jan 2018 16:13 by Brandon