The EVAL-ADICUP360 is an Arduino-like platform based on the ADUCM360 fully integrated, 3.9 kSPS, 24-bit data acquisition system that incorporates dual high performance, multichannel sigma-delta (Σ-Δ) analog-to-digital converters (ADCs), a 32-bit ARM Cortex™-M3 processor, and Flash/EE memory on a single chip. The platform has an Arduino-Due form factor and has two additional PMOD connectors. An Eclipse based development environment is provided for code development and debugging. The base platform is accompanied by a set of shields provided by Analog Devices but it can also work with 3rd party Aduino shields.
This guide is structured as follows: