Wiki

This version is outdated by a newer approved version.DiffThis version (02 Dec 2016 15:54) was approved by Brandon Bushey.The Previously approved version (28 Sep 2016 09:34) is available.Diff

This is an old revision of the document!


EVAL-CN0216-ARDZ Shield

CN-0216 is a precision weigh scale signal conditioning system. It uses the AD7791, a low power buffered 24-bit sigma-delta ADC along with dual external ADA4528-2 zero-drift amplifiers. This solution allows for high dc gain with a single supply.

Ultralow noise, low offset voltage, and low drift amplifiers are used at the front end for amplification of the low-level signal from the load cell. The circuit yields 15.3 bit noise-free code resolution for a load cell with a full-scale output of 10 mV.

This circuit allows great flexibility in designing a custom low-level signal conditioning front end that gives the user the ability to easily optimize the overall transfer function of the combined sensor-amplifier-converter circuit. The AD7791 maintains good performance over the complete output data range, from 9.5 Hz to 120 Hz, which allows it to be used in weigh scale applications that operate at various low speeds.





Extremely important to note that the EVAL-CN0216-ARDZ is powered from the VIN connector on the Arduino Uno header. This is because the bridge drive voltage of the EVAL-CN0216-ARDZ requires more than 5V to power the bridge. Therefore it is required to supply power from the baseboard through the DC power connector in order for proper functionality. The board will not work properly if you try only to power it from the USB.

Connectors and Jumper Configurations


Sensor Connector

Pin NumberPin Function
Pin 1Not Used
Pin 2- Excitation
Pin 3+ Signal
Pin 4- Sense
Pin 5+ Sense
Pin 6- Signal
Pin 7+ Excitation
Pin 8Not Used



REF SEL / Bridge Configuration

These set of jumpers allow the circuit to be configured for use with 4-wire or 6-wire load cells.


NOTE - Any 4 or 6 wire load cells can be used with the EVAL-CN0216-ARDZ.
The Tedeah Huntleigh Model 1042 load cell was used during testing.


Place jumpers/shunts as shown above for 6-wire resistive bridge configuration

  • P1 - Connects ADC REFIN+ to Sensor +Sense pin
  • P2 - Connects ADC REFIN- to Sensor -Sense pin



Place jumpers/shunts as shown above for 4-wire resistive bridge configuration

  • P1 - Connects ADC REFIN+ to 5V supply
  • P2 - Connects ADC REFIN- to GND


Chip Select

This set of jumpers allows for changing the pin mapping of the AD7791 chip select line to different Arduino digital pins. Place jumper/shunt as shown to connect to the corresponding Digital IO pin
CS - Arduino Digital Pin 10
CS - Arduino Digital Pin 9
CS - Arduino Digital Pin 8

If using an EVAL-CN0216-ARDZ board prior to Rev.C:
To change the CS pin, Install a 0-ohm resistor to resistor pads R7,R8 or R9

  • R7 - Arduino Digital Pin 8
  • R8 - Arduino Digital Pin 9
  • R9 - Arduino Digital Pin 10

Schematic, Bill of Materials, Gerber Files, Layout Files

Change Log

RevB to RevC:

  • U3 (from ADG3304BRUZ to NLSX4402FMUTCG)
  • U4 added (NLSX4402FMUTCG)
  • C19 and C20 added (0.1uF)
  • R7, R8, R9 added to short MOSI, MISO, SCLK lines between ICSP and arduino D11, D12, D13
  • AD7791_CS header added

Software

Navigation - EVAL-ADICUP360

resources/eval/user-guides/eval-adicup360/hardware/cn0216.1479572691.txt.gz · Last modified: 19 Nov 2016 17:24 by Jordan Lucht