This chapter contains hardware-related information about the EVAL-ADICUP3029 base board and the various hardware add on modules which can be used with the base board. Each sub-section contains a general description of the board, detailed description of the connectors, jumpers, and buttons (if any). It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects.
The following boards are currently available: