Wiki

This version is outdated by a newer approved version.DiffThis version (24 May 2017 19:27) was approved by Brandon Bushey.The Previously approved version (22 May 2017 15:51) is available.Diff

This is an old revision of the document!


Hardware

This chapter contains hardware-related information about the EVAL-ADICUP3029 base board and the various hardware add on modules which can be used with the base board. Each sub-section contains a general description of the board, detailed description of the connectors, jumpers, and buttons (if any). It also provides links to the Schematics, Bill of materials, design projects, and Technical documentation. It also gives internal links to the provided example demo software projects.

The following boards are currently available:

resources/eval/user-guides/eval-adicup3029/hardware.1495646834.txt.gz · Last modified: 24 May 2017 19:27 by Brandon Bushey