EVALUATING THE AD9780/AD9781/AD9783 DIGITAL-TO-ANALOG CONVERTERS
Preface
This user guide describes both the hardware and software setup needed to acquire data capture from AD9783-DPG2-EBZ evaluation board to characterize AD9780/AD9781/AD9783 12-/14-/16- bit 500MSPS high-speed digital-to-analog converter
This guide shows how AD9783-DPG2-EBZ works with ADS7-V2/SDP-H1 controller boards developed by Analog Devices. Link to the old user guide document is provided for customers who still have DPG2 and DPG3 controller boards.
Typical Setup
Figure 1a. EVAL-AD978x with SDP-H1
Figure 1b. EVAL-AD978x with ADS7-V2
Tip: Click on any picture in this guide to open an enlarged version.
Helpful Files
Software Needed:
Known Issue: ACE may fail to detect HS-DAC boards, details
here.
Hardware Needed:
-
-
5Vdc 1A Power supply for the evaluation board
AD-DAC-FMC-ADP High-Speed DAC Evaluation Board to
FMC Adapter Board
PC with ACE and DPG Lite Software Applications
High-Frequency Continuous Wave Generator (Clock Source)
Signal/Spectrum Analyzer
(2) SMA Cables
(2) Banana Plug Cables
The following are to be included if using SDP-H1 Evaluation Kit:
12Vdc 1A Wall Adapter
(2)
USB-A to
USB-Mini Cable
The following are to be included if using ADS7-V2 Evaluation Kit:
12Vdc Power Supply
Power Cord
-
Quick Start Guide
Attach
AD9783-DPG2-EBZ to controller board's (SDP-H1/ADS7-V2)
FMC connector using the AD-DAC-
FMC-ADP adapter board.
Connect the controller board (SDP-H1/ADS7-V2) to PC via
USB and to a
12V power supply.
Connect the evaluation board to PC via
USB and to a
5Vdc 1A power supply on
P5 and
P6. Refer to Figures 1a and 1b.
Connect continuous wave generator for clock input to SMA J1 and DAC output from SMA J5 (IOUT1P) or SMA J9 (IOUT2P) to a signal/spectrum analyzer.
Set clock input to 200MHz, 3dBm.
Open ACE. The board will be automatically recognized by the software. Click the plugin. Otherwise, install the
ACE plugin for AD9783.
On the ACE Board View, double click the AD9783 block to access the Chip View.
Figure 3. AD9783 Chip View
The default values for the register is displayed and set. The values can be changed on the Chip View
GUI, or on the
Memory Map for registers not available in the
GUI. For more info on the memory map, refer to
AD978x datasheet. Once the desired values are set, Click
Apply Changes and then
Read All on the upper right window.
Figure 4. Apply Changes and Read All button
Start DPG Downloader Lite. The controller board (SDP-H1/ADS7-V2), the device part number and clock frequency should be displayed. Refer to Figures 5a and 5b.
Figure 5a. DPG Lite Session for EVAL-AD9783 with SDP-H1
Figure 5b. DPG Lite Session for EVAL-AD9783 with ADS7-V2
In DPG Downloader Lite, from the Add Generator Waveforms pulldown menu select Single Tone and apply the settings as shown in Figures 5a and 5b. Set the Data Rate to 200MHz and Desired Frequency to 16MHz. Set DAC Resolution to 16 for AD9783, 14 for AD9781, and 12 for AD9780. Uncheck the Unsigned Data box and Check the Generate Complex Data (I & Q).
Select the I/Q tone from the I/Q Data Vector pulldown menu.
Press the download arrow and then the play button. The spectrum similar to Figure 6 should appear in the signal/spectrum analyzer.
Figure 6. Spectrum Output for AD9783; Fdac = 200MSPS, Fout = 16MHz
Using the ADL5375 Modulator
By default, solder jumpers JP4, JP5, JP6, and JP7 are configured to route the DAC outputs to SMA J5 (IOUT1P) and to J9 (IOUT2P). This jumper setting is shown on Figure 7a. To connect the DAC output to the filter that feeds into the ADL5375, the solder jumpers should be reconfigured as shown in Figure 7b. Source the desired LO of the modulator (i.e. 900 or 1800MHz, 3dBm) on SMA J2 (LO IN). The ADL5375 Modulator output can be observed on SMA J6 (RF OUT).
Figure 7a (left). DAC Output Configuration; Figure 7b (right) Modulator Output Configuration
Troubleshooting
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur:
Check the voltage rails of the evaluation board. P5 and P6 should be 5V; TP3, TP5, and TP7 should be 3.3V; TP9 and TP11 should be 1.8V.
Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of the controller board (SDP-H1/ADS7-V2) if not lit up.
Check if controller board (SDP-H1/ADS7-V2) is being supplied properly by 12Vdc adapter. Some LEDs on the controller board should lit up.
Perform a chip reset by pressing S2 on the AD9783 evaluation board.
Power cycle both the controller board (SDP-H1/ADS7-V2) and the AD9783 evaluation board.
Probe C18 and C19 to make sure a clock signal is being sent into the DAC.
Check if XD1 is lit up on the evaluation board. Reconnect/replace the
USB cable connection to the evaluation board if it's not lit up.
Disconnect and reconnect the controller board (SDP-H1/ADS7-V2) and AD9783 evaluation board. Reopen ACE and DPG Lite software.