This is an old revision of the document!
The JESD204 Linux Kernel Framework is a Finite State Machine (FSM) that is meant to synchronize other Linux device drivers to be able to properly bring-up & manage a single or multiple JESD204 links.
The JESD204 link bring-up and management is complicated, and it requires that many actors (device drivers), be in sync with each other, in various link bring-up states/stages. Typical components of an JESD204 link are the physical layer (PHY), link layer (LL), transport layer (TPL) and the high speed converter device and clocking layer with all it's constrains and inter-dependencies. This has to happen not just at boot-time, but also during run-time, in case a link is going to be reconfigured or breaks and has to recover.
To achieve this, the JESD204 Linux Kernel Framework hooks into all the drivers that participate in the link management (bring-up/bring-down) and each driver provides a set of callbacks for each state that it supports.
The relationship between the devices is defined in the device-tree. The relationship is called a connection so as not to re-use the term link, which can cause confusion with the term link from the JESD204 standard. The whole group of devices, is actually a graph (or topology), with a single top-level device.
To illustrate, here's an example device-tree and below it how the graph representation looks like for an ADRV9009 FMC card on a ZC706.
// SPDX-License-Identifier: GPL-2.0 /* * Analog Devices ADRV9009 (via jesd204-fsm) * https://wiki.analog.com/resources/eval/user-guides/adrv9009 * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/adrv9009 * https://wiki.analog.com/resources/tools-software/linux-software/adrv9009_advanced_plugin * * hdl_project: <adrv9009/zc706> * board_revision: <> * * Copyright (C) 2020 Analog Devices Inc. */ #include "zynq-zc706-adv7511-adrv9009.dts" #include <dt-bindings/iio/adc/adi,adrv9009.h> &trx0_adrv9009 { jesd204-device; #jesd204-cells = <2>; jesd204-top-device = <0>; /* This is the TOP device */ jesd204-link-ids = <DEFRAMER_LINK_TX FRAMER_LINK_RX FRAMER_LINK_ORX>; jesd204-inputs = <&axi_adrv9009_rx_jesd 0 FRAMER_LINK_RX>, <&axi_adrv9009_rx_os_jesd 0 FRAMER_LINK_ORX>, <&axi_adrv9009_tx_jesd 0 DEFRAMER_LINK_TX>; /delete-property/ interrupts; }; &axi_adrv9009_rx_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_rx 0 FRAMER_LINK_RX>; }; &axi_adrv9009_rx_os_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_rx_os 0 FRAMER_LINK_ORX>; }; &axi_adrv9009_tx_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_tx 0 DEFRAMER_LINK_TX>; }; &axi_adrv9009_adxcvr_rx { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&clk0_ad9528 0 FRAMER_LINK_RX>; clocks = <&clk0_ad9528 1>; /* div40 is controlled by axi_adrv9009_rx_jesd */ clock-names = "conv"; }; &axi_adrv9009_adxcvr_rx_os { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&clk0_ad9528 0 FRAMER_LINK_ORX>; clocks = <&clk0_ad9528 1>; /* div40 is controlled by axi_adrv9009_rx_os_jesd */ clock-names = "conv"; }; &axi_adrv9009_adxcvr_tx { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&clk0_ad9528 0 DEFRAMER_LINK_TX>; clocks = <&clk0_ad9528 1>; /* div40 is controlled by axi_adrv9009_tx_jesd */ clock-names = "conv"; }; &clk0_ad9528 { jesd204-device; #jesd204-cells = <2>; jesd204-sysref-provider; adi,sysref-pattern-mode = <SYSREF_PATTERN_NSHOT>; /delete-property/ adi,sysref-request-enable; };
The structure above translates to the image below.
The picture in the diagram makes thinks look really simple, but in reality they aren't. If any of the devices in that topology/graph has a change of state, or an error occurs, multiple devices must be re-synchronized.
Also, the device-tree described above, is an actual working device-tree. Some variations may be found in the ADI Linux kernel repository (i.e. some more nodes in-between the nodes described above).
There may be other frameworks in Linux that describe this topology, but the challenge with JESD204 is that (at this current point in time), there is no clear idea of the minimum amount of states needed to synchronize or re-synchronize in order to recover a JESD204 link if it goes down.
The end-result is an FSM that tries to make all the devices go through the same states at once.
Some design principles, defined so far for this framework:
The current source code of the JESD204 Linux framework resides in https://github.com/analogdevicesinc/linux/blob/master/drivers/jesd204/
It is comprised of the current source files:
A typical driver needs to provide some data to the framework. Example (for ADRV9009):
static const struct jesd204_dev_data jesd204_adrv9009_init = { .state_ops = { [JESD204_OP_DEVICE_INIT] = { .per_device = adrv9009_jesd204_uninit, }, [JESD204_OP_LINK_INIT] = { .per_link = adrv9009_jesd204_link_init, }, [JESD204_OP_CLOCKS_ENABLE] = { .per_link = adrv9009_jesd204_clks_enable, }, [JESD204_OP_LINK_SETUP] = { .per_device = adrv9009_jesd204_link_setup, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, .post_state_sysref = true, }, [JESD204_OP_LINK_ENABLE] = { .per_link = adrv9009_jesd204_link_enable, .post_state_sysref = true, }, [JESD204_OP_LINK_RUNNING] = { .per_link = adrv9009_jesd204_link_running, }, [JESD204_OP_OPT_SETUP_STAGE1] = { .per_device = adrv9009_jesd204_setup_stage1, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, .post_state_sysref = true, }, [JESD204_OP_OPT_SETUP_STAGE2] = { .per_device = adrv9009_jesd204_setup_stage2, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, .post_state_sysref = true, }, [JESD204_OP_OPT_SETUP_STAGE3] = { .per_device = adrv9009_jesd204_setup_stage3, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, .post_state_sysref = true, }, [JESD204_OP_OPT_SETUP_STAGE4] = { .per_device = adrv9009_jesd204_setup_stage4, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, }, [JESD204_OP_OPT_SETUP_STAGE5] = { .per_device = adrv9009_jesd204_setup_stage5, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, }, [JESD204_OP_OPT_POST_RUNNING_STAGE] = { .per_device = adrv9009_jesd204_post_running_stage, .mode = JESD204_STATE_OP_MODE_PER_DEVICE, }, }, .num_links = 3, .sizeof_priv = sizeof(struct adrv9009_jesd204_priv), };
The driver needs to call devm_jesd204_dev_register(). All this does, is to bind the driver from the probe the device-tree binding/definition for this device's place in a JESD204 topology. If the devm_jesd204_dev_register() function returns NULL, this driver is not part of any JESD204 topology/operation. For example, some clock-chip drivers can operate as clock-drivers, or as JESD204 providers.
Example:
jdev = devm_jesd204_dev_register(&spi->dev, jesd204_init); if (IS_ERR(jdev)) return PTR_ERR(jdev);
All drivers must finally call (in probe) the jesd204_fsm_start() on their object from the framework. This is true for all devices, even the ones that are not top-level devices.
Example:
ret = jesd204_fsm_start(jdev, JESD204_LINKS_ALL);
If jdev is NULL, that is fine. Typically, a driver may call this FSM for all JESD204 links that are defined in the device-tree. With the sysfs, the jesd204_fsm_start() may be called for a single JESD204 link.
There's an equivalent jesd204_fsm_stop() that will stop the FSM.
The proper functioning of the FSM relies on the driver correctly using the framework and that that connections between devices be properly defined in the device-tree.
The initialization data has type:
/** * struct jesd204_dev_data - JESD204 device initialization data * @sysref_cb SYSREF callback, if this device/driver supports it * @sizeof_priv amount of data to allocate for private information * @links JESD204 initial link configuration * @num_links number of JESD204 links * @num_retries number of retries in case of error (only for top-level device) * @state_ops ops for each state transition of type @struct jesd204_state_op */ struct jesd204_dev_data { jesd204_sysref_cb sysref_cb; size_t sizeof_priv; const struct jesd204_link *links; unsigned int num_links; unsigned int num_retries; struct jesd204_state_op state_ops[__JESD204_MAX_OPS]; };
Each driver hooks it's callback by adding the proper entry in the state_ops array. The type of a state_op is defined as (may be subject to change):
/** * struct jesd204_state_op - JESD204 device per-state op * @mode mode for this state op, depending on this @per_device or @per_link is called * @per_device op called for each JESD204 **device** during a transition * @per_link op called for each JESD204 **link** individually during a transition * @post_state_sysref true if a SYSREF should be issued after the state change */ struct jesd204_state_op { enum jesd204_state_op_mode mode; jesd204_dev_cb per_device; jesd204_link_cb per_link; bool post_state_sysref; };
During a state-transition a state callback will be called:
It's unsure (yet) whether it makes sense to call both per_link and per_device callbacks for a state. It could be an option at a later point in time.
Optionally, each state may request a SYSREF call, by setting post_state_sysref to true.
Important JESD204-FSM link states in a nutshell.
LINK_INIT
The JESD204-FSM calls this callback (struct jesd204_dev_data) init.num_links
times. The TOP device fills in the (struct jesd204_link
) parameter for each link. These parameters include all the JESD204 link parameters, the sample rate and SYSREF mode settings, such as continuous or pulsed SYSREF operation.
LINK_SUPPORTED
During this state the FSM core, calls for each link of a topology into each device in order to query if this configuration is supported. Whether a configuration is supported or not depends on a number of constrains and synthesis parameters. In case all devices support the configuration, the FSM moves on to the next state. The clock chip drivers use this state to compute the LMFC/LMEC of all links and find it’s GCD, so that a common SYSREF frequency can be computed which satisfies all links requirements.
LINK_PRE_SETUP
Typically, this state is used by the CLK chip drivers to configure the output channels dedicated as SYSREF, applies the previously computed SYSREF frequency and configures the mode.Optional CLK_SYNC_STAGEs
These states can be used by clock chip drivers to implement a Clock Tree Synchronization mechanism. This is typically device specific or might not be supported by the clock chip in question.
Right now, there are 3 states reserved for this. Based on the HMC7044 example this is what happens in each state.
CLK_SYNC_STAGE1
The SYNC provider and consumers are configured to generate or receive a synchronization request.
CLK_SYNC_STAGE2
The synchronization request is issued at the TOP most device in the clock tree. For the HMC7044, this is the SYSREF PROVIDER.
CLK_SYNC_STAGE3
In this last CLK SYNC state, the SYNC status of each CLK device is validated.
LINK_SETUP
In this state all actors (link devices) are setup and configured, based on the mode and configuration previously validated. A lot of devices typically found on multi-chip setups, require additional synchronization steps such as MCS (Mult-chip Sync), Phase/NCO Sync, or calibrations which take a lot of time and would benefit from being done in parallel to save some time.
For those cases OPT_SETUP_STAGE1 to OPT_SETUP_STAGE5 can be used to implement these High-Speed converter device specific configuration, synchronization and calibration steps.
CLOCKS_ENABLE & LINK_ENABLE
Depending on the direction of the JESD204 link, different link components may implement different things. However, as the name implies it’s about enabling the JESD204 links. This includes taking the Link Layer cores out of RESET, enabling the SYSREF receivers for SUBCLASS 1 operation, requesting a SYSREF pulse, etc.
LINK_RUNNING
In this state all links of a topology assumed running. This is typically being checked in this state.
Drivers can also use this state to complete setup and configuration which is required after the JESD204 links are running. In case another state is required drivers can also implement the optional OPT_POST_RUNNING_STAGE for these purposes.
Before the introduction of the JESD204-FSM kernel framework, JESD204 link bring-up and management was subject to some known deficiencies, incurred by the Linux driver model. In order to understand the original challenges, they are in following explained with their new solution.
Bringing up a JESD204 link, involves several HDL cores and device device drivers. Some of the configuration was done in the device tree, some were synthesis parameters, etc. It was necessary to provide similar device tree configuration in multiple places. In the new kernel framework, the TOP device sets the configuration and is then broadcasted to all link components and checked for validity. Each component now understands the big picture and can act accordingly. For example, the CLK and SYSREF provider now knows the LMFC/LMEC frequencies of all links on a topology, so it can compute a suitable SYSREF frequency common to all JESD204 links.
Prior to the new kernel framework, each converter driver required a lot of Linux kernel common clock framework (CCF) clocks connected. There used to be one for the JESD lane clock, the JESD core/link clock (typical lane rate / 40), the converter clock and the SYSREF clock. Each converter driver implemented some math on how to calculate the link and lane clock from its configuration. This caused a lot of duplicated boilerplate code. However more problematic was that the link enable was done using the CCF clk_prepare_enable() API. This was convenient since the CCF ensured that the parent of each clock was enabled prior to its childs. But depending on the JESD204 link direction this was not always the ideal sequence across the entire chain. Error propagation was also suboptimal, since an error code delivered to the driver which controlled the clk_enable could have been originated anywhere in the clock tree, from clock-chip, via the PHY-Layer, LINK-Layer, etc. One other issue was that besides clk_enable and clk_set_rate() there were other things to control, such as SYSREF N-SHOT mode, which wasn’t possible due to the lack of a proper API. Also, the CCF uses reference counting, so disabling a clock doesn’t necessarily disable the clock in case it was enabled twice, possibly from a different device. There were many more things such as controlling a clock from a CCF clock implementation wasn’t possible due to the global CCF lock (spinlock). The new implementation still used CCF clocks in its intended way, but no longer using it for link bring-up and enable which it wasn’t intended for. Last but not least, on 32-bit Linux systems the CCF rate is handled as 32-bit value, which without truncation easily overflowed with the JESD204 lane rate passed in Hz. With the new framework required clocks are automatically computed and checked. The framework implements the sequence, error conditions are detected and handled.
Converter devices in a multi-chip setup often require additional synchronization steps which must be issued in parallel. So that the same pulse hits all devices at the same time during an initialization sequence. This is rather difficult to achieve in case devices are instantiated/probed sequentially from its bus management core. Prior to the FSM kernel framework, the workaround was done from Linux user space in writing some magic numbers to an SYSFS attribute typically called multichip_sync. Also problematic was the fact that SYSREF requests were only possible from one device, since the request was done via the GPIO API, and the GPIO is a protected resource and can’t be controlled from multiple entities concurrently. In some setups the workaround was to use continuous SYSREF, however this is rather suboptimal since SYSREF can cause clock spurs in the high-speed converter spectrum. With the new kernel framework each device can request a SYSREF pulse asynchronously, but in most situations the framework request SYSREF pulses as part of the required state transitions.
Below example is taken from ADRV9009-ZU11EG System on Module on the ADRV2CRR-FMC carrier board with an additional FMCOMMS8 FMC board connected. So, in total there are 4x ADRV9009 RF transceivers in this design, with a two-level clock tree. The JESD204-FSM topology and input connections can be found below.
Devicetree: zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8-jesd204-fsm.dts
// SPDX-License-Identifier: GPL-2.0 /* * Analog Devices ADRV2CRR-FMC using ADRV9009-ZU11EG System on Module + AD-FMCOMMS8-EBZ * https://wiki.analog.com/resources/eval/user-guides/adrv9009-zu11eg/adrv2crr-fmc_carrier_board * https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms8-ebz * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/adrv9009 * https://wiki.analog.com/resources/tools-software/linux-software/adrv9009_advanced_plugin * * hdl_project: <adrv9009zu11eg/adrv2crr_fmcomms8> * board_revision: <> * * Copyright (C) 2020 Analog Devices Inc. */ #include "zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8.dts" #include <dt-bindings/iio/frequency/hmc7044.h> #include <dt-bindings/iio/adc/adi,adrv9009.h> &trx0_adrv9009 { jesd204-device; #jesd204-cells = <2>; jesd204-top-device = <0>; /* This is the TOP device */ jesd204-link-ids = <DEFRAMER_LINK_TX FRAMER_LINK_RX FRAMER_LINK_ORX>; jesd204-inputs = <&trx1_adrv9009 0 FRAMER_LINK_RX>, <&trx1_adrv9009 0 FRAMER_LINK_ORX>, <&trx1_adrv9009 0 DEFRAMER_LINK_TX>; /delete-property/ interrupts; adi,jesd204-framer-a-lmfc-offset = <15>; }; &trx1_adrv9009 { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&trx2_adrv9009 0 FRAMER_LINK_RX>, <&trx2_adrv9009 0 FRAMER_LINK_ORX>, <&trx2_adrv9009 0 DEFRAMER_LINK_TX>; /delete-property/ interrupts; adi,jesd204-framer-a-lmfc-offset = <15>; }; &trx2_adrv9009 { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&trx3_adrv9009 0 FRAMER_LINK_RX>, <&trx3_adrv9009 0 FRAMER_LINK_ORX>, <&trx3_adrv9009 0 DEFRAMER_LINK_TX>; /delete-property/ interrupts; adi,jesd204-framer-a-lmfc-offset = <15>; }; &trx3_adrv9009 { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_rx_jesd 0 FRAMER_LINK_RX>, <&axi_adrv9009_rx_os_jesd 0 FRAMER_LINK_ORX>, <&axi_adrv9009_core_tx 0 DEFRAMER_LINK_TX>; /delete-property/ interrupts; adi,jesd204-framer-a-lmfc-offset = <15>; }; &axi_adrv9009_core_tx { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_tx_jesd 0 DEFRAMER_LINK_TX>; }; &axi_adrv9009_rx_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_rx 0 FRAMER_LINK_RX>; clocks = <&zynqmp_clk 71>, <&hmc7044 7>, <&axi_adrv9009_adxcvr_rx 0>, <&hmc7044_fmc 5>; clock-names = "s_axi_aclk", "device_clk", "lane_clk", "conv2"; }; &axi_adrv9009_rx_os_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_rx_os 0 FRAMER_LINK_ORX>; clocks = <&zynqmp_clk 71>, <&hmc7044 6>, <&axi_adrv9009_adxcvr_rx_os 0>, <&hmc7044_fmc 4>; clock-names = "s_axi_aclk", "device_clk", "lane_clk", "conv2"; }; &axi_adrv9009_tx_jesd { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&axi_adrv9009_adxcvr_tx 0 DEFRAMER_LINK_TX>; clocks = <&zynqmp_clk 71>, <&hmc7044 6>, <&axi_adrv9009_adxcvr_tx 0>, <&hmc7044_fmc 4>; clock-names = "s_axi_aclk", "device_clk", "lane_clk", "conv2"; }; &axi_adrv9009_adxcvr_rx { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&hmc7044 0 FRAMER_LINK_RX>; clock-names = "conv", "conv2"; clocks = <&hmc7044 5>, <&hmc7044_fmc 5>; }; &axi_adrv9009_adxcvr_rx_os { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&hmc7044 0 FRAMER_LINK_ORX>; clock-names = "conv", "conv2"; clocks = <&hmc7044 4>, <&hmc7044_fmc 4>; }; &axi_adrv9009_adxcvr_tx { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&hmc7044 0 DEFRAMER_LINK_TX>; clock-names = "conv", "conv2"; clocks = <&hmc7044 4>, <&hmc7044_fmc 4>; }; &hmc7044 { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&hmc7044_fmc 0 FRAMER_LINK_RX>, <&hmc7044_fmc 0 FRAMER_LINK_ORX>, <&hmc7044_fmc 0 DEFRAMER_LINK_TX>; adi,pulse-generator-mode = <HMC7044_PULSE_GEN_16_PULSE>; adi,sync-pin-mode = <1>; /delete-property/ adi,pll2-autocal-bypass-manual-cap-bank-sel; adi,hmc-two-level-tree-sync-en; }; &hmc7044_fmc { jesd204-device; #jesd204-cells = <2>; jesd204-inputs = <&hmc7044_car 0 FRAMER_LINK_RX>, <&hmc7044_car 0 FRAMER_LINK_ORX>, <&hmc7044_car 0 DEFRAMER_LINK_TX>; adi,pulse-generator-mode = <HMC7044_PULSE_GEN_16_PULSE>; adi,sync-pin-mode = <1>; /delete-property/ adi,pll2-autocal-bypass-manual-cap-bank-sel; adi,hmc-two-level-tree-sync-en; }; &hmc7044_car { adi,pll1-clkin-frequencies = <0 30720000 0 38400000>; adi,pll1-ref-prio-ctrl = <0x8D>; /* CLKIN1 -> CLKIN3 -> CLKIN0 -> CLKIN2 */ adi,pll1-ref-autorevert-enable; jesd204-device; #jesd204-cells = <2>; jesd204-sysref-provider; adi,pulse-generator-mode = <HMC7044_PULSE_GEN_16_PULSE>; adi,sync-pin-mode = <0>; /delete-property/ adi,pll2-autocal-bypass-manual-cap-bank-sel; adi,hmc-two-level-tree-sync-en; };
Multi-chip designs often require modular and complex clocking trees with multiple synchronized clock providers. Besides core and FPGA reference clocks used in such systems, the SYSREF signal acts as the master timing reference and aligns all the internal dividers from device clocks as well as the local multiframe clocks in each JESD204 transmitter and receiver. SYSREF helps to ensure deterministic latency through the system. Therefore designing a clocking tree needs some extra attention.
One of the key challenges in JESD204B/C system design is ensuring the synchronization of data converter frame alignment across the system, from the FPGA to ADCs and DACs through a large clock tree that can comprise multiple clock generation and distribution ICs. The HMC7044 which is used in this example is specifically designed to offer features to address this challenge. An external reference-based synchronization feature (SYNC via PLL2 or RF SYNC only in fanout mode) synchronizes multiple devices, that is, it ensures that all clock outputs start with same rising edge. This operation is achieved by rephasing the SYSREF control unit deterministically, and then restarting the output dividers with this new desired phase. A SYSREF/PULSOR request issued at the TOP device in the clocking tree will propagate down in the hierarchy. This feature is extremely important in the JESD204-FSM implementation since there can be only one SYSREF PROVIDER per topology.
Taking this one step further, by adding another layer in the clock tree this concept can be expanded.
In the example above let’s assume the left setup (#1) controls the top-level clock-chip (hmc7044_ext), which acts as the external SYSREF PROVIDER. We call this the PRIMARY setup. The right setup (#2) is therefore called SECONDARY.
The devicetrees for both of them can be found below. They include the above example and just add/remove pieces which are required to synchronize such a distributed Multi-Topology system.
#include "zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8-jesd204-fsm.dts" #include <dt-bindings/iio/frequency/hmc7044.h> #include <dt-bindings/jesd204/device-states.h> &trx0_adrv9009 { jesd204-stop-states = < JESD204_FSM_STATE_CLK_SYNC_STAGE1 JESD204_FSM_STATE_CLK_SYNC_STAGE2 JESD204_FSM_STATE_CLK_SYNC_STAGE3 JESD204_FSM_STATE_LINK_SETUP JESD204_FSM_STATE_OPT_SETUP_STAGE1 JESD204_FSM_STATE_OPT_SETUP_STAGE2 JESD204_FSM_STATE_OPT_SETUP_STAGE3 JESD204_FSM_STATE_OPT_SETUP_STAGE4 JESD204_FSM_STATE_OPT_SETUP_STAGE5 JESD204_FSM_STATE_CLOCKS_ENABLE JESD204_FSM_STATE_LINK_ENABLE>; }; &hmc7044_car { jesd204-inputs = <&hmc7044_ext 0 FRAMER_LINK_RX>, <&hmc7044_ext 0 FRAMER_LINK_ORX>, <&hmc7044_ext 0 DEFRAMER_LINK_TX>; /delete-property/ jesd204-sysref-provider; }; &hmc7044_ext { jesd204-device; #jesd204-cells = <2>; jesd204-sysref-provider; adi,pulse-generator-mode = <HMC7044_PULSE_GEN_1_PULSE>; adi,hmc-two-level-tree-sync-en; };
On the devicetree for the PRIMARY device:
jesd204-device
property and connecting the jesd204-inputs
of the hmc7044_car.jesd204-sysref-provider
moves form the hmc7044_car to the hmc7044_ext device.jesd204-top-device
trx0_adrv9009 now defines a jesd204-stop-states
array. These are states in which the jesd204-fsm framework pauses (stops) and waits for some external resume event to occur.#include "zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8-jesd204-fsm.dts" #include <dt-bindings/jesd204/device-states.h> &trx0_adrv9009 { jesd204-stop-states = < JESD204_FSM_STATE_CLK_SYNC_STAGE1 JESD204_FSM_STATE_CLK_SYNC_STAGE2 JESD204_FSM_STATE_CLK_SYNC_STAGE3 JESD204_FSM_STATE_LINK_SETUP JESD204_FSM_STATE_OPT_SETUP_STAGE1 JESD204_FSM_STATE_OPT_SETUP_STAGE2 JESD204_FSM_STATE_OPT_SETUP_STAGE3 JESD204_FSM_STATE_OPT_SETUP_STAGE4 JESD204_FSM_STATE_OPT_SETUP_STAGE5 JESD204_FSM_STATE_CLOCKS_ENABLE JESD204_FSM_STATE_LINK_ENABLE>; }; &hmc7044_car { /delete-property/ jesd204-sysref-provider; jesd204-secondary-sysref-provider; }; &hmc7044_ext { status = "disabled"; };
On the devicetree for the SECONDARY device:
jesd204-stop-states
at the jesd204-top-device
in this topology/setup.jesd204-sysref-provider
is completely removed.jesd204-secondary-sysref-provider
attribute.A secondary sysref-provider is only used in distributed multi-topology systems. It’s purely used for JESD204 link (re-)establishment and not for other synchronization purposes.
The secondary sysref-provider, in case it exists, is only called if the jesd204-fsm device uses the jesd204_sysref_async_force() function.
Right now, this is done only in the driver for the axi_jesd204_rx link layer peripheral in case a link error interrupt is issued, or the watchdog detects an issue. The secondary sysref-provider is always assumed to be part of the JESD204 clocking tree. Furthermore, it is assumed that the SYSREF timer and frequency is already synced with the remaining part of the clocking tree.
In such situations the asynchronous request further down the clocking tree is never going to be an issue for JESD204 link bring-up and maintenance.
Well some more complex converter systems with internal NCOs and multi-chip sync capabilities need synchronization events that are carried out across all devices in a larger Multi-Topology system at the same instance in time.
In such systems the topology which controls the top-level clock distribution device registers the primary sysref-provider. The jesd204-fsm jesd204-stop-states
are used to pause the device initialization and link bring-up in certain states.
Some external manager controls this and resumes the devices in a proper order.
Example: iio_jesd204_fsm_sync
This utility resumes a number of iio devices across different IIO context from the jesd204-fsm stop-states. It’s intended to sync multiple FPGA systems across jesd204-fsm topologies. There is always one primary device, the device which controls the sysref-provider and an open list of secondary devices which are synced by the same sysref-provider connected clock source.
Usage: iio_jesd204_fsm_sync -d <primary-device> -u <primary-uri> <secondary uris> ...
Example: #iio_jesd204_fsm_sync -d adrv9009-phy -u ip10.48.65.140 ip:10.48.65.244 --------------------------------------------------------------------------- DEVICE0: adrv9009-phy uri=ip:10.48.65.140 (Primary) created DEVICE1: adrv9009-phy uri=ip:10.48.65.244 (Secondary) created --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <clk_sync_stage1> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <clk_sync_stage1> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <clk_sync_stage2> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <clk_sync_stage2> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <clk_sync_stage3> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <clk_sync_stage3> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <link_setup> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <link_setup> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <opt_setup_stage1> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <opt_setup_stage1> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <opt_setup_stage2> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <opt_setup_stage2> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <opt_setup_stage3> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <opt_setup_stage3> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <opt_setup_stage4> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <opt_setup_stage4> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <opt_setup_stage5> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <opt_setup_stage5> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <clocks_enable> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <clocks_enable> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- DEVICE1: Is <Paused> in state <link_enable> with status <Success (0)> --- RESUME DEVICE1 --- DEVICE0: Is <Paused> in state <link_enable> with status <Success (0)> --- RESUME DEVICE0 --- --------------------------------------------------------------------------- --- DONE ---