This is an old revision of the document!
The ADC JESD204B/C Transport Peripheral implements the transport level handling of a JESD204B/C transmitter device. It is compatible with a wide range of Analog Devices high-speed analog-to-digital converters.
The core handles the JESD204B/C de-framing of the payload data.
The peripheral can be configured at runtime through a AXI4-Lite memory mapped register map.
Name | Description | Default |
---|---|---|
ID | Instance identification number. | 0 |
NUM_LANES | Number of lanes supported by the peripheral. Equivalent to JESD204 L parameter. | 4 |
NUM_CHANNELS | Number of converters supported by the peripheral. Equivalent to JESD204 M parameter. | 2 |
SAMPLES_PER_FRAME | Number of samples per frame. Equivalent to JESD204 S parameter. | 1 |
CONVERTER_RESOLUTION | Resolution of the converter. Equivalent to JESD204 N parameter. | 16 |
BITS_PER_SAMPLE | Number of bits per sample. Equivalent to JESD204 NP parameter. | 16 |
OCTETS_PER_BEAT | Number of bytes per beat for each link. | 4 |
Name | Type | Description |
---|---|---|
s_axi_aclk | Clock | All S_AXI signals are synchronous to this clock. |
s_axi_aresetn | Synchronous active low reset | Resets the internal state of the peripheral. |
S_AXI | AXI4-Lite bus slave | Memory mapped AXI-lite bus that provides access to modules register map. |
Link layer interface | ||
link_clk | Clock | Device clock for the JESD204B interface. Must be line clock / 40 for correct 204B operation. Must be line clock / 66 for correct 64b66b 204C operation. |
LINK_DATA | AXI4-Streaming interface slave | JESD204 link data interface. |
Application layer interface | ||
enable | Output | Channel enable indicator. |
adc_valid | Output | Qualifier signal for each channel. Always '1'. |
adc_data | Output | Raw application layer data, every channel concatenated. |
adc_dovf | Input | Application layer overflow. |
The S_AXI interface is synchronous to the s_axi_aclk clock. All other signals and interfaces are synchronous to the device_clk clock.
The peripheral features a register map configuration interface that can be accessed through the AXI4-Lite S_AXI
port. The register map can be used to configure the peripherals operational parameters, query the current status of the device and query the features supported by the device.
The link layer interface description can be found in the User Data Interface section of the JESD204B/C Link Receive Peripheral IP.
The application layer is connected to the deframer block output. The deframer module creates sample data from the lane mapped and formatted JESD204 link data based on the specified deframer configuration.
The data in the application layer interface adc_data
has the following layout:
MSB LSB [ MmSn, ..., MmS1, MnS0, ..., M1Sn, ... M1S1, M1S0, M0Sn, ... M0S1, M0S0 ]
Where MjSi refers to the i-th sample of the j-th converter. With m being the number of converters and n the number of samples per converter per beat.
The core asserts the enable
signal for each channel that is enabled by the software.
The REG_STATUS
(0x054
) register CLK_FREQ
field allows to determine the clock rate of the device clock (link_clk
) relative to the AXI interface clock (s_axi_aclk
). This can be used to verify that the device clock is running at the expected rate.
The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock this corresponds to a resolution of 1.523kHz per LSB. A raw value of 0 indicates that the link clock is currently not active.
The component is configured by the REG_CHAN_CNTRL
register FORMAT_SIGNEXT,FORMAT_TYPE,FORMAT_ENABLE
fields.
The block introduces one clock cycle latency.
The block can monitor and compare the incoming deframed raw data against PN9 or PN23 patterns selected by the ADC_PN_SEL
field of REG_CHAN_CNTRL_3
register.
ADC_PN_SEL | PN |
---|---|
0 | PN9 |
others | PN23 |
For each channel mismatches are reported in PN_ERR
and PN_OOS
fields of the REG_CHAN_STATUS
register.
An external synchronization signal adc_sync_in
can be used to trigger data movement from the link layer to user application layer.
The external synchronization signal should be synchronous with the adc clock. Synchronization will be done on the rising edge of the signal.
The self clearing SYNC
control bit from the REG_CNTRL (0x44)
register will arm the trigger logic to wait for the external sync signal. The ADC_SYNC
status bit from REG_SYNC_STATUS (0x68)
register will show that the synchronization is armed but the synchronization signal has not yet been received.
Once the sync signal is received the data will start to flow and the ADC_SYNC
status bit will reflect that with a deassertion.
While the synchronization mechanism is armed, the adc_rst
output signal is set so downstream logic can be cleared in order to have a fresh start once the trigger is received.
Reduced number of octets-per-frame (F
) settings. The following values are supported by the peripheral: 1, 2, 4
Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the EngineerZone.