This is an old revision of the document!
The util_adxcvr IP core instantiate a Gigabit Transceiver (GT) and set's up the required configuration. Basically is a simple wrapper file for a GT* Column, exposing just the necessary ports and attributes.
Currently this IP supports three different GT type:
The following diagram shows a GTXE2 Column, which contains four GT Quad. Each quad contains a GTEX2_COMMON and four GTXE2_CHANNEL primitive.
Name | Description | Default Value |
---|---|---|
XCVR_TYPE | Define the current GT type, GTXE2(0), GTHE3(1), GTHE4(2) | 0 |
QPLL_REFCLK_DIV | QPLL reference clock divider M, see User Guide for more info | 1 |
QPLL_FBDIV_RATIO | QPLL reference clock divider N ratio, see User Guide for more info | 1 |
QPLL_CFG | Configuration settings for QPLL, see User Guide for more info | 27'h0680181 |
QPLL_FBDIV | QPLL reference clock divider N, see User Guide for more info | 10'b0000110000 |
CPLL_FBDIV | CPLL feedback divider N2 settings, see User Guide for more info | 2 |
CPLL_FBDIV_45 | CPLL reference clock divider N1 settings, see User Guide for more info | 5 |
TX_NUM_OF_LANES | Number of transmit lanes. | 8 |
TX_OUT_DIV | CPLL/QPLL output clock divider D for the TX datapath, see User Guide for more info | 1 |
TX_CLK25_DIV | Divider for internal 25 MHz clock for the TX datapath, see User Guide for more info | 20 |
TX_LANE_INVERT | Per lane polarity inversion. Set the n-th bit to invert the polarity of the n-th transmit lane. | 0 |
RX_NUM_OF_LANES | Number of transmit lanes | 8 |
RX_OUT_DIV | CPLL/QPLL output clock divider D for the RX datapath, see User Guide for more info | 1 |
RX_CLK25_DIV | Divider for internal 25 MHz clock for the RX datapath, see User Guide for more info | 20 |
RX_DFE_LPM_CFG | Configure the GT use modes, LPM or DFE, see User Guide for more info | 16'h0104 |
RX_PMA_CFG | Search for PMA_RSV in User Guide for more info | 32'h001e7080 |
RX_CDR_CFG | Configure the RX clock data recovery circuit for GTXE2, see User Guide for more info | 72'h0b000023ff10400020 |
RX_LANE_INVERT | Per lane polarity inversion. Set the n-th bit to invert the polarity of the n-th receive lane. | 0 |
Interface | Pin | Type | Description |
---|---|---|---|
Microprocessor clock and reset | |||
up_clk | input | System clock, running on 100 MHz | |
up_rstn | input | System reset, the same as AXI memory map slave interface reset | |
PLL reference clock | |||
qpll_ref_clk_0 | input | Reference clock for the QPLL | |
cpll_ref_clk_0 | input | Reference clock for the CPLL | |
RX interface | |||
rx_*_p | input | Positive differential serial data input | |
rx_*_n | input | Negative differential serial data input | |
rx_out_clk_* | output | Core logic clock output. Frequency = serial line rate/40 | |
rx_clk_* | input | Core logic clock loop-back input | |
rx_charisk_* | output[ 3:0] | RX Char is K to the JESD204B IP | |
rx_disperr_* | output[ 3:0] | RX disparity error to the JESD204B IP | |
rx_notintable_* | output[ 3:0] | RX Not In Table to the JESD204B IP | |
rx_data_* | output[31:0] | RX data to the JESD204B IP | |
rx_calign_* | input | RX enable comma alignment from the JESD204B IP | |
TX interface | |||
tx_*_p | output | Positive differential serial output | |
tx_*_n | output | Negative differential serial output | |
tx_out_clk_* | output | Core logic clock output. Frequency = lane rate/40 | |
tx_clk_* | input | Core logic clock loop-back input | |
tx_charisk_* | input[ 3:0] | TX Char is K from the JESD204B IP | |
tx_data_* | input[31:0] | TX data from the JESD204B IP | |
Common DRP interface | |||
up_cm_* | IO | The common DRP interface, must be connected to the equivalent DRP ports of AXI_ADXCVR. This is a QUAD interface, shared by four transceiver lanes. This interface is available only if parameter QPLL_ENABLE is set to 0x1. | |
Channel DRP interface | |||
up_ch_* | IO | The channel DRP interface, must be connected to the equivalent DRP ports of AXI_ADXCVR. This is a channel interface, one per each transceiver lane. | |
Eye Scan DRP interface | |||
up_es_* | IO | The Eye-Scan DRP interface, must be connected to the equivalent DRP ports of UTIL_ADXCVR. This is a channel interface, one per each transceiver lane. This interface is available only if parameter TX_OR_RX_N is set to 0x0. |
For porting on different Xilinx transceiver types, there is the following guide.
The software can configure this core through the AXI_ADXCVR IP core.