The AXI_DAC_INTERPOLATE IP allows interpolation of the input data by 10/100/1000/10000/100000, with filtering and arbitrary zero-hold interpolation.
More about the generic framework interfacing DACs can be read here: axi_dac_ip.
Name | Description | Default Value |
---|---|---|
CORRECTION_DISABLE | Disable scale correction of the CIC output | 1 |
Interface | Pin | Type | Description |
---|---|---|---|
Clock | |||
dac_clk | input | Clock input | |
Reset | |||
dac_rst | input | Reset, synchronous on the dac_clk clock domain | |
Data Inputs | |||
dac_data_a | input[15:0] | Analog data for channel A | |
dac_data_b | input[15:0] | Analog data for channel B | |
dac_data_valid_a | input | Data valid signal for channel A | |
dac_data_valid_b | input | Data valid signal for channel B | |
Interpolated Outputs | |||
dac_int_data_a | output[15:0] | Interpolated data for channel A | |
dac_int_data_b | output[15:0] | Interpolated data for channel B | |
dac_int_valid_a | output | Data valid for channel A | |
dac_int_valid_b | output | Data valid for channel B | |
Trigger input | |||
trigger_i | input[1:0] | External trigger pins | |
trigger_adc | input | ADC trigger | |
trigger_la | input | Logic Analyzer trigget | |
AXI_S_MM interface | |||
s_axi_* | Standard AXI Slave Memory Map interface |
For some applications, the maximum sampling rate of the DAC is too high and leads to a bad utilization of the memory or USB bandwidth. In order to avoid that, the interpolation IP can be used.
The interpolation block allows interpolation by 10, 100, 1000, 10000,100000 with filtering. The filtering is implemented using an FIR compensation filter (interpolation by 2) for the CIC and a 6 stage CIC interpolation filter allowing interpolation by 5/50/500/5000/50000.
At the end of the filter blocks, there is an arbitrary interpolation zero-order hold block which holds the value for a configurable number of samples.
The axi_dac_interpolate also controls the data flow, being the middle man between axi_ad9963 as the main data flow controller(consumer) and the DMA a subordinate in the path. This control is done through registers:
The actual control consists in fetching data from the DMA:
If the DMA is stopped through the axi_dac_interpolate (dma_transfer_suspend or external trigger) and not by disabling the DMA from it's register map, the DAC data path will keep a few residual samples in the DMA's pipes. This samples will be the first samples to be transferred when a new buffer is pushed. To avoid this one can use the DMA flush feature which clears the DMA when stopped by the consumer.
By default the flush flag is active. It should be disabled only if the user wants a “pause” functionality. Meaning, the transfer is stopped on a event and then, on another event, the transfer will continue from the same point without having to create a new buffer. The event can be the set/clearing of dma_transfer_suspend or an external trigger.
Another feature is the stop_sync. There is only one usecase for it. Stopping the other channel(configured at a different rate and/or in cyclic mode) when the first channel(DMA) finishes the transfer of a non-cyclic buffer.
The RAW transfer feature enables the user to transfer data(written into a register inside the axi_dac_interpolate)without needing DMA(buffer) config(delays).
Address | Bits | Name | Type | Default | Description | |
DWORD | BYTE | |||||
0x0000 | 0x0000 | REG_VERSION | Version Register | |||
---|---|---|---|---|---|---|
[31:0] | VERSION | RO | 0x00 | Version number | ||
0x0001 | 0x0004 | REG_SCRATCH | Scratch Register | |||
[31:0] | SCRATCH | RW | 0x00 | Scratch register | ||
0x0010 | 0x0040 | REG_ARBITRARY_INTERPOLATION_RATIO_A | Control Arbitrary Interpolation Ratio for Channel A | |||
[31:0] | FILTERED_INTERPOLATION | RW | 0x00 | Set the arbitrary zero-order hold interpolation ratio at the end of the interpolation chain | ||
0x0011 | 0x0044 | REG_INTERPOLATION_RATIO_A | Control Filtered Interpolation for Channel A | |||
[2:0] | FILTERED_INTERPOLATION | RW | 0x00 | Enables the filtered interpolation: 0: No filtered interpolation 1: Interpolation by 10. Result should be corrected by a 1.531 factor 2: Interpolation by 100. Result should be corrected by a 1.168 factor 3: Interpolation by 1000. Result should be corrected by a 1.783 factor 6: Interpolation by 10000. Result should be corrected by a 1.360 factor 7: Interpolation by 100000. Result should be corrected by a 1.038 factor default: No filtered interpolation |
||
0x0012 | 0x0048 | REG_ARBITRARY_INTERPOLATION_RATIO_B | Control Arbitrary Interpolation Ratio for Channel B | |||
[31:0] | FILTERED_INTERPOLATION | RW | 0x00 | Set the arbitrary zero-order hold interpolation ratio at the end of the interpolation chain | ||
0x0013 | 0x004c | REG_INTERPOLATION_RATIO_B | Control Filtered Interpolation for Channel B | |||
[2:0] | FILTERED_INTERPOLATION | RW | 0x00 | Enables the filtered interpolation: 0: No filtered interpolation 1: Interpolation by 10. Result should be corrected by a 1.531 factor 2: Interpolation by 100. Result should be corrected by a 1.168 factor 3: Interpolation by 1000. Result should be corrected by a 1.783 factor 6: Interpolation by 10000. Result should be corrected by a 1.360 factor 7: Interpolation by 100000. Result should be corrected by a 1.038 factor default: No filtered interpolation |
||
0x0014 | 0x0050 | REG_FLAGS | Control Flags | |||
[5] | CH_B_RAW_TRANSFER_EN | RW | 0 | If set to 1, The core will ignore the DMA data and it will only send the raw data from reg 0x19 - 0x64 | ||
[4] | CH_A_RAW_TRANSFER_EN | RW | 0 | If set to 1, The core will ignore the DMA data and it will only send the raw data from reg 0x19 - 0x64 | ||
[3] | FLUSH_DMA | RW | 0 | When set to 1, whenever the DMAs are stopped by signal/flag dma_transfer_suspend, the remaining data inside the DMAs will be flushed out and the data sent by the core is the raw data, see REG 0x19 | ||
[2] | STOP_SYNC_CHANNELS | RW | 0 | when is set to 1, in case one DMA stopes, the other DMA is stopped. Either because the first DMA is in non-cyclic mode and transmission ends, or the DMA is stopped by it's enable flag. This flag must be clear when only one channel is active | ||
[1] | START_SYNC_CHANNELS | RW | 0 | If set to 1, The core waits for both channel DMA's to have valid data, and only then the transmission is started. When only one channel is active, this flag must be set to 0, otherwise the active DMA will never get the ready signal. | ||
[0] | SUSPEND_TRANSFER | RW | 0 | If set to 1, the interpolation filters are in reset and no data is requested. from the DMA. Can be used to synchronize data transfer from two different DMAs. The above is only valid if FLUSH_DMA is not set. See FLUSH_DMA for more info. | ||
0x0015 | 0x0054 | REG_CONFIG | Configuration Register | |||
[1] | CORRECTION_ENABLE_B | RW | 0x00 | If set to 1, correction is enabled on channel B. The input data will be multiplied with the value from the CORRECTION_COEFFICIENT_B register. | ||
[0] | CORRECTION_ENABLE_A | RW | 0x00 | If set to 1, correction is enabled on channel A. The input data will be multiplied with the value from the CORRECTION_COEFFICIENT_A register. | ||
0x0016 | 0x0058 | REG_CORRECTION_COEFFICIENT_A | Correction Coefficient A | |||
[15:0] | CORRECTION_COEFFICIENT | RW | 0x00 | Scale correction (if equipped) coefficient for channel A. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. | ||
0x0017 | 0x005c | REG_CORRECTION_COEFFICIENT_B | Correction Coefficient B | |||
[15:0] | CORRECTION_COEFFICIENT | RW | 0x00 | Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. | ||
0x0018 | 0x0060 | REG_TRIGGER_CONFIG | Trigger configuration | |||
[19] | EN_TRIGGER_LA | RW | 0x00 | Enable trigger from Logic Analyzer | ||
[18] | EN_TRIGGER_ADC | RW | 0x00 | Enable trigger from ADC | ||
[17] | EN_TRIGGER_TO | RW | 0x00 | Enable trigger from To | ||
[16] | EN_TRIGGER_TI | RW | 0x00 | Enable trigger from Ti | ||
[9:8] | FALL_EDGE | RW | 0x00 | Falling edge triggering for TRIGGER[0](Ti) or TRIGGER[1](To) pin | ||
[7:6] | RISE_EDGE | RW | 0x00 | Rising edge triggering for TRIGGER[0](Ti) or TRIGGER[1](To) pin | ||
[5:4]] | ANY_EDGE | RW | 0x00 | Any edge triggering for TRIGGER[0](Ti) or TRIGGER[1](To) pin | ||
[3:2] | HIGH_LEVEL | RW | 0x00 | High level triggering for TRIGGER[0](Ti) or TRIGGER[1](To) pin | ||
[1:0] | LOW_LEVEL | RW | 0x00 | Low level triggering for TRIGGER[0](Ti) or TRIGGER[1](To) pin | ||
0x0019 | 0x0064 | REG_RAW_CHANNEL_DATA | ||||
[31:16] | CHANNEL_B_DATA | RW | 0x00 | Channel a raw data | ||
[15:0] | CHANNEL_A_DATA | RW | 0x00 | Channel b raw data | ||
Fri Sep 4 17:18:13 2020 |