This is an old revision of the document!
Parameter name | Default value | Description |
---|---|---|
CMOS_LVDS_N | 0 | Source synchronous interface type; 0 - LVDS ; 1 - CMOS |
TDD_DISABLE | 0 | Controls the insertion of the TDD core. If set the TDD controller won't be part of the implementation. |
DDS_DISABLE | 0 | If resource utilization is a concern, by setting this parameter you can remove the dual tone DDS logic from the Tx channels. This will reduce resource utilization significantly but loosing the ability to generate a test tone. |
INDEPENDENT_1R1T_SUPPORT | 1 | 0 - Rx2 (adc_2_*) and Tx2 (dac_2_*) data channels will be disabled; RX2 TPL, TX2 TPL cores are disabled. 1 - Allows independent control of Rx2/Tx2 PHY either from Rx12/Tx12 TPL or Rx2/Tx2 TPL blocks; |
COMMON_2R2T_SUPPORT | 1 | 0 - puts the Rx12/Tx12 TPL in R1_MODE, having access only to Rx1/Tx1 PHYs; 1 - Allows Rx12/Tx12 TPL to operate in 2R 2T mode having control over Rx2/Tx2 PHY |
RX_USE_BUFG | 0 | Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Rx clock path. Useful if user logic does not fits in a clock region. |
TX_USE_BUFG | 0 | Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Tx clock path. Useful if user logic does not fits in a clock region. |
USE_RX_CLK_FOR_TX | 0 | In case the received clock on the Tx source synchronous interface is not routed to clock capable pins, when setting this to 1 the Rx clock will be used to drive the Tx interface |
IO_DELAY_GROUP | “dev_if_delay_group” | Used in case of Xilinx devices. Identifier of the IODELAYCTRL cell. |
FPGA_TECHNOLOGY | 0 | Auto populated by IPI. |
FPGA_FAMILY | 0 | Auto populated by IPI. |
SPEED_GRADE | 0 | Auto populated by IPI. |
DEV_PACKAGE | 0 | Auto populated by IPI. |
The register map of the core contains instances of several generic register maps like ADC common, ADC channel, DAC common, DAC channel etc. The following table presents the base addresses of each instance, after that can be found the detailed description of each generic register map. The absolute address of a register should be calculated by adding the instance base address to the registers relative address.
Address | Name | Description | |||
DWORD | BYTE | ||||
0x0000 | 0x0000 | RX1 BASE | See the Base (common to all cores) table for more detail | ||
---|---|---|---|---|---|
0x0000 | 0x0000 | RX1 COMMON | See the ADC Common table for more detail | ||
0x0000 | 0x0000 | RX1 CHANNELS | See the ADC Channel table for more detail | ||
0x0200 | 0x0800 | RX1 Delay control | See the IO Delay Control table for more detail | ||
0x0400 | 0x1000 | RX2 BASE | See the Base (common to all cores) table for more detail | ||
0x0400 | 0x1000 | RX2 COMMON | See the ADC Common table for more detail | ||
0x0400 | 0x1000 | RX2 CHANNELS | See the ADC Channel table for more detail | ||
0x0600 | 0x1800 | RX2 Delay control | See the IO Delay Control table for more detail | ||
0x0800 | 0x2000 | TX1 BASE | See the Base (common to all cores) table for more detail | ||
0x0800 | 0x2000 | TX1 COMMON | See the DAC Common table for more detail | ||
0x0800 | 0x2000 | TX1 CHANNELS | See the DAC Channel table for more detail | ||
0x1000 | 0x4000 | TX2 BASE | See the Base (common to all cores) table for more detail | ||
0x1000 | 0x4000 | TX2 COMMON | See the DAC Common table for more detail | ||
0x1000 | 0x4000 | TX2 CHANNELS | See the DAC Channel table for more detail | ||
0x1200 | 0x4800 | TDD1 | See the Transceiver TDD Control table for more detail | ||
0x1300 | 0x4C00 | TDD2 | See the Transceiver TDD Control table for more detail |
The following operation modes are supported by the physical layer. CMOS (CSSI) and LVDS (LSSI) selection is done through synthesis parameter. Other parameter (column B, G, H) can be run time modified preferably while the core is in reset.
A | B | C | D | E | F | G | H |
---|---|---|---|---|---|---|---|
CSSI 1-lane | 1 | 32 | 80 | 80 | 2.5 | SDR | 8 |
CSSI 1-lane | 1 | 32 | 160 | 80 | 5 | DDR | 4 |
CSSI 1-lane* | 1 | 16 | 80 | 80 | - | SDR | 4 |
CSSI 1-lane* | 1 | 16 | 160 | 80 | - | DDR | 2 |
CSSI 1-lane** | 1 | 8 | 80 | 80 | - | SDR | 2 |
CSSI 1-lane** | 1 | 8 | 160 | 80 | - | DDR | 1 |
CSSI 4-lane | 4 | 8 | 80 | 80 | 10 | SDR | 2 |
CSSI 4-lane | 4 | 8 | 160 | 80 | 20 | DDR | 1 |
LSSI 1-lane | 1 | 32 | 983.04 | 491.52 | 30.72 | DDR | 4 |
LSSI 2-lane | 2 | 16 | 983.04 | 491.52 | 61.44 | DDR | 2 |
* ADRV9001 data port transmit/receive 16-bit data symbols
** ADRV9001 data port transmit/receive 8-bit data symbols. In case of 8-bit and 2-bit data symbols we'll use aligned MSBs
Columns description:
The following equations apply:
where :
Since the is an integer multiple (column H) of the the interface toward the user logic has a valid qualifier which is not active on every clock cycle.
Register 0x0048 REG_CNTRL_2
Register 0x04c REG_RATECNTRL
Register 0x0044 REG_CNTRL
For Rx interfaces the source synchronous associated clock is used to sample the input data. Software configuration is required described in Configure ADC common interface section. Input delays of the FPGA or output delays of the ADRV9001 can be tuned by software for optimize sampling.
For Tx interfaces the clock received from the transceiver is used to drive the output data. Software configuration is required for clock rate selection described in Configure DAC common interface section. Input delays of the ADRV9001 can be tuned by software for optimize sampling.
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.