Wiki

This version (01 Mar 2022 10:43) was approved by Laszlo Nagy.The Previously approved version (24 Nov 2021 11:31) is available.Diff

AXI_ADRV9001/AXI_ADRV9002 Interface Core

Block diagram

Parameters

Parameter name Default value Description
CMOS_LVDS_N 0 Source synchronous interface type;
0 - LVDS ; 1 - CMOS
TDD_DISABLE 0 Controls the insertion of the TDD core. If set the TDD controller won't be part of the implementation.
DDS_DISABLE 0 If resource utilization is a concern, by setting this parameter you can remove the dual tone DDS logic from the Tx channels. This will reduce resource utilization significantly but loosing the ability to generate a test tone.
INDEPENDENT_1R1T_SUPPORT 1 0 - Rx2 (adc_2_*) and Tx2 (dac_2_*) data channels will be disabled; RX2 TPL, TX2 TPL cores are disabled.
1 - Allows independent control of Rx2/Tx2 PHY either from Rx12/Tx12 TPL or Rx2/Tx2 TPL blocks;
COMMON_2R2T_SUPPORT 1 0 - puts the Rx12/Tx12 TPL in R1_MODE, having access only to Rx1/Tx1 PHYs;
1 - Allows Rx12/Tx12 TPL to operate in 2R 2T mode having control over Rx2/Tx2 PHY
RX_USE_BUFG 0 Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Rx clock path. Useful if user logic does not fits in a clock region.
TX_USE_BUFG 0 Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Tx clock path. Useful if user logic does not fits in a clock region.
USE_RX_CLK_FOR_TX 0 In case the received clock on the Tx source synchronous interface is not routed to clock capable pins, when setting this to 1 the Rx clock will be used to drive the Tx interface
IODELAY_CTRL 1 IODELAY_CTRL parameter can have the values 0 or 1, conditioning the instantiation of the IODELAY_CTRL primitive. You can place only one IODELAY_CTRL per I/O bank, and need to set the same IO_DELAY_GROUP for the interfaces placed in that I/O bank.
IO_DELAY_GROUP “dev_if_delay_group” Used in case of Xilinx devices. Identifier of the IODELAYCTRL cell.
FPGA_TECHNOLOGY 0 Auto populated by IPI.
FPGA_FAMILY 0 Auto populated by IPI.
SPEED_GRADE 0 Auto populated by IPI.
DEV_PACKAGE 0 Auto populated by IPI.

Register Map

The register map of the core contains instances of several generic register maps like ADC common, ADC channel, DAC common, DAC channel etc. The following table presents the base addresses of each instance, after that can be found the detailed description of each generic register map. The absolute address of a register should be calculated by adding the instance base address to the registers relative address.

Register Map base addresses for axi_ad9001

Address Name Description
DWORD BYTE
0x0000 0x0000 RX1 BASE See the Base (common to all cores) table for more detail
0x0000 0x0000 RX1 COMMON See the ADC Common table for more detail
0x0000 0x0000 RX1 CHANNELS See the ADC Channel table for more detail
0x0200 0x0800 RX1 Delay control See the IO Delay Control table for more detail
0x0400 0x1000 RX2 BASE See the Base (common to all cores) table for more detail
0x0400 0x1000 RX2 COMMON See the ADC Common table for more detail
0x0400 0x1000 RX2 CHANNELS See the ADC Channel table for more detail
0x0600 0x1800 RX2 Delay control See the IO Delay Control table for more detail
0x0800 0x2000 TX1 BASE See the Base (common to all cores) table for more detail
0x0800 0x2000 TX1 COMMON See the DAC Common table for more detail
0x0800 0x2000 TX1 CHANNELS See the DAC Channel table for more detail
0x1000 0x4000 TX2 BASE See the Base (common to all cores) table for more detail
0x1000 0x4000 TX2 COMMON See the DAC Common table for more detail
0x1000 0x4000 TX2 CHANNELS See the DAC Channel table for more detail
0x1200 0x4800 TDD1 See the Transceiver TDD Control table for more detail
0x1300 0x4C00 TDD2 See the Transceiver TDD Control table for more detail

Base (common to all cores)

Click to expand regmap

ADC Common (axi_ad*)

Click to expand regmap

ADC Channel (axi_ad*)

Click to expand regmap

DAC Common (axi_ad)

Click to expand regmap

DAC Channel (axi_ad*)

Click to expand regmap

IO Delay Control (axi_ad*)

Click to expand regmap

Transceiver TDD Control (axi_ad*)

Click to expand regmap

Physical Interface

The following operation modes are supported by the physical layer. CMOS (CSSI) and LVDS (LSSI) selection is done through synthesis parameter. Other parameter (column B, G, H) can be run time modified preferably while the core is in reset.

A B C D E F G H
CSSI 1-lane 1 32 80 80 2.5 SDR 8
CSSI 1-lane 1 32 160 80 5 DDR 4
CSSI 1-lane* 1 16 80 80 - SDR 4
CSSI 1-lane* 1 16 160 80 - DDR 2
CSSI 1-lane** 1 8 80 80 - SDR 2
CSSI 1-lane** 1 8 160 80 - DDR 1
CSSI 4-lane 4 8 80 80 10 SDR 2
CSSI 4-lane 4 8 160 80 20 DDR 1
LSSI 1-lane 1 32 983.04 491.52 30.72 DDR 4
LSSI 2-lane 2 16 983.04 491.52 61.44 DDR 2

* ADRV9001 data port transmit/receive 16-bit data symbols

** ADRV9001 data port transmit/receive 8-bit data symbols. In case of 8-bit and 2-bit data symbols we'll use aligned MSBs

Columns description:

  • A - SSI Modes
  • B - Data Lanes Per Channel
  • C - Serialization factor Per data lane
  • D - Max data lane rate(MHz)
  • E - Max Clock rate (MHz)
  • F - Max Sample Rate for I/Q (MHz)
  • G - Data Type
  • H - User Interface Clock to Sample Clock ratio (aka DDS Rate) for Xilinx devices

The following equations apply:

MaxDataLaneRate = MaxSampleRateForIQ*16*2/DataLanesPerChannel

MaxClockRate = MaxDataLaneRate / (1+(DataType = DDR))

UserInterfaceClock = MaxClockRate / InternalDivider

UserInterfaceClock = MaxSampleRateForIQ*32/DataLanesPerChannel*(1+(DataType = DDR))*InternalDivider

DDS rate = 32/DataLanesPerChannel*(1+(DataType = DDR))*InternalDivider

where :

  • MaxDataLaneRate - number of bits transferred in a second per active lane
  • MaxClockRate - represents the source synchronous interface clock frequency
  • UserInterfaceClock - represents the frequency of the clock the user interface logic is connected
  • InternalDivider - represents the division factor the source synchronous interface clock is divided to get the user interface clock. This is implementation specific. Xilinx CMOS and LVDS = 4; Intel CMOS = 1

Since the UserInterfaceClock is an integer multiple (column H) of the MaxSampleRateForIQ the interface toward the user logic has a valid qualifier which is not active on every clock cycle.

Configure DAC common interface

Register 0x0048 REG_CNTRL_2

  • [12:8] - NUM_LANES (new) - number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)
  • [14] - SYMB_8_16B (new) - select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)
  • [15] - SYMB_OP (new) - select symbol data format mode
  • [16] - SDR_DDR_N (new) - interface type (1 represents SDR, 0 represents DDR)

Register 0x04c REG_RATECNTRL

  • [7:0] RATE - must be set according to column H of the table

Configure ADC common interface

Register 0x0044 REG_CNTRL

  • [12:8] - NUM_LANES (new) - number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)
  • [14] - SYMB_8_16B (new) - select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)
  • [15] - SYMB_OP (new) - select symbol data format mode
  • [16] - SDR_DDR_N (new) - interface type ( 1 represents SDR, 0 represents DDR)

Requirements

  • Rx1 clock and Rx2 clock should be length matched
  • Clock and data in SSI interface must be length matched

Xilinx Physical interface

RX Component mode

For Rx interfaces the source synchronous associated clock is used to sample the input data. Software configuration is required described in Configure ADC common interface section. Input delays of the FPGA or output delays of the ADRV9001 can be tuned by software for optimize sampling.

TX Using dedicated clock

For Tx interfaces the clock received from the transceiver is used to drive the output data. Software configuration is required for clock rate selection described in Configure DAC common interface section. Input delays of the ADRV9001 can be tuned by software for optimize sampling.

Support

Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.

resources/eval/user-guides/adrv9002/axi_adrv9002.txt · Last modified: 01 Mar 2022 10:35 by Laszlo Nagy