This is an old revision of the document!
The AD7616 is a 16-bit, data acquisition system (DAS) that supports dual simultaneous sampling of 16 channels. The AD7616 operates from a single 5 V supply and can accommodate ±10 V, ±5 V, and ±2.5 V true bipolar input signals while sampling at throughput rates up to 1 MSPS per channel pair with 90 dB SNR. Higher SNR performance can be achieved with the on-chip oversampling mode; 92 dB for an oversampling ratio of 2.
The input clamp protection circuitry can tolerate voltages up to ±20 V. The AD7616 has 1 MΩ analog input impedance regardless of sampling frequency. The single supply operation, on-chip filtering, and high input impedance eliminate the need for driver op-amps and external bipolar supplies.
Each device contains analog input clamp protection, a dual, 16-bit charge redistribution successive approximation analog-to-digital converter (ADC), a flexible digital filter, a 2.5 V reference and reference buffer, and high-speed serial and parallel interfaces.
Applications:
In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design in general.
In the axi_ad7616's wiki page, can be found a detailed description of the core.
The data path of the HDL design is simple as follows:
In order to build the HDL design the user has to go through the following steps:
Before power-up the board, the user has to choose the required device interface and setup, in function of the required interface mode some hardware modification needs to be done on the board and/or Tcl script:
1) In case of the SERIAL interface:
set ad7616_if 0
2) In case of the PARALLEL interface:
set ad7616_if 1
Function | Description |
---|---|
int32_t ad7616_read(ad7616_dev *dev, uint8_t reg_addr, uint16_t *reg_data); | SPI read from device. |
int32_t ad7616_write(ad7616_dev *dev, uint8_t reg_addr, uint16_t reg_data); | SPI write to device. |
int32_t ad7616_read_mask(ad7616_dev *dev, uint8_t reg_addr, uint16_t mask, uint16_t *data); | SPI read from device using a mask. |
int32_t ad7616_write_mask(ad7616_dev *dev, uint8_t reg_addr, uint16_t mask, uint16_t data); | SPI write to device using a mask. |
int32_t ad7616_spi_read(ad7616_dev *dev, uint8_t reg_addr, uint16_t *reg_data); | SPI read from device. |
int32_t ad7616_spi_write(ad7616_dev *dev, uint8_t reg_addr, uint16_t reg_data); | SPI write to device. |
int32_t ad7616_par_read(ad7616_dev *dev, uint8_t reg_addr, uint16_t *reg_data); | PAR read from device. |
int32_t ad7616_par_write(ad7616_dev *dev, uint8_t reg_addr, uint16_t reg_data); | PAR write to device. |
int32_t ad7616_reset(ad7616_dev *dev); | Perform a full reset of the device. |
int32_t ad7616_set_range(ad7616_dev *dev, ad7616_ch ch, ad7616_range range); | Set the analog input range for the selected analog input channel. |
int32_t ad7616_set_mode(ad7616_dev *dev, ad7616_mode mode); | Set the operation mode (software or hardware). |
int32_t ad7616_set_oversampling_ratio(ad7616_dev *dev, ad7616_osr osr); | Set the oversampling ratio. |
int32_t ad7616_setup(ad7616_dev **device, adc_core *core, ad7616_init_param init_param); | Initialize the device. |
typedef enum { AD7616_SW, AD7616_HW, } ad7616_mode; typedef enum { AD7616_SERIAL, AD7616_PARALLEL, } ad7616_interface; typedef enum { AD7616_VA0, AD7616_VA1, AD7616_VA2, AD7616_VA3, AD7616_VA4, AD7616_VA5, AD7616_VA6, AD7616_VA7, AD7616_VB0, AD7616_VB1, AD7616_VB2, AD7616_VB3, AD7616_VB4, AD7616_VB5, AD7616_VB6, AD7616_VB7, } ad7616_ch; typedef enum { AD7616_2V5 = 1, AD7616_5V = 2, AD7616_10V = 3, } ad7616_range; typedef enum { AD7616_OSR_0, AD7616_OSR_2, AD7616_OSR_4, AD7616_OSR_8, AD7616_OSR_16, AD7616_OSR_32, AD7616_OSR_64, AD7616_OSR_128, } ad7616_osr; typedef struct { /* SPI */ spi_device spi_dev; /* GPIO */ gpio_device gpio_dev; int8_t gpio_hw_rngsel0; int8_t gpio_hw_rngsel1; int8_t gpio_reset; int8_t gpio_os0; int8_t gpio_os1; int8_t gpio_os2; /* Device Settings */ ad7616_interface interface; ad7616_mode mode; ad7616_range va[8]; ad7616_range vb[8]; ad7616_osr osr; adc_core *core; } ad7616_dev; typedef struct { /* SPI */ uint8_t spi_chip_select; spi_mode spi_mode; spi_type spi_type; uint32_t spi_device_id; /* GPIO */ gpio_type gpio_type; uint32_t gpio_device_id; int8_t gpio_hw_rngsel0; int8_t gpio_hw_rngsel1; int8_t gpio_reset; int8_t gpio_os0; int8_t gpio_os1; int8_t gpio_os2; /* Device Settings */ ad7616_mode mode; ad7616_range va[8]; ad7616_range vb[8]; ad7616_osr osr; } ad7616_init_param; |
To run the application the user has to create an Empty Application Project using Xilinx SDK, and have to copy all the design sources to the sw directory. (see SDK Software Setup for more detailed instructions) Another option for building the no-OS is using the Makefile. (see Build no-OS with GNU make)
Questions? Feel free to ask your questions in EngineerZone support forums.