Some applications (
e.g. FMCOMMSx), when a Microblaze processor is used, requires an increased HEAP size for dynamic memory allocation. Make sure the HEAP size is at least
0x100000.
//#define XILINX
#define ALTERA
After the FPGA was programmed, we need to create a new Run configuration, by selecting Run → Run Configurations…, in the Run Configuration windows select the Xilinx C/C++ application (System Debugger) and click at the New Configuration button at the upper left corner.
If your target carrier has a Zync SoC, make sure, that you specify the Initialization file, and select the Run ps7_init and Run ps7_post_config options.
The output of the example program can be viewed in the SDK console by enabling the Connect STDIO Console option and setting the baud rate of the
UART port to 115200.
As an alternative a
UART terminal can be used to capture the output of the example program. The number of used
UART port depends on the computer's configuration. The following settings must be used in the
UART terminal:
Baud Rate: 115200bps
Data: 8 bit
Parity: None
Stop bits: 1 bit
Flow Control: none