This is an old revision of the document!
This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the FMCOMMS8 on ADRV9009-ZU11EG and ZCU102.
Instructions on how to build the ZynqMP / MPSoC Linux kernel and devicetrees from source can be found here:
The project will be release as part of 2019_r2 release.Before then, the SD image for 2019_r1 can be used.
Details on how to write the SD card can be found here: Zynq & Altera SoC Quick Start Guide including the 2019_R1 image.
After writing the image, on the boot partition FMCOMMS8 specific files can be added from:
Copy:
→ To the root directory of the SD-Card FAT32 BOOT partition.
OR
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
ADRV9009-ZU11EG
System on Module to the ADRV2CRR-FMC
carrier board.P11
P8
(Micro USB) to your host PC.P9
P15
.S13
, S14
, S15
, S16
. See picture below.ADRV2CRR-FMC
for SD BOOT from carrier using S9
. See picture below.S12
.This specifies any shell prompt running on the target
Release 2018.3 Mar 9 2020 - 12:23:37 U-Boot 2018.01-21435-g099c929 (May 28 2019 - 08:42:11 +0000) Analog Devices Inc. ADR9009-ZU11EG I2C: ready DRAM: 4 GiB EL Level: EL2 Chip ID: zu11eg MMC: sdhci@ff170000: 0 (SD) *** Warning - bad CRC, using default environment In: serial@ff010000 Out: serial@ff010000 Err: serial@ff010000 Bootmode: LVL_SHFT_SD_MODE1 Net: ZYNQ GEM: ff0b0000, phyaddr 1, interface sgmii i2c_mux_set: could not set mux: id: 5 chip: 74 channel: 0 I2C EEPROM MAC address read failed Warning: ethernet@ff0b0000 (eth1) using random MAC address - 62:74:59:ed:d4:0d eth1: ethernet@ff0b0000ZYNQ GEM: ff0e0000, phyaddr 0, interface rgmii-id I2C EEPROM MAC address read failed Warning: ethernet@ff0e0000 (eth0) using random MAC address - 42:d0:73:57:9c:b7 , eth0: ethernet@ff0e0000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Device: sdhci@ff170000 Manufacturer ID: 27 OEM: 5048 Name: APUSD Tran Speed: 50000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 7.4 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes reading uEnv.txt 416 bytes read in 11 ms (36.1 KiB/s) Loaded environment from uEnv.txt Importing environment from SD ... Running uenvcmd ... Copying Linux from SD to RAM... ** No boot file defined ** reading system.dtb 78202 bytes read in 27 ms (2.8 MiB/s) reading Image 18403840 bytes read in 1202 ms (14.6 MiB/s) ## Flattened Device Tree blob at 04000000 Booting using the fdt blob at 0x4000000 Loading Device Tree to 000000000ffe9000, end 000000000ffff179 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.0-g85e0210 (acostina@romlx2.adlk.analog.com) (gcc version 8.2.0 (GCC)) #154 SMP Mon Mar 9 15:02:46 GMT 2020 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] Machine model: Analog Devices ADRV9009-ZU11EG Rev.B [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8') [ 0.000000] bootconsole [cdns0] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] random: fast init done . . . [ 4.217212] adrv9009 spi1.0: adrv9009_probe : enter [ 4.222255] adrv9009 spi1.1: adrv9009_probe : enter [ 4.227253] adrv9009 spi2.0: adrv9009_probe : enter [ 4.232258] adrv9009 spi2.1: adrv9009_probe : enter [ 4.291617] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A40000 mapped to 0xffffff80095a5000. Number of lanes: 8. [ 4.306239] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A60000 mapped to 0xffffff80095ad000. Number of lanes: 8. [ 4.320207] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0x84A20000 mapped to 0xffffff80095b5000. Number of lanes: 16. [ 4.334717] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 4.345022] macb ff0b0000.ethernet: Not enabling partial store and forward [ 4.352352] libphy: MACB_mii_bus: probed [ 4.368115] mmc0: new high speed SDHC card at address 0007 [ 4.373751] mmcblk0: mmc0:0007 APUSD 7.42 GiB [ 4.378802] mmcblk0: p1 p2 p3 [ 4.427364] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 13 (62:74:59:ed:d4:0d) [ 4.437185] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL) [ 4.451429] adrv9009 spi1.0: adrv9009_probe : enter [ 4.458924] adrv9009 spi1.0: ADIHAL_resetHw at index [ 4.787278] [drm] Cannot find any crtc or sizes [ 4.858803] random: crng init done [ 12.003164] adrv9009 spi1.0: TAL_DEFRAMER_A deframerStatus 0x12 [ 12.009165] adrv9009 spi1.0: TAL_FRAMER_A framerStatus 0x21 [ 12.014823] adrv9009 spi1.0: TAL_FRAMER_B framerStatus 0x29 [ 12.124377] adrv9009 spi1.0: adrv9009_probe: adrv9009-x4 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 12.135923] adrv9009 spi1.1: adrv9009_probe : enter [ 12.143165] adrv9009 spi1.1: ADIHAL_resetHw at index [ 19.673166] adrv9009 spi1.1: TAL_FRAMER_A framerStatus 0x1 [ 19.678735] adrv9009 spi1.1: TAL_FRAMER_B framerStatus 0x9 [ 19.788165] adrv9009 spi1.1: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 19.799446] adrv9009 spi2.0: adrv9009_probe : enter [ 19.806693] adrv9009 spi2.0: ADIHAL_resetHw at index [ 27.596084] adrv9009 spi2.0: TAL_FRAMER_A framerStatus 0x1 [ 27.601663] adrv9009 spi2.0: TAL_FRAMER_B framerStatus 0x9 [ 27.611311] adrv9009 spi2.0: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 27.622593] adrv9009 spi2.1: adrv9009_probe : enter [ 27.629845] adrv9009 spi2.1: ADIHAL_resetHw at index [ 28.371288] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 6 desynced (15 errors), restarting link [ 28.380066] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 7 desynced (8 errors), restarting link [ 28.488779] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 6 desynced (26 errors), restarting link [ 28.497558] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 7 desynced (354 errors), restarting link [ 29.491289] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 7 desynced (102 errors), restarting link [ 35.763278] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 6 desynced (31 errors), restarting link [ 35.772054] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 7 desynced (22 errors), restarting link [ 35.883345] adrv9009 spi2.1: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 35.912777] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0xffffff800beb0000, probed DDS ADRV9009-X4 [ 35.927747] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 35.958482] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0xffffff800bec8000, probed ADC ADRV9009-X4 as MASTER [ 35.971835] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 35.982836] input: gpio_keys as /devices/platform/gpio_keys/input/input0 [ 35.989688] hctosys: unable to open rtc device (rtc0) [ 35.995840] ALSA device list: [ 35.998794] No soundcards found. [ 36.002623] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 36.667288] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 36.675383] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 36.689156] devtmpfs: mounted [ 36.692213] Freeing unused kernel memory: 512K [ 36.755282] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 6 desynced (12 errors), restarting link [ 36.764059] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 7 desynced (9 errors), restarting link Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 37.059089] init: hwclock main process (1822) terminated with status 1 * Setting up X socket directories... [ OK ] * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting * Starting IIO Daemon iiod [ OK ] Last login: Thu Jan 1 00:00:43 UTC 1970 on ttyPS0 Welcome to Linaro 14.04 (GNU/Linux 4.14.0-g85e0210 aarch64) * Documentation: https://wiki.analog.com/ https://ez.analog.com/ New release '16.04.6 LTS' available. Run 'do-release-upgrade' to upgrade to it.
This specifies any shell prompt running on the target
root@analog:~# iio_info | grep iio:device iio:device0: ams iio:device1: hmc7044-car iio:device10: axi-adrv9009-rx-obs-hpc (buffer capable) iio:device11: axi-adrv9009-tx-hpc (buffer capable) iio:device12: axi-adrv9009-rx-hpc (buffer capable) iio:device2: hmc7044-ext iio:device3: hmc7044-fmc iio:device4: adm1177 iio:device5: hmc7044 iio:device6: adrv9009-phy iio:device7: adrv9009-phy-b iio:device8: adrv9009-phy-c iio:device9: adrv9009-phy-d
After changing the clock structure, a sysref request from HMC7044-CAR needs to be issued in order for the clock tree to be properly synchronized. At boot, the clock tree is not synchronized.
This specifies any shell prompt running on the target
root@analog:~# iio_attr -q -d hmc7044-car sysref_request 1
This specifies any shell prompt running on the target
root@analog:~# iio_attr -q -D hmc7044 status --- PLL1 --- Status: Locked Using: CLKIN1 @ 122880000 Hz PFD: 30720 kHz --- PLL2 --- Status: Locked (Synchronized) Frequency: 2949120000 Hz SYSREF Status: Valid & Locked SYNC Status: Synchronized Lock Status: PLL1 & PLL2 Locked root@analog:~# iio_attr -q -D hmc7044-fmc status --- PLL1 --- Status: Locked Using: CLKIN1 @ 122880000 Hz PFD: 30720 kHz --- PLL2 --- Status: Locked (Synchronized) Frequency: 2949120000 Hz SYSREF Status: Valid & Locked SYNC Status: Synchronized Lock Status: PLL1 & PLL2 Locked root@analog:~# iio_attr -q -D hmc7044-car status --- PLL1 --- Status: Holdover Using: CLKIN1 @ 30720000 Hz PFD: 30720 kHz --- PLL2 --- Status: Locked (Unsynchronized) Frequency: 2949120000 Hz SYSREF Status: Valid & Locked SYNC Status: Unsynchronized Lock Status: Unlocked
After the HMC7044s are synchronized, a MCS sync procedure should be issued in order to synchronize the ADRV9009 LOs. This can be done through IIO-Oscilloscope, by pressing the MCS Sync button.
Using the JESD204B Status Utility
This specifies any shell prompt running on the target
root@analog:~# TERM=vt100 jesd_status -s (DEVICES) Found 3 JESD204 Link Layer peripherals (0): 84a30000.axi-jesd204-tx (1): 84a50000.axi-jesd204-rx (2): 84a70000.axi-jesd204-rx (STATUS) (0) (1) (2) Link is enabled enabled enabled Link Status DATA DATA DATA Measured Link Clock 122.879 245.758 122.878 Reported Link Clock 122.880 245.760 122.880 Lane rate 4915.200 9830.400 4915.200 Lane rate / 40 122.880 245.760 122.880 LMFC rate 7.680 7.680 3.840 SYSREF captured Yes Yes Yes SYSREF alignment error No No No SYNC~ deasserted (LANE STATUS) (1) (2) Lane# 0 1 2 3 4 5 6 7 0 1 2 3 4 5 6 7 Errors 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Latency (Multiframes/Octets) 2/81 2/78 2/73 2/78 2/80 2/81 2/84 2/83 2/54 2/53 2/52 2/54 2/54 2/53 2/57 2/55 CGS State DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA DATA Initial Frame Sync Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Initial Lane Alignment Sequence Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes Yes
For ZCU102, FMCOMMS8 board connects to the HPC0 connector. The carrier setup requires power, UART (115200), ethernet (Linux), DisplayPort and/or JTAG connections.
This specifies any shell prompt running on the target
Xilinx Zynq MP First Stage Boot Loader Release 2018.3 Mar 9 2020 - 12:23:38 NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000 NOTICE: BL31: Secure code at 0x0 NOTICE: BL31: Non secure code at 0x8000000 NOTICE: BL31: v1.5(release):xilinx-v2018.3 NOTICE: BL31: Built : 15:00:47, Mar 18 2019 PMUFW: v1.1 U-Boot 2018.01 (Jun 29 2018 - 13:20:51 +0200) Xilinx ZynqMP ZCU102 rev1.0 I2C: ready DRAM: 4 GiB EL Level: EL2 Chip ID: zu9eg MMC: sdhci@ff170000: 0 (SD) *** Warning - bad CRC, using default environment In: serial@ff000000 Out: serial@ff000000 Err: serial@ff000000 Bootmode: LVL_SHFT_SD_MODE1 Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id Warning: ethernet@ff0e0000 using MAC address from ROM eth0: ethernet@ff0e0000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Device: sdhci@ff170000 Manufacturer ID: 27 OEM: 5048 Name: APUSD Tran Speed: 50000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 7.4 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes reading uEnv.txt 416 bytes read in 11 ms (36.1 KiB/s) Loaded environment from uEnv.txt Importing environment from SD ... ## Error: Can't overwrite "ethaddr" himport_r: can't insert "ethaddr=56:7f:a2:a4:16:78" into hash table Running uenvcmd ... Copying Linux from SD to RAM... ** No boot file defined ** reading system.dtb 65923 bytes read in 26 ms (2.4 MiB/s) reading Image 18328064 bytes read in 1208 ms (14.5 MiB/s) ## Flattened Device Tree blob at 04000000 Booting using the fdt blob at 0x4000000 Loading Device Tree to 000000000ffec000, end 000000000ffff182 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.0-g338c0a9 (acostina@romlx2.adlk.analog.com) (gcc version 8.2.0 (GCC)) #153 SMP Mon Mar 9 12:28:26 GMT 2020 . . . [ 2.318130] axi_adxcvr 85a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x85A40000 mapped to 0xffffff800949d000. Number of lanes: 4. [ 2.326997] axi_adxcvr 85a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x85A60000 mapped to 0xffffff80094a5000. Number of lanes: 4. [ 2.339170] axi_adxcvr 85a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0x85A20000 mapped to 0xffffff80094ad000. Number of lanes: 8. . . . [ 12.329405] adrv9009 spi1.0: TAL_FRAMER_A framerStatus 0x21 [ 12.335076] adrv9009 spi1.0: TAL_FRAMER_B framerStatus 0x29 [ 12.344932] adrv9009 spi1.0: adrv9009_probe: adrv9009-x2 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 12.356531] adrv9009 spi1.1: adrv9009_probe : enter [ 12.364150] adrv9009 spi1.1: ADIHAL_resetHw at index [ 13.330586] axi-jesd204-rx 85a70000.axi-jesd204-rx: Lane 2 desynced (16 errors), restarting link [ 13.339365] axi-jesd204-rx 85a70000.axi-jesd204-rx: Lane 3 desynced (14 errors), restarting link [ 13.448169] axi-jesd204-rx 85a50000.axi-jesd204-rx: Lane 2 desynced (7 errors), restarting link [ 13.456860] axi-jesd204-rx 85a50000.axi-jesd204-rx: Lane 3 desynced (9 errors), restarting link [ 20.615101] adrv9009 spi1.1: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 20.647340] cf_axi_dds 85a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x85A04000 mapped to 0xffffff800d690000, probed DDS ADRV9009-X2 [ 20.682658] cf_axi_adc 85a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x85A00000 mapped to 0xffffff800d6a8000, probed ADC ADRV9009-X2 as MASTER [ 20.696663] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 20.703559] rtc_zynqmp ffa60000.rtc: setting system clock to 2020-03-10 12:54:31 UTC (1583844871) [ 20.712654] PLL: shutdown [ 20.715274] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13 [ 20.723339] ALSA device list: [ 20.726296] #0: DisplayPort monitor [ 20.730238] axi-jesd204-rx 85a50000.axi-jesd204-rx: Lane 2 desynced (136 errors), restarting link [ 20.739106] axi-jesd204-rx 85a50000.axi-jesd204-rx: Lane 3 desynced (9 errors), restarting link [ 21.339935] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 21.348040] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 21.374271] devtmpfs: mounted [ 21.377345] Freeing unused kernel memory: 512K [ 21.618589] axi-jesd204-rx 85a70000.axi-jesd204-rx: Lane 2 desynced (22 errors), restarting link [ 21.627370] axi-jesd204-rx 85a70000.axi-jesd204-rx: Lane 3 desynced (12 errors), restarting link Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 21.874594] axi-jesd204-rx 85a50000.axi-jesd204-rx: Lane 2 desynced (51 errors), restarting link * Setting up X socket directories... [ OK ] * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting * Starting IIO Daemon iiod [ OK ] Last login: Tue Mar 10 12:44:48 UTC 2020 on ttyPS0 Welcome to Linaro 14.04 (GNU/Linux 4.14.0-g338c0a9 aarch64) * Documentation: https://wiki.analog.com/ https://ez.analog.com/ root@analog:~#
This specifies any shell prompt running on the target
root@analog:~# iio_info | grep iio:device iio:device0: ams iio:device1: hmc7044 iio:device2: ad7291 iio:device3: adrv9009-phy iio:device4: adrv9009-phy-b iio:device5: axi-adrv9009-rx-obs-hpc (buffer capable) iio:device6: axi-adrv9009-tx-hpc (buffer capable) iio:device7: axi-adrv9009-rx-hpc (buffer capable)
This specifies any shell prompt running on the target
root@analog:~# iio_attr -q -D hmc7044 status --- PLL1 --- Status: Holdover Using: CLKIN1 @ 122880000 Hz PFD: 7680 kHz --- PLL2 --- Status: Locked (Unsynchronized) Frequency: 2949120000 Hz SYSREF Status: Valid & Locked SYNC Status: Unsynchronized Lock Status: Unlocked
An MCS sync procedure should be issued in order to synchronize the ADRV9009 LOs. This can be done through IIO-Oscilloscope, by pressing the MCS Sync button.
Using the JESD204B Status Utility
This specifies any shell prompt running on the target
root@analog:~# TERM=vt100 jesd_status -s (DEVICES) Found 3 JESD204 Link Layer peripherals (0): 85a50000.axi-jesd204-rx (1): 85a70000.axi-jesd204-rx (2): 85a30000.axi-jesd204-tx (STATUS) (0) (1) (2) Link is enabled enabled enabled Link Status DATA DATA DATA Measured Link Clock 245.784 122.891 122.893 Reported Link Clock 245.760 122.880 122.880 Lane rate 9830.400 4915.200 4915.200 Lane rate / 40 245.760 122.880 122.880 LMFC rate 7.680 3.840 7.680 SYSREF captured Yes Yes Yes SYSREF alignment error No No No SYNC~ deasserted (LANE STATUS) (0) (1) Lane# 0 1 2 3 0 1 2 3 Errors 0 0 54 0 0 0 0 0 Latency (Multiframes/Octets) 2/76 2/78 2/81 2/79 2/50 2/49 2/50 2/49 CGS State DATA DATA DATA DATA DATA DATA DATA DATA Initial Frame Sync Yes Yes Yes Yes Yes Yes Yes Yes Initial Lane Alignment Sequence Yes Yes Yes Yes Yes Yes Yes Yes
The default configuration for most of the projects is to use the HDMI output, but for this project the DisplayPort is used.
In order for it to work, you should follow the steps described here: DisplayPort No Picture
After following the steps, the board should be rebooted.
Please see also here:Oscilloscope
The IIO Oscilloscope application can be used to connect to another platform that has a connected device in order to configure the device and read data from it.
Build and start osc on a network enabled Linux host.
Once the application is launched goto Settings → Connect and enter the IP address of the target in the popup window.
Even thought this is Linux, this is a persistent file systems. Care should be taken not to corrupt the file system -- please shut down things, don't just turn off the power switch. Depending on your monitor, the standard power off could be hiding. You can do this from the terminal as well with sudo shutdown -h now