This is an old revision of the document!
The HDL reference design is an embedded system built around a processor core either ARM, NIOS-II or Microblaze. A functional block diagram of the system is shown below. The high speed digital interface of the converters is handled by the JESD204B framework. Due to the system's memory interface bandwidth limitation, there are intermediary buffers in the both TX and RX data paths, in order to save and push data using high data rates. In case of the ZC706 carrier board, the RX buffer depth is 1Gbyte, and TX buffer depth is 1Mbyte. This depths can be swapped if required.
By default the AD9162 is configured in complex mode with 8 lanes (see Table 16. in data sheet), and the AD9625 is configured in generic operation mode with 8 lanes (see Table 16. in data sheet). Both JESD204 interfaces run in Subclass 0.
Other configurations can be used too, but the user needs to make sure that all the parties (clock chip, converters and FPGA JESD204 IPs) of the interface are reconfigured accordingly.
The reference design is a processor based embedded system. The sources are split into three different folders:
The reference design is a processor based (ARM or Microblaze) embedded system. A functional block diagram of the system is given above. The data path consist of the shared transceivers, then are followed by the individual JESD204B link and transport layer IP cores. The cores are programmable through an AXI-lite interface.
The digital interface consists of 8 transmit and 8 receive lanes running at 9.8304Gbps and 4.9152 respectively, by default. The transceivers interface the DAC/ADC cores at 256bits@245.76MHz and 256bit@122.88MHz respectively. The data is sent or received based on the configuration of separate transmit and receive chains.
The entry point for project creation is system_project.tcl
. Some support scripts are first loaded then the project is created. Based on the suffix of the project, the carrier board is automatically detected. The constraint files and custom modules instantiated directly in the system_top module must be added to the project files list.
system_project.tcl file:
source ../../scripts/adi_env.tcl source $ad_hdl_dir/projects/scripts/adi_project.tcl source $ad_hdl_dir/projects/scripts/adi_board.tcl adi_project_xilinx fmcomms11_zc706 adi_project_files fmcomms11_zc706 [list \ "../common/fmcomms11_spi.v" \ "system_top.v" \ "system_constr.xdc"\ "$ad_hdl_dir/library/xilinx/common/ad_iobuf.v" \ "$ad_hdl_dir/projects/common/zc706/zc706_plddr3_constr.xdc" \ "$ad_hdl_dir/projects/common/zc706/zc706_system_constr.xdc" ] adi_project_run fmcomms11_zc706
When the project is created, system_bd.tcl
is sourced. system_bd.tcl
will generate the IP Integrator system. The resulting system will be instantiated in the system_top module.
The first step is to instantiate the ZC706 base design:
source $ad_hdl_dir/projects/common/zc706/zc706_system_bd.tcl
In order to use the ADC/DAC FIFOs, the corresponding tcl files must be sourced.
source $ad_hdl_dir/projects/common/zc706/zc706_plddr3_adcfifo_bd.tcl source $ad_hdl_dir/projects/common/xilinx/dacfifo_bd.tcl
If the user wants to swap the resources allocated to the FIFO, the following scripts should be sourced instead:
source $ad_hdl_dir/projects/common/zc706/zc706_plddr3_dacfifo_bd.tcl source $ad_hdl_dir/projects/common/xilinx/adcfifo_bd.tcl
The following parameters will define the FIFO's depth. Note, if the FIFO is using the PL side DDR interface, the address width parameter can be ignored, and the FIFO will have an equal depth with the DDR memory. (e.g. in case of the ZC706 board is 1Gbyte)
# the DAC FIFO has a 500KSMP depth - 1 Mbyte set dac_fifo_address_width 15 # by default PLDDR is used (1 Gbyte), this varible should be ignored set adc_fifo_address_width 15
The next step is to source the FMCOMMS11 specific design.
source ../common/fmcomms11_bd.tcl
When using the JESD204 Framework we need to source the JESD204 support script. In this script several procedures which simplify the design are defined:
source $ad_hdl_dir/library/jesd204/scripts/jesd204.tcl
The main JESD204 configuration parameters are defined. These parameters are essential and need to respect the device side configuration in order to have a successful link bring up.
# JESD204 TX parameters set TX_NUM_OF_LANES 8 ; # L set TX_NUM_OF_CONVERTERS 2 ; # M set TX_SAMPLES_PER_FRAME 2 ; # S set TX_SAMPLE_WIDTH 16 ; # N/NP set TX_SAMPLES_PER_CHANNEL [expr [expr $TX_NUM_OF_LANES * 32 ] / \ [expr $TX_NUM_OF_CONVERTERS * $TX_SAMPLE_WIDTH]] ; # L * 32 / (M * N) # JESD204 RX parameters set RX_NUM_OF_LANES 8 ; # L set RX_NUM_OF_CONVERTERS 1 ; # M set RX_SAMPLES_PER_FRAME 4 ; # S set RX_SAMPLE_WIDTH 16 ; # N/NP
The physical layer is responsible for instantiating and configuring the high speed serial transceivers in the FPGA. The physical layer is implemented with the use of two modules: AXI_ADXCVR and UTIL_ADXCVR. AXI_ADXCVR provides an AXI interface for performing DRP reads and writes to the transceivers, allowing for dynamic reconfiguration. Given that the hardware implements 8 data lines, that's how we'll configure the NUM_OF_LANES parameter. QPLL_ENABLE parameter gives control to this IP of the QPLL reconfiguration for the Transceiver QUAD. If the QUAD is shared with other RX IPs (as it is in this design), the second ADXCVR IP will need to have QPLL_ENABLE set to 0.
ad_ip_instance axi_adxcvr axi_ad9162_xcvr [list \ NUM_OF_LANES 8 \ QPLL_ENABLE 1 \ TX_OR_RX_N 1 \ ]
Instantiation of the ADC transceiver controller. For this IP, QPLL_ENABLE is set to 0.
ad_ip_instance axi_adxcvr axi_ad9625_xcvr [list \ NUM_OF_LANES 8 \ QPLL_ENABLE 0 \ TX_OR_RX_N 0 \ ]
Given that the IP uses the same QUAD as the DAC, performing channel reconfiguration may affect the DAC and vice versa. When using the JESD204B framework, this is taken into consideration by software.
The actual transceiver blocks are instantiated in UTIL_ADXCVR.
ad_ip_instance util_adxcvr util_fmcomms11_xcvr [list \ QPLL_FBDIV 0x120 \ CPLL_FBDIV 4 \ TX_NUM_OF_LANES 8 \ TX_CLK25_DIV 7 \ RX_NUM_OF_LANES 8 \ RX_CLK25_DIV 7 \ RX_DFE_LPM_CFG 0x0904 \ RX_CDR_CFG 0x03000023ff10400020 \ ]
Xilinx JESD204-PHY IP can be used as an alternative to implementing the physical layer, as it's part of Vivado without additional licensing. We don't currently provide software support for the Xilinx IP. The drawback when using the Xilinx IP is that it doesn't provide Eyescan functionality.
Reference clocks are needed to be feed to the QPLL/CPLL. In this design, we are using a shared reference clock for both receive and transmit channels. What is important to note is that the reference clocks for the transceiver QUAD must be connected to the MGTREFCLK pins either for the QUAD or an adjacent QUAD.
create_bd_port -dir I tx_ref_clk_0 create_bd_port -dir I rx_ref_clk_0 ad_xcvrpll tx_ref_clk_0 util_fmcomms11_xcvr/qpll_ref_clk_* ad_xcvrpll rx_ref_clk_0 util_fmcomms11_xcvr/cpll_ref_clk_* ad_xcvrpll axi_ad9162_xcvr/up_pll_rst util_fmcomms11_xcvr/up_qpll_rst_* ad_xcvrpll axi_ad9625_xcvr/up_pll_rst util_fmcomms11_xcvr/up_cpll_rst_*
The JESD204 data link layer is instantiated in the next lines, for both TX and RX type of peripheral paths. The ADI AD-IP-JESD204 implements the data link layer, supporting subclass 0 and run time reconfiguration through an AXI memory mapped interface.
adi_axi_jesd204_tx_create axi_ad9162_jesd 8 adi_axi_jesd204_rx_create axi_ad9625_jesd 8
The IP is equivalent with the Xilinx licensed JESD204 IP.
The transport layer peripherals are responsible for converter specific data framing and de-framing and provide a generic FIFO interface to the rest of the system.
adi_tpl_jesd204_tx_create axi_ad9162_core $TX_NUM_OF_LANES \ $TX_NUM_OF_CONVERTERS \ $TX_SAMPLES_PER_FRAME \ $TX_SAMPLE_WIDTH adi_tpl_jesd204_rx_create axi_ad9625_core $RX_NUM_OF_LANES \ $RX_NUM_OF_CONVERTERS \ $RX_SAMPLES_PER_FRAME \ $RX_SAMPLE_WIDTH
When UTIL_ADXCVR is instantiated, the channel inside of the IP may be different than the hardware pin connection to lessen the layout burden. Because of this, the UTIL_ADXCVR IP will rearrange the inside channels so that they correspond to the outside pin connection for the RX path, keeping a common transport layer.
ad_xcvrcon util_fmcomms11_xcvr axi_ad9162_xcvr axi_ad9162_jesd ad_xcvrcon util_fmcomms11_xcvr axi_ad9625_xcvr axi_ad9625_jesd
For a complete system, we use additional modules to transfer data. The transport layer transfers data continuously from/to the ADC/DAC. In the TX data path UPACK will only send the enabled channels to the DMA which in turn will transfer it to the system memory. Depending on system specifics, data offload FIFOs may be inserted between upack/cpack and the DMA. When a FIFO is used, the DMA connection to the DDR can run at a lower speed, as data capture cannot be done continuously.
ad_ip_instance util_upack2 util_ad9162_upack [list \ NUM_OF_CHANNELS $TX_NUM_OF_CONVERTERS \ SAMPLES_PER_CHANNEL $TX_SAMPLES_PER_CHANNEL \ SAMPLE_DATA_WIDTH $TX_SAMPLE_WIDTH \ ] ad_ip_instance axi_dmac axi_ad9162_dma [list \ DMA_TYPE_SRC 0 \ DMA_TYPE_DEST 1 \ ID 1 \ AXI_SLICE_SRC 0 \ AXI_SLICE_DEST 0 \ DMA_LENGTH_WIDTH 24 \ DMA_2D_TRANSFER 0 \ CYCLIC 0 \ DMA_DATA_WIDTH_SRC 256 \ DMA_DATA_WIDTH_DEST 256 \ ]
ad_ip_instance axi_dmac axi_ad9625_dma [list \ DMA_TYPE_SRC 1 \ DMA_TYPE_DEST 0 \ ID 0 \ AXI_SLICE_SRC 0 \ AXI_SLICE_DEST 0 \ SYNC_TRANSFER_START 0 \ DMA_LENGTH_WIDTH 24 \ DMA_2D_TRANSFER 0 \ CYCLIC 0 \ DMA_DATA_WIDTH_SRC 64 \ DMA_DATA_WIDTH_DEST 64 \ ]
# connections (dac) ad_connect axi_ad9162_core/dac_valid_0 util_ad9162_upack/fifo_rd_en for {set i 0} {$i < $TX_NUM_OF_CONVERTERS} {incr i} { ad_connect util_ad9162_upack/fifo_rd_data_$i axi_ad9162_core/dac_data_$i ad_connect axi_ad9162_core/dac_enable_$i util_ad9162_upack/enable_$i } ad_connect util_fmcomms11_xcvr/tx_out_clk_0 axi_ad9162_fifo/dac_clk ad_connect axi_ad9162_jesd_rstgen/peripheral_reset axi_ad9162_fifo/dac_rst ad_connect sys_cpu_clk axi_ad9162_fifo/dma_clk ad_connect sys_cpu_reset axi_ad9162_fifo/dma_rst ad_connect sys_cpu_clk axi_ad9162_dma/m_axis_aclk ad_connect sys_cpu_resetn axi_ad9162_dma/m_src_axi_aresetn ad_connect util_ad9162_upack/s_axis_valid VCC ad_connect util_ad9162_upack/s_axis_ready axi_ad9162_fifo/dac_valid ad_connect util_ad9162_upack/s_axis_data axi_ad9162_fifo/dac_data ad_connect axi_ad9162_core/dac_dunf axi_ad9162_fifo/dac_dunf ad_connect axi_ad9162_fifo/dma_xfer_req axi_ad9162_dma/m_axis_xfer_req ad_connect axi_ad9162_fifo/dma_ready axi_ad9162_dma/m_axis_ready ad_connect axi_ad9162_fifo/dma_data axi_ad9162_dma/m_axis_data ad_connect axi_ad9162_fifo/dma_valid axi_ad9162_dma/m_axis_valid ad_connect axi_ad9162_fifo/dma_xfer_last axi_ad9162_dma/m_axis_last ad_connect dac_fifo_bypass axi_ad9162_fifo/bypass # connections (adc) ad_connect axi_ad9625_jesd/rx_sof axi_ad9625_core/link_sof ad_connect axi_ad9625_jesd/rx_data_tdata axi_ad9625_core/link_data ad_connect axi_ad9625_jesd/rx_data_tvalid axi_ad9625_core/link_valid ad_connect util_fmcomms11_xcvr/rx_out_clk_0 axi_ad9625_fifo/adc_clk ad_connect axi_ad9625_jesd_rstgen/peripheral_reset axi_ad9625_fifo/adc_rst ad_connect axi_ad9625_core/adc_valid_0 axi_ad9625_fifo/adc_wr ad_connect axi_ad9625_core/adc_data_0 axi_ad9625_fifo/adc_wdata ad_connect sys_cpu_clk axi_ad9625_fifo/dma_clk ad_connect sys_cpu_clk axi_ad9625_dma/s_axis_aclk ad_connect sys_cpu_resetn axi_ad9625_dma/m_dest_axi_aresetn ad_connect axi_ad9625_fifo/dma_wr axi_ad9625_dma/s_axis_valid ad_connect axi_ad9625_fifo/dma_wdata axi_ad9625_dma/s_axis_data ad_connect axi_ad9625_fifo/dma_wready axi_ad9625_dma/s_axis_ready ad_connect axi_ad9625_fifo/dma_xfer_req axi_ad9625_dma/s_axis_xfer_req ad_connect axi_ad9625_core/adc_dovf axi_ad9625_fifo/adc_wovf
The below instructions assign addresses to all AXI modules in the design. These will be used when generating the device tree in linux.
ad_cpu_interconnect 0x44A60000 axi_ad9162_xcvr ad_cpu_interconnect 0x44A00000 axi_ad9162_core ad_cpu_interconnect 0x44A90000 axi_ad9162_jesd ad_cpu_interconnect 0x7c420000 axi_ad9162_dma ad_cpu_interconnect 0x44A50000 axi_ad9625_xcvr ad_cpu_interconnect 0x44A10000 axi_ad9625_core ad_cpu_interconnect 0x44AA0000 axi_ad9625_jesd ad_cpu_interconnect 0x7c400000 axi_ad9625_dma
The below instructions assign an HP port to all AXI masters, through an interconnect. If there is a single master per interconnect, it will be bypassed in the interconnect. The HP3 connections allow the physical layer to transmit eyescan data to memory, without software interference.
# gt uses hp3, and 100MHz clock for both DRP and AXI4 ad_mem_hp3_interconnect sys_cpu_clk sys_ps7/S_AXI_HP3 ad_mem_hp3_interconnect sys_cpu_clk axi_ad9625_xcvr/m_axi # interconnect (mem/dac) ad_mem_hp1_interconnect sys_cpu_clk sys_ps7/S_AXI_HP1 ad_mem_hp1_interconnect sys_cpu_clk axi_ad9162_dma/m_src_axi ad_mem_hp2_interconnect sys_cpu_clk sys_ps7/S_AXI_HP2 ad_mem_hp2_interconnect sys_cpu_clk axi_ad9625_dma/m_dest_axi
ad_cpu_interrupt ps-10 mb-15 axi_ad9162_jesd/irq ad_cpu_interrupt ps-11 mb-14 axi_ad9625_jesd/irq ad_cpu_interrupt ps-12 mb-12 axi_ad9162_dma/irq ad_cpu_interrupt ps-13 mb-13 axi_ad9625_dma/irq
The reference clock that is used for the transceivers, must be captured by an IBUFDS_GTE2 block. Because UTIL_ADXCVR doesn't have the buffer instantiated, the best place to instantiate it is in system_top.v
.
IBUFDS_GTE2 i_ibufds_tx_ref_clk ( .CEB (1'd0), .I (trx_ref_clk_p), .IB (trx_ref_clk_n), .O (trx_ref_clk), .ODIV2 ());
We prefer using single ended signals as much as possible in the IPI system.
As shown below, the transceiver channels and ADC and DAC channels are not connected one to one.
set_property -dict {PACKAGE_PIN AH10} [get_ports rx_data_p[0]] ; ## C06 FMC_HPC_DP0_M2C_P set_property -dict {PACKAGE_PIN AH9 } [get_ports rx_data_n[0]] ; ## C07 FMC_HPC_DP0_M2C_N set_property -dict {PACKAGE_PIN AJ8 } [get_ports rx_data_p[1]] ; ## A02 FMC_HPC_DP1_M2C_P set_property -dict {PACKAGE_PIN AJ7 } [get_ports rx_data_n[1]] ; ## A03 FMC_HPC_DP1_M2C_N set_property -dict {PACKAGE_PIN AG8 } [get_ports rx_data_p[2]] ; ## A06 FMC_HPC_DP2_M2C_P set_property -dict {PACKAGE_PIN AG7 } [get_ports rx_data_n[2]] ; ## A07 FMC_HPC_DP2_M2C_N set_property -dict {PACKAGE_PIN AE8 } [get_ports rx_data_p[3]] ; ## A10 FMC_HPC_DP3_M2C_P set_property -dict {PACKAGE_PIN AE7 } [get_ports rx_data_n[3]] ; ## A11 FMC_HPC_DP3_M2C_N set_property -dict {PACKAGE_PIN AD6 } [get_ports rx_data_p[4]] ; ## B12 FMC_HPC_DP7_M2C_P set_property -dict {PACKAGE_PIN AD5 } [get_ports rx_data_n[4]] ; ## B13 FMC_HPC_DP7_M2C_N set_property -dict {PACKAGE_PIN AH6 } [get_ports rx_data_p[5]] ; ## A14 FMC_HPC_DP4_M2C_P set_property -dict {PACKAGE_PIN AH5 } [get_ports rx_data_n[5]] ; ## A15 FMC_HPC_DP4_M2C_N set_property -dict {PACKAGE_PIN AF6 } [get_ports rx_data_p[6]] ; ## B16 FMC_HPC_DP6_M2C_P set_property -dict {PACKAGE_PIN AF5 } [get_ports rx_data_n[6]] ; ## B17 FMC_HPC_DP6_M2C_N set_property -dict {PACKAGE_PIN AG4 } [get_ports rx_data_p[7]] ; ## A18 FMC_HPC_DP5_M2C_P set_property -dict {PACKAGE_PIN AG3 } [get_ports rx_data_n[7]] ; ## A19 FMC_HPC_DP5_M2C_N set_property -dict {PACKAGE_PIN AK10} [get_ports tx_data_p[0]] ; ## C02 FMC_HPC_DP0_C2M_P set_property -dict {PACKAGE_PIN AK9 } [get_ports tx_data_n[0]] ; ## C03 FMC_HPC_DP0_C2M_N set_property -dict {PACKAGE_PIN AK6 } [get_ports tx_data_p[1]] ; ## A22 FMC_HPC_DP1_C2M_P set_property -dict {PACKAGE_PIN AK5 } [get_ports tx_data_n[1]] ; ## A23 FMC_HPC_DP1_C2M_N set_property -dict {PACKAGE_PIN AJ4 } [get_ports tx_data_p[2]] ; ## A26 FMC_HPC_DP2_C2M_P set_property -dict {PACKAGE_PIN AJ3 } [get_ports tx_data_n[2]] ; ## A27 FMC_HPC_DP2_C2M_N set_property -dict {PACKAGE_PIN AK2 } [get_ports tx_data_p[3]] ; ## A30 FMC_HPC_DP3_C2M_P set_property -dict {PACKAGE_PIN AK1 } [get_ports tx_data_n[3]] ; ## A31 FMC_HPC_DP3_C2M_N set_property -dict {PACKAGE_PIN AD2 } [get_ports tx_data_p[4]] ; ## B32 FMC_HPC_DP7_C2M_P set_property -dict {PACKAGE_PIN AD1 } [get_ports tx_data_n[4]] ; ## B33 FMC_HPC_DP7_C2M_N set_property -dict {PACKAGE_PIN AH2 } [get_ports tx_data_p[5]] ; ## A34 FMC_HPC_DP4_C2M_P set_property -dict {PACKAGE_PIN AH1 } [get_ports tx_data_n[5]] ; ## A35 FMC_HPC_DP4_C2M_N set_property -dict {PACKAGE_PIN AE4 } [get_ports tx_data_p[6]] ; ## B36 FMC_HPC_DP6_C2M_P set_property -dict {PACKAGE_PIN AE3 } [get_ports tx_data_n[6]] ; ## B37 FMC_HPC_DP6_C2M_N set_property -dict {PACKAGE_PIN AF2 } [get_ports tx_data_p[7]] ; ## A38 FMC_HPC_DP5_C2M_P set_property -dict {PACKAGE_PIN AF1 } [get_ports tx_data_n[7]] ; ## A39 FMC_HPC_DP5_C2M_N
In default configuration the reference clocks run at 122.88 MHz, the RX core clock at 122.88MHz and TX core clock at 245.76MHz. See the block diagram above for detailed clock tree.
create_clock -name rx_ref_clk -period 6.40 [get_ports trx_ref_clk_p] create_clock -name tx_div_clk -period 3.20 [get_pins i_system_wrapper/system_i/util_fmcomms11_xcvr/inst/i_xch_0/i_gtxe2_channel/TXOUTCLK] create_clock -name rx_div_clk -period 6.40 [get_pins i_system_wrapper/system_i/util_fmcomms11_xcvr/inst/i_xch_0/i_gtxe2_channel/RXOUTCLK]
When building the project, you should always use the recommended version of the tools for the specific release. In this example, we'll use release 2019_r1, which has Vivado 2018.3 as the recommended version. If you're using different Vivado versions, it's possible that there are slight modifications on how the synthesis works, or different Xilinx IP changes, which affect the system functionality.
mkdir adi cd adi git clone https://github.com/analogdevicesinc/hdl.git cd hdl/ git status ## check for everything, including branch name git checkout hdl_2019_r1 ## change to the hdl_2019_r1 branch make -C projects/fmcomms11/zc706
Questions? Feel free to ask your questions in EngineerZone support forums.