Wiki

This version is outdated by a newer approved version.DiffThis version (08 May 2014 12:37) was approved by Andrei Cozma.The Previously approved version (06 May 2014 16:43) is available.Diff

This is an old revision of the document!


AD-FMCMOTCON1-EBZ User Guide

The AD-FMCMOTCON1-EBZ is a complete motor drive system on an FMC board. Information on the card, and how to use it, the design package that surrounds it, and the software which can make it work, can be found here.

The purpose of the AD-FMCMOTCON1-EBZ is to provide a complete motor drive system demonstrating efficient control of Brushed DC, BLDC, PMSM and Stepper motors. It consists of 2 boards: a controller board and a drive board. The system incorporates high quality power sources; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; flexible control with FPGA/SoC interface.

The AD-DYNO1-EBZ dynamometer is provided as an extension of the drive system. This is a dynamically adjustable load that can be used to test real-time motor control performance. It consists of two BLDC motors directly coupled through a rigid connection. One of the BLDC motors acts as a load and is controlled by the DYNO’s embedded control system while then second motor is driven by the AD-FMCMOTCON1-EBZ.

This platform is intended to be used as a prototyping system to verify the hardware and the control algorithms before moving to the production stage. It helps reduce the time needed to move a motor control system from concept to production. Example reference designs showing how to use the control solution with Xilinx FPGAs or SoCs and Simulink from Mathworks are provided together with the hardware.

Videos

3540825244001

resources/eval/user-guides/ad-fmcmotcon1-ebz.1399545465.txt.gz · Last modified: 08 May 2014 12:37 by Andrei Cozma