The Linux Industrial I/O (IIO) subsystem is intended to provide support for devices that, in some sense, are analog-to-digital or digital-to-analog converters. Devices that fall into this category are:
The IIO Divers for the motor control solution require the HDL cores to have a specified register map. A DMA interface is set up for high speed data transfer using multiple multiplexed data channels. Below is the list of IIO drivers for the motor control solution.
IIO DriverName | Description | Channels |
---|---|---|
ad-mc-adc | Driver for the controller board ADCs | CH1 - Ia measurement CH2 - Ib measurement CH3 - It measurement CH4 - Vbus measurement |
ad-mc-adc2 | Driver for the low voltage drive board ADCs | CH1 - Ia measurement CH2 - Ib measurement CH3 - It measurement |
ad-mc-speed | Driver for the speed and position processing block | CH1 - Speed measurement |
ad-mc-ctrl | Driver for the motor controller block | CH1 : CH8 - Controller monitoring signals |
Each IIO driver has in the device tree and entry related to the actual driver and an entry corresponding to the allocated DMA. Below is an example of how the device tree looks for the motor control IIO drivers.
ad-mc-adc@40500000 { compatible = "xlnx,axi-ad-mc-adc-1.00.a"; reg = <0x40500000 0x10000>; dmas = <&axi_dma_0 0>; dma-names = "ad-mc-adc-dma"; }; axi_dma_1: axidma1@40420000 { compatible = "adi,axi-dmac-1.00.a"; reg = <0x40420000 0x10000>; #dma-cells = <1>; interrupts = <0 54 0>; clocks = <&clkc 16>; dma-channel { adi,buswidth = <32>; adi,type = <0>; }; }; ad-mc-ctrl@40520000 { compatible = "xlnx,axi-ad-mc-ctrl-1.00.a"; reg = <0x40520000 0x10000>; dmas = <&axi_dma_1 0>; dma-names = "ad-mc-ctrl-dma"; }; axi_dma_2: axidma2@40410000 { compatible = "adi,axi-dmac-1.00.a"; reg = <0x40410000 0x10000>; #dma-cells = <1>; interrupts = <0 56 0>; clocks = <&clkc 16>; dma-channel { adi,buswidth = <32>; adi,type = <0>; }; }; ad-mc-speed@40510000 { compatible = "xlnx,axi-ad-mc-speed-1.00.a"; reg = <0x40510000 0x10000>; dmas = <&axi_dma_2 0>; dma-names = "ad-mc-speed-dma"; }; axi_dma_3: axidma3@40430000 { compatible = "adi,axi-dmac-1.00.a"; reg = <0x40430000 0x10000>; #dma-cells = <1>; interrupts = <0 53 0>; clocks = <&clkc 16>; dma-channel { adi,buswidth = <64>; adi,type = <0>; }; }; ad-mc-adc2@40530000 { compatible = "xlnx,axi-ad-mc-adc-1.00.a"; reg = <0x40530000 0x10000>; dmas = <&axi_dma_3 0>; dma-names = "ad-mc-adc-dma"; };