In electronics, a diode is a two-terminal component with an asymmetric current vs. voltage characteristic, with low (ideally zero) resistance to current flow in one direction, and high (ideally infinite) resistance in the other. A silicon semiconductor diode, the most common type, is a single crystal piece of semiconductor material with a PN junction connected to two electrical terminals.
A PN junction is formed by joining p-type and n-type semiconductors together in a single crystal lattice. The term junction refers to the boundary interface where the two regions of the semiconductor meet. If the junction was constructed of two separate pieces this would introduce a discontinuity in the crystal lattice, so PN junctions are created in a single crystal of semiconductor by introducing certain impurities called dopants, for example by ion implantation, diffusion, or by epitaxy (growing a layer of crystal doped with n-type impurities on top of a layer of crystal doped with p-type impurities for example).
PN junctions are the elementary building blocks of almost all semiconductor electronic devices such as diodes, transistors, solar cells, LEDs, and integrated circuits; they are the active sites where the electronic action of the device takes place. For example, a common type of transistor, the bipolar junction transistor, consists of two PN junctions in series, in the form NPN or PNP.
The PN junction exhibits some interesting properties which have useful applications in solid state electronics. A p-doped semiconductor is relatively conductive. The same is true of an n-doped semiconductor, but the junction between p and n type regions is a nonconductor. This non-conducting layer, called the depletion layer, occurs because the electrically charged carriers, electrons in n-type and holes p-type silicon, diffuse into the other type of material (i.e. electrons in p-type and holes in n-type) and eliminate each other in a process called recombination. This diffusion of charge causes a built in potential difference across the depletion region. By manipulating this non-conductive layer, PN junctions are commonly used as diodes: circuit elements that allow a flow of electricity in one direction but not in the other (opposite) direction. This property is explained in terms of forward bias and reverse bias, where the term bias refers to the application of an electric voltage across the PN junction. A PN junction will conduct current when the applied external voltage exceeds the built in potential of the junction.
In a PN junction, without an external applied voltage, an equilibrium condition is reached in which a potential difference is formed across the junction. This potential difference is called the built-in potential, VBI.
At the junction of p-type and n-type semiconductors, higher concentration of electrons in the n-type region near the PN interface tend to diffuse into the p-type region. As electrons diffuse, they leave positively charged ions (donors) in the n region. Similarly, the higher concentration of holes on the p-type side near the PN interface begin to diffuse into the n-type region leaving fixed ions (acceptors) with negative charge. The regions just adjacent on either side of the PN interface lose their neutrality and become charged, forming the space charge region or depletion layer (see figure 5.1).
Figure 5.1 PN junction at equilibrium
The electric field created by the space charge region opposes the diffusion process for both electrons and holes. There are two simultaneous phenomena: the diffusion process that tends to generate more space charge, and the electric field generated by the space charge that tends to counteract the diffusion. At equilibrium these two forces balance each other. The carrier concentration profile at equilibrium is shown in figure 5.1 with blue and red lines. Also shown are the two counterbalancing phenomena that establish equilibrium.
The space charge region is a zone with a net charge provided by the fixed ions (donors or acceptors) that have been left uncovered by majority carrier diffusion. When equilibrium is reached, the charge density is approximated by the displayed step function in the figure 5.2 Q(x) graph. In fact, the region is completely depleted of majority carriers (leaving a charge density equal to the net doping level), and the edge between the space charge region and the neutral region is quite sharp. The space charge region has the same charge on both sides of the PN interface, thus it extends farther into the less heavily doped side (the n side in figures 5.1 and 5.2).
Figure 5.2
In forward bias, a positive voltage is applied to the p-type side with respect to the n-type side of the junction. With a voltage applied in this way, the holes in the p-type region and the electrons in the n-type region are forced towards the junction. This reduces the width of the depletion layer. The positive charge applied to the p-type material repels the holes, while the negative charge applied to the n-type material repels the electrons. The distance between the electrons and holes decreases as they are forced towards the junction. This lowers the built in potential barrier. With increasing forward-bias voltage, the depletion layer eventually becomes thin enough that the built in electric field can no longer counteract the charge carrier motion across the PN junction, consequently reducing the electrical resistance. The electrons which cross the PN junction into the p-type material (or holes which cross into the n-type material) will diffuse in the near-neutral region. Therefore, the amount of minority diffusion in the near-neutral zones determines the amount of current that may flow through the diode.
Only majority carriers (electrons in n-type material or holes in p-type) can flow through a semiconductor for a macroscopic length. With this in mind, consider the flow of electrons across the junction. The forward bias causes a force on the electrons pushing them from the N side toward the P side. With forward bias, the depletion region is narrow enough that electrons can cross the junction and are injected into the p-type material. However, they do not continue to flow through the p-type material indefinitely, because it is energetically favorable for them to recombine with holes. The average length an electron travels through the p-type material before recombining is called the diffusion length, and it is typically on the order of microns.
Although the electrons penetrate only a short distance into the p-type material before recombining, the electric current continues uninterrupted, because holes (the majority carriers) begin to flow in the opposite direction replacing the ones that the minority carrier electrons recombined with. The total current (the sum of the electron and hole currents) is constant in space, because any variation would cause charge to build up over time (this is Kirchhoff's current law). The flow of holes from the p-type region into the n-type region is exactly analogous to the flow of electrons from N to P (electrons and holes swap roles and the signs of all currents and voltages are reversed).
Therefore, the macroscopic picture of the current flow through the diode involves electrons flowing through the n-type region toward the junction, holes flowing through the p-type region in the opposite direction toward the junction, and the two kinds of carriers constantly recombining in the vicinity (given by the diffusion length) of the junction. The electrons and holes travel in opposite directions, but they also have opposite charges, so the overall current is in the same direction on both sides of the diode, as required.
Reverse bias usually refers to how a diode is used in a circuit. If a diode is reverse biased, the voltage at the cathode is higher than that at the anode. Therefore, no current will flow until the electric field is so high that the diode breaks down.
Because the p-type material is now connected to the negative side of the applied voltage, the holes in the p-type material are pulled away from the junction, causing the thickness of the depletion layer to increase. Similarly, because the n-type region is connected to the positive side, the electrons will also be pulled away from the junction. Therefore the depletion layer widens, and does so increasingly with increasing reverse-bias voltage. This increases the voltage barrier causing a high resistance to the flow of charge carriers thus allowing only a very small electric current to leak across the PN junction.
The strength of the depletion layer electric field increases as the reverse-bias voltage increases. Once the electric field intensity increases beyond a critical level, the PN junction depletion layer breaks-down and current begins to flow, usually by either the Zener or avalanche breakdown processes. Both of these breakdown processes are non-destructive and are reversible, as long as the amount of current flowing does not reach levels that cause the semiconductor material to overheat and cause thermal damage.
This effect is used to one's advantage in zener diode regulator circuits. Zener diodes have a well-defined low reverse breakdown voltage by design. A typical value for the breakdown voltage is for instance 6.2V. This means that the voltage at the cathode can never be more than 6.2V higher than the voltage at the anode, because the diode will break down, and therefore conduct, if the voltage gets any higher. This effectively limits the voltage across the diode.
Another application where reverse biased diodes are used is in varactor (variable capacitor) diodes. The depletion layer acts as an insulator between the two conducting plates or terminals of the diode. The capacitance is a function of the width of the insulating layer and its area. The width of the depletion zone of any diode changes with the voltage applied. This varies the capacitance of the diode. Varactors are purposely designed with one side of the PN junction lightly doped so there will be a large depletion region on that side of the diode. This thicker region will also be effected more by the applied bias voltage and thus the change in capacitance of the diode ( ΔC/ΔV ) will be a strong function of the applied bias.
The forward-bias and the reverse-bias properties of the PN junction imply that it can be used as a diode. A PN junction diode allows electric charges to flow in one direction, but not in the opposite direction; negative charges (electrons) can easily flow through the junction from N to P but not from P to N and the reverse is true for holes. When the PN junction is forward biased, electric charge flows freely due to reduced resistance of the PN junction. When the PN junction is reverse biased, however, the junction barrier (and therefore resistance) becomes greater and charge flow is very small.
The figure 5.3 below gives the schematic symbol for a diode (a) and a picture of a typical diode from the lab (b). Diodes are quite common and useful devices. One can think of a diode as a device which allows current to flow in only one direction. This is an over-simplification, but a good approximation.
(a)
(b)
Figure 5.3: (a) Diode Schematic Symbol (b) small signal diode.
As was discussed earlier, semiconductor diodes are fabricated as a two layer structure forming a PN junction. Semiconductors, such as silicon or germanium, can be doped with small concentrations of specific impurities to yield a material which conducts electricity via electron transport (n-type) or via holes (p-type). When layers of these two types of doped semiconductor are constructed to form a PN junction, electrons migrate away from the n-type side and holes migrate away from the p-type side, as shown in figure. 5.1. This redistribution of charge gives rise to a potential gap VBI across the junction, as depicted in the Figure. This gap is VBI ~0.7 V for silicon and ~0.3 V for germanium.
Figure 5.4 A PN junction, forming a voltage gap across the junction
When this PN junction diode is now connected to an external voltage, this can effectively increase or decrease the built in potential gap. This gives rise to very different behavior, depending upon the polarity of this external voltage, as shown by the typical V - I plot of figure. 5.5. When the diode is reverse biased, as depicted in figure 5.6, the gap increases, and very little current flows across the junction (until eventually in this example at ~ 6.2V field break down occurs). Conversely, a forward biased configuration decreases the gap, approaching zero for an external voltage equal to the gap voltage, and current can flow easily.
The expression for the (forward bias) diode voltage VD is as follows:
Where:
VD = applied voltage across the diode
k = Boltzman constant (1.38E-23 Joules/Kelvin)
T = the absolute temperature in Kelvin
q = the electron charge (1.6E-19 Coulombs)
ID = the actual current through the diode
IS = the diffusion current (a device dependent constant)
(The so called thermal voltage, VT, is kT/q = 26 mV at room temperature.)
The equation above can be rearranged to provide ID:
Thus, when reverse biased, the diode behaves much like an open switch; and when forward biased, for currents of about 10 mA or greater, the diode gives a nearly constant voltage drop of ~0.7 V. The diffusion current, IS,is dependent on the doping level of n-type and p-type impurities, the area of the diode and (very much) on temperature. A reasonable starting point for a small-geometry Integrated Circuit diode is IS=1E-16.
Figure 5.5: The voltage, VD vs. current, ID behavior of a diode
The opposing charges in a semiconductor junction are no different from those on the plates of a capacitor. So every junction has a capacitance; but since the distance between the electrons and holes, the depletion layer, changes with applied voltage, the capacitance depends on the applied voltage. The lower the voltage, the higher the capacitance, and it will increase right into the forward bias region.
Figure 5.6 Voltage vs. Current behavior of a 6.2 Volt Zener diode
One additional thing to note about real diodes, is the series resistance in the semiconductor material not taken up by the depletion region. For a common concentration of 5E15 (dopant atoms per cubic centimeter, giving a practical breakdown voltage in an IC of about 25 Volts), the bulk resistivity is about 1 Ohm-cm for phosphorus (n-type) doped silicon and 3 Ohm-cm for boron (p-type). For comparison, a metal like aluminum has a resistivity of 2.8 microOhm-cm, copper 1.7 microOhm-cm. Bulk Resistivity (ρ or rho) is measured between opposite surfaces of a cube of material with a side-length (w, h, l) of 1cm (10mm).
From the diode voltage equation, 5.1, we can see that it contains the absolute temperature term T. In addition, the diffusion current, IS, is not actually constant but is highly temperature dependent. In the lower set of plots in figure 5.7 the simulated diode voltage vs. temperature is plotted for four different diode currents (green=1 mA, blue=2 mA, red=5mA and cyan=10mA). It is apparent from the curves that the diode voltage has a rather strong negative temperature dependence.
In the upper plot the difference between the 2mA and the 1mA curves is plotted along with the difference between the 5mA and 10mA curves. These two results lie exactly on top of each other. The reason for this is apparent if we examine the diode voltage equation more closely.
Figure 5.7 Diode Voltage vs. Temperature at 1mA, 2mA, 5mA and 10mA
Rearranging and assuming IS1 = IS2 we get:
Now the strong temperature effect of ISdrops out of the equation and we are left with just the absolute temperature term, T, which makes ΔVDproportional to absolute temperature (PTAT). Both VD2-VD1 and VD4-VD3 have the same 2:1 ratio for their currents and thus the ΔVD curves will exactly lie on top of each other. At room temperature the thermal voltage VT is about 26 mV which when multiplied by ln(2) is the approximately 18mV seen in the graph at 25 degrees.
The linear model of the diode approximates the exponential I - V characteristics by a straight line that is tangent to the actual curve at the DC bias point. Figure 5.8 shows the curve with the tangent line at the point (VD, ID). The curve intersects the horizontal axis at the voltage VD0. For small changes in VDand ID about the tangent point, the tangent line gives a good approximation to the actual curve.
Figure 5.8 I - V characteristics with tangent line at (VD, ID)
The slope of the tangent line is given by:
ID is often much larger than ISso the equation is often simplified to:
The equation of the tangent line is:
Because the diode equation for ID as a function of VD is non-linear, the tools of linear circuit analysis cannot be applied to circuits containing diodes the same way one would a circuit containing just resistors. However, if the diode current is known for a particular voltage, linear circuit analysis can be used to predict the change in current for a given change in voltage, provided the change is incrementally small. Such an approach is called a small-signal analysis. A few words about notation:
Where:
VD and ID are DC bias values and vd and id are small-signal changes about the bias values.
The small-signal resistance is defined as the ratio of vd to id and is given by:
This results in the same rd as in the linear tangent model of the diode in figure 5.8. Thus the small-signal model of the diode when forward biased is a resistor of value rd. The value of rd is inversely proportional to the current through it. Each time the current is doubled, the resistance is halved. It follows from the linear diode model that rd can be interpreted graphically as the reciprocal of the slope of the iD versus vD curve at the point (VD, ID).
ADALM1000 Lab Activity 2. Diode I vs. V curves
ADALM1000 Lab Activity, The voltage dependent capacitance of the PN junction
ADALM2000 Lab Activity 2. Diode I vs. V curves
ADALM2000 Lab Activity, The voltage dependent capacitance of the PN junction
ADALM2000 Lab Activity: Differential Temperature Sensor
Return to Previous Chapter
Go to Next Chapter
Return to Table of Contents