The AD5758 is a single-channel, voltage and current output digital-to-analog converter (DAC) that operates with a power supply range from −33 V minimum on AVSS to +33 V maximum on AVDD1 with a maximum operating voltage between the two rails of 60 V. On-chip DPC minimizes package power dissipation, which is achieved by regulating the supply voltage (VDPC+) to the VIOUT output driver circuitry from 5 V to 27 V using a buck dc-to-dc converter, optimized for minimum on-chip power dissipa-tion. The CHART pin enables a HART signal to be coupled onto the current output.
The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, DSP, and microcontroller interface standards. The interface also features an optional SPI cyclic redundancy check (CRC) and a watchdog timer. The AD5758 offers improved diagnostic features from its predecessors, such as output current monitoring and an integrated 12-bit diagnostic ADC. Additional robustness is provided by the inclusion of a fault protection switch on VIOUT, +VSENSE, and −VSENSE pins.
In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design in general.
In order to build the HDL design the user has to go through the following steps:
In order to perform the software setup the user has to go through the following steps:
Function | Description |
---|---|
static uint8_t ad5758_compute_crc8(uint8_t *data, uint8_t data_size) | Compute CRC8 checksum. |
static int32_t ad5758_spi_reg_read(struct ad5758_dev *dev, uint8_t reg_addr, uint16_t *reg_data); | Read from device. |
static int32_t ad5758_spi_reg_write(struct ad5758_dev *dev, uint8_t reg_addr, uint16_t reg_data); | Write to device. |
static int32_t ad5758_spi_write_mask(struct ad5758_dev *dev, uint8_t reg_addr, uint32_t mask, uint16_t data); | SPI write to device using a mask. |
int32_t ad5758_set_crc(struct ad5758_dev *dev, uint8_t crc_en); | Enable/disable SPI CRC function. |
int32_t ad5758_wait_for_refresh_cycle(struct ad5758_dev *dev); | Busy wait until CAL_MEM_UNREFRESHED bit in the DIGITAL_DIAG_RESULTS clears. |
int32_t ad5758_soft_reset(struct ad5758_dev *dev); | Initiate a software reset. |
int32_t ad5758_calib_mem_refresh(struct ad5758_dev *dev); | Initiate a calibration memory refresh to the shadow registers. |
int32_t ad5758_set_dc_dc_conv_mode(struct ad5758_dev *dev, enum ad5758_dc_dc_mode mode); | Configure the dc-to-dc controller mode. |
int32_t ad5758_set_dc_dc_ilimit(struct ad5758_dev *dev, enum ad5758_dc_dc_ilimt ilimit); | Set the dc-to-dc converter current limit. |
int32_t ad5758_fault_prot_switch_en(struct ad5758_dev *dev, uint8_t enable); | Enable/disable VIOUT Fault Protection Switch. |
int32_t ad5758_internal_buffers_en(struct ad5758_dev *dev, uint8_t enable); | Enable/disable Enable Internal Buffers. |
int32_t ad5758_set_out_range(struct ad5758_dev *dev, enum ad5758_output_range range); | Select Output Range. |
int32_t ad5758_slew_rate_config(struct ad5758_dev *dev, enum ad5758_slew_rate_clk clk, uint8_t enable); | Configure the slew rate by setting the clock and enable/disable the control. |
int32_t ad5758_dac_input_write(struct ad5758_dev *dev, uint16_t code); | Write DAC data to the input register. |
int32_t ad5758_dac_output_en(struct ad5758_dev *dev, uint8_t enable); | Enable/disable VIOUT. |
int32_t ad5758_clear_dig_diag_flag(struct ad5758_dev *dev, enum ad5758_dig_diag_flags flag); | Clear the error flags for the on-chip digital diagnostic features. |
int32_t ad5758_set_clkout_config(struct ad5758_dev *dev, enum ad5758_clkout_config config, enum ad5758_clkout_freq freq); | Configure CLKOUT by setting the frequency and enabling/disabling the option. |
int32_t ad5758_select_adc_ip(struct ad5758_dev *dev, enum ad5758_adc_ip adc_ip_sel); | Select which node to multiplex to the ADC. |
int32_t ad5758_select_adc_depth(struct ad5758_dev *dev, uint8_t num_of_channels); | Set depth of the sequencer. |
int32_t ad5758_set_adc_channel_input(struct ad5758_dev *dev, uint8_t channel, enum ad5758_adc_ip adc_ip_sel); | Load the desired channel into the sequencer with the adc input. |
int32_t ad5758_set_adc_mode(struct ad5758_dev *dev, enum ad5758_adc_mode adc_mode, uint8_t enable); | Configure the ADC into one of four modes of operation. |
int32_t ad5758_init(struct ad5758_dev **device, struct ad5758_init_param init_param); | Set up the device from power-on or reset condition with the correct. |
enum ad5758_dc_dc_mode { DC_DC_POWER_OFF, DPC_CURRENT_MODE, DPC_VOLTAGE_MODE, PPC_CURRENT_MODE, }; enum ad5758_dig_diag_flags { DIAG_SPI_CRC_ERR, DIAG_SLIPBIT_ERR, DIAG_SCLK_COUNT_ERR, DIAG_INVALID_SPI_ACCESS_ERR = 4, DIAG_CAL_MEM_CRC_ERR, DIAG_INVERSE_DAC_CHECK_ERR, DIAG_DAC_LATCH_MON_ERR = 8, DIAG_THREE_WI_RC_ERR, DIAG_WDT_ERR = 11, DIAG_ERR_3WI, DIAG_RESET_OCCURRED, }; enum ad5758_clkout_config { CLKOUT_DISABLE, CLKOUT_ENABLE, }; enum ad5758_clkout_freq { CLKOUT_FREQ_416_KHZ, CLKOUT_FREQ_435_KHZ, CLKOUT_FREQ_454_KHZ, CLKOUT_FREQ_476_KHZ, CLKOUT_FREQ_500_KHZ, CLKOUT_FREQ_526_KHZ, CLKOUT_FREQ_555_KHZ, CLKOUT_FREQ_588_KHZ, }; enum ad5758_slew_rate_clk { SR_CLOCK_240_KHZ, SR_CLOCK_200_KHZ, SR_CLOCK_150_KHZ, SR_CLOCK_128_KHZ, SR_CLOCK_64_KHZ, SR_CLOCK_32_KHZ, SR_CLOCK_16_KHZ, SR_CLOCK_8_KHZ, SR_CLOCK_4_KHZ, SR_CLOCK_2_KHZ, SR_CLOCK_1_KHZ, SR_CLOCK_512_HZ, SR_CLOCK_256_HZ, SR_CLOCK_128_HZ, SR_CLOCK_64_HZ, SR_CLOCK_16_HZ, }; enum ad5758_dc_dc_ilimt { ILIMIT_150_mA, ILIMIT_200_mA, ILIMIT_250_mA, ILIMIT_300_mA, ILIMIT_350_mA, ILIMIT_400_mA, }; enum ad5758_output_range { RANGE_0V_5V, RANGE_0V_10V, RANGE_M5V_5V, RANGE_M10V_10V, RANGE_0mA_20mA = 8, RANGE_0mA_24mA, RANGE_4mA_24mA, RANGE_M20mA_20mA, RANGE_M24mA_24mA, RANGE_M1mA_22mA, }; enum ad5758_adc_ip { ADC_IP_MAIN_DIE_TEMP, ADC_IP_DCDC_DIE_TEMP, ADC_IP_REFIN = 3, ADC_IP_REF2, ADC_IP_VSENSE = 13, ADC_IP_MVSENSE, ADC_IP_INT_AVCC = 20, ADC_IP_REGOUT, ADC_IP_VLOGIC, ADC_IP_INT_CURR_MON_VOUT, ADC_IP_REFGND, ADC_IP_AGND, ADC_IP_DGND, ADC_IP_VDPC, ADC_IP_AVDD2, ADC_IP_AVSS, ADC_IP_DCDC_DIE_NODE, ADC_IP_REFOUT, }; enum ad5758_adc_mode { ADC_MODE_KEY_SEQ = 2, ADC_MODE_AUTO_SEQ, ADC_MODE_SINGLE_CONV, ADC_MODE_SINGLE_KEY_CONV, }; struct ad5758_dev { /* SPI */ struct spi_desc *spi_desc; /* GPIO */ struct gpio_desc *reset_n; struct gpio_desc *ldac_n; /* Device Settings */ uint8_t crc_en; enum ad5758_dc_dc_mode dc_dc_mode; }; struct ad5758_init_param { /* SPI */ struct spi_init_param spi_init; /* GPIO */ struct gpio_init_param reset_n; struct gpio_init_param ldac_n; /* Device Settings */ uint8_t crc_en; enum ad5758_dc_dc_mode dc_dc_mode; enum ad5758_clkout_config clkout_config; enum ad5758_clkout_freq clkout_freq; enum ad5758_dc_dc_ilimt dc_dc_ilimt; enum ad5758_output_range output_range; enum ad5758_slew_rate_clk slew_rate_clk; }; |