The script can be run with no parameters. In this case, you will be asked to introduce the path and the name of the .hdf file and the path and the name of the folder where the project will be created.
For example:
Enter the system_top.hdf location "example => C:/workspace/my_proj1_hdf/system_top.hdf" system_top.hdf Enter the project build folder "example => C:/my_workspaces Note: use "/" instead of "\"" fmcomms2_zc706
The parameters that were specified in the previous example, can be passed directly if the script is run from a command line.
For example:
create_xilinx_sdk_project.bat D:/workspace/example_hdf/system_top.hdf D:/workspace/example_project/fmcadc2_zc706
Using “Xilinx Software Command Line Tool”, the projects can be created using the Makefiles.
If no parameters are specified, the default location of the .hdf file and of the folder where the project will be created is the current directory.
For example:
Xilinx Software Commandline Tool (XSCT) v2015.2 Build date : Jun 26 2015-17:09:09 Copyright 1986-2015 Xilinx, Inc. All Rights Reserved. Got $XILINX_SDK: C:/Xilinx/SDK/2015.2 xsct% cd C:/workspace/git/no-os/ad9361 xsct% dir Volume in drive C is DRIVE_C Volume Serial Number is CCB3-25B7 Directory of C:\workspace\git\no-os\ad9361 02/16/2016 02:57 PM <DIR> . 02/16/2016 02:57 PM <DIR> .. 10/14/2015 01:55 PM <DIR> chipscope 02/16/2016 01:55 PM 574 create_xilinx_sdk_project.bat 01/05/2016 01:18 PM 768 create_xilinx_sdk_project.sh 01/05/2016 01:18 PM 823 Makefile 01/05/2016 01:18 PM 429 README.md 01/05/2016 01:18 PM <DIR> scripts 02/16/2016 02:54 PM <DIR> sdk_project 01/29/2016 11:59 AM <DIR> sw 02/09/2016 12:15 PM 1,082,772 system_top.hdf 5 File(s) 1,085,366 bytes 6 Dir(s) 132,785,848,320 bytes free xsct% make -f Makefile 'creating project' xsct -s ../build_scripts/xilinx/create_sdk_project.tcl system_top.hdf sdk_project Got $XILINX_SDK: C:/Xilinx/SDK/2015.2 hdf file used: C:/workspace/git/no-OS/ad9361/system_top.hdf The build directory is: sdk_project C:/workspace/git/no-OS/ad9361/sdk_project was created FPGA CPU: ps7_cortexa9_0 Hardware platform project 'hw' created successfully. BSP project 'bsp' created successfully. Application project 'sw' created successfully. ./sw/ ./sw/platform_xilinx/ Building All Projects... Building workspace Building '/bsp' Invoking Make Builder...bsp Building '/hw' Building '/sw' Invoking scanner config builder on project Done. xsct%
The location of the .hdf file and of the folder where the project will be created can be also specified if it is required.
For example:
make -f Makefile hdf_file=./system_top.hdf project=./fmcomms2_zc706
The script can be run with no parameters. In this case, you will be asked to introduce the path and the name of the .hdf file and the path and the name of the folder where the project will be created.
The parameters that were specified in the previous example, can be passed directly if the script is run from a command line.
For example:
create_xilinx_sdk_project.sh ./system_top.hdf ./fmcomms2_zc706
The projects can be created using the Makefiles.
If no parameters are specified, the default location of the .hdf file and of the folder where the project will be created is the current directory.
The location of the .hdf file and of the folder where the project will be created can be also specified if it is required.
The workspaces created using the methods described previously, can be also opened using the Xilinx SDK GUI.
Open “Xilinx SDK” and browse for the location of the workspace.
The prebuilt project is included in the opened workspace.