This is an old revision of the document!
Click here to return to the Multiplexers and Demultiplexers page
The Cross Mux block allows route an input to one of selected output pins. The output for each input is selected based on the numeric value on the control.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Mono | No | Yes | No | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input Channel 0 |
Name | Type | Description |
---|---|---|
Output0 | Audio | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Index_Channel0 | 0 | 0 to number of outputs | Selects the output channel to route the input |
NumInputs | 1 | 1 to 20 | Number of input channels. Change in this value requires re-compilation |
NumOuputs | 1 | 1 to 20 | Number of input channels. Change in this value requires re-compilation |
Here,
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
Index_Channel0 | Selects the output channel to route the input | Float |
Here,