Click here to return to the Multiplexers and Demultiplexers page
The Cross Mux block allows route an input to one of selected output pins. The output for each input is selected based on the numeric value on the control.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————— | ——————-- | ——————————-- | —————————- |
Cross Mux | B | B | NA |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
InputX | Audio | Input Channel X |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
OutputX | Audio | Output Channel X |
Note:
GUI Parameter | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————————— | —————————————- |
Index_ChannelX | 0 | 0 to NumOuputs-1 | Selects the output channel to route the input |
NumInputs | 1 | 1 to 20 | Number of input channels. Change in this value requires re-compilation |
NumOuputs | 1 | 1 to 20 | Number of input channels. Change in this value requires re-compilation |
Note:
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————————- | ——————————————————————————-- | —————————————- | —————————- |
Index_ChannelX | Selects the output channel to route the input | Float | NA |
Note: