This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:inputoutput:output [05 Feb 2020 07:25] – Added an image Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:inputoutput:output [06 May 2021 07:54] – Prasad Kamath | ||
---|---|---|---|
Line 14: | Line 14: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^Name^ADSP-214xx^ADSP-215xx/ |
- | |Output| Yes | Yes|Yes| Yes| | + | |------------------|------------------------|--------------------------------------|----------------------------------| |
+ | |Output| Block & Sample| Block & Sample| Sample| | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | |--------------------------------|-------------------------------------------------------|-------------------------------------------------------------------| | ||
|input0|Audio|Outputs the audio to the hardware pin| | |input0|Audio|Outputs the audio to the hardware pin| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |--------------------------------|----------------------|--------------------------------|----------------------------------------| | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== |