This is an old revision of the document!
Click here to return to the IO page
The Output block routes signals to the hardware's physical outputs. Each block is linked to a single output channel.
Using the drop-down list, select the output channel to associate with a particular block.
Observe that as you drag more output blocks to your schematic, the number of output channels available in the drop-down list decreases because each output can only be associate with a single output block at a time.
The hardware outputs for a particular processor are limited. While designing you can see the number of outputs that are still available from the HWOutputs item of the Resources window.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Output | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
input0 | Audio | Outputs the audio to the hardware pin |
GUI Parameter Name | Default Value | Range | Function Description |
---|
No DSP Parameters