Click here to return to the IO page
The Output block routes signals to the hardware's physical outputs. Each block is linked to a single output channel.
Using the drop-down list, select the output channel to associate with a particular block.
Observe that as you drag more output blocks to your schematic, the number of output channels available in the drop-down list decreases because each output can only be associate with a single output block at a time.
The hardware outputs for a particular processor are limited. While designing you can see the number of outputs that are still available from the HWOutputs item of the Resources window.
Name | ADSP-214xx | ADSP-215xx/ADSP-SC5xx | ADAU145x/ADAU146x |
---|---|---|---|
—————— | ———————— | ————————————-- | ———————————- |
Output | Block & Sample | Block & Sample | Sample |
Name | Type | Description |
---|---|---|
——————————-- | ——————————————————- | ——————————————————————- |
input0 | Audio | Outputs the audio to the hardware pin |
Not applicable
No DSP Parameters