This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:filters:firfilter [05 Feb 2020 09:05] – Added an image Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:filters:firfilter [09 Aug 2023 12:15] (current) – Chiranjeevi Palle | ||
---|---|---|---|
Line 12: | Line 12: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |FirFilter| Yes | Yes|Yes| Yes| | + | | ------------------------- |
+ | |FIR Filter| B/S | B/S | S | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------ | ------------------------------ | ------------------------------------------------ | | ||
|Input0|Audio|Input Channel 0| | |Input0|Audio|Input Channel 0| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Output0|Control|Output channel 0| | + | | ------------------------------ | ------------------------------ | ------------------------------------------------ | |
+ | |Output0|Audio|Output channel 0| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |---------------------------------------|---------------------------|---------------------------------------------|----------------------------------------------------------| | ||
|NoOfTableValues|10|2 to 10000|Specifies the number of the coefficients used for FIR filter calculation| | |NoOfTableValues|10|2 to 10000|Specifies the number of the coefficients used for FIR filter calculation| | ||
|ByPassEnable|False|True/ | |ByPassEnable|False|True/ | ||
Line 31: | Line 35: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^ Parameter Name |
- | |NoOfTableValues|Specifies the number of the coefficients used for FIR filter calculation|Float| | + | | ------------------------------------ | ------------------------------------------------------------------------------------------------ | ---------------------------------------- | ---------------------------- | |
- | |ByPassEnable|Enabled/ | + | |NoOfTableValues|Specifies the number of the coefficients used for FIR filter calculation|Integer32|Integer32| |
- | |TableValues|Coefficients used to calcualte the FIR Filter|Float| | + | |TableValues|Coefficients used to calcualte the FIR Filter|Float|FixPoint8d24| |
\\ | \\ | ||