Click here to return to the Basic page
The Seven-Band Level Detector block calculates the input signal level, reading directly from the hardware in real-time, and displays the level graphically in seven frequency band meter displays:
The level detector performs the analysis only and does not modify the input signal. The signal at the output pin is identical to the input.
Use the On / Off button to enable or disable the display. The level detector will not function until the schematic design has been compiled and downloaded to the hardware and a USB communication channel is properly configured.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————————————-- | ——————-- | ——————————-- | —————————- |
Seven Band Level Detector | B/S | B/S | NA |
———————- | ————-- | ———————- |
Input0 | Audio | Input Channel 0 |
———————- | ————-- | ———————- |
Output0 | Audio | Output channel 0 |
GUI Parameter | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————— | —————————————- |
On/Off Switch | OFF | ON/OFF | Enable or Disable the Level Detector |
No DSP Parameters