This is an old revision of the document!
Click here to return to the Basic page
The Seven-Band Level Detector block calculates the input signal level, reading directly from the hardware in real-time, and displays the level graphically in seven frequency band meter displays:
The level detector performs the analysis only and does not modify the input signal. The signal at the output pin is identical to the input.
Use the On / Off button to enable or disable the display. The level detector will not function until the schematic design has been compiled and downloaded to the hardware and a USB communication channel is properly configured.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Seven Band Level Detector | Yes | Yes | Yes | Yes |
Input0 | Audio | Input Channel 0 |
Output0 | Control | Output channel 0 |
No configurable parameters
No DSP Parameters